In this example, we will be utilizing the XBOXUSB example from the USB_Host_Shield_2.0 Arduino library. This example can be found in the File dropdown menu (i.e. (1) File > Examples > USB Host Shield Library 2.0 > Xbox > XBOXUSB). Once the example has been opened, users should see the XBOXUSB.ino example sketch.
Select the XBOXUSB example sketch from the File drop-down menu.
/* Example sketch for the Xbox 360 USB library - developed by Kristian Lauszus For more information visit my blog: http://blog.tkjelectronics.dk/ or send me an e-mail: kristianl@tkjelectronics.com */#include<XBOXUSB.h>// Satisfy the IDE, which needs to see the include statment in the ino too.#ifdef dobogusinclude#include<spi4teensy3.h>#endif#include<SPI.h>USBUsb;XBOXUSBXbox(&Usb);voidsetup(){Serial.begin(115200);#if !defined(__MIPSEL__)while(!Serial);// Wait for serial port to connect - used on Leonardo, Teensy and other boards with built-in USB CDC serial connection#endifif(Usb.Init()==-1){Serial.print(F("\r\nOSC did not start"));while(1);//halt}Serial.print(F("\r\nXBOX USB Library Started"));}voidloop(){Usb.Task();if(Xbox.Xbox360Connected){if(Xbox.getButtonPress(LT)||Xbox.getButtonPress(RT)){Serial.print("LT: ");Serial.print(Xbox.getButtonPress(LT));Serial.print("\tRT: ");Serial.println(Xbox.getButtonPress(RT));Xbox.setRumbleOn(Xbox.getButtonPress(LT),Xbox.getButtonPress(RT));}elseXbox.setRumbleOn(0,0);if(Xbox.getAnalogHat(LeftHatX)>7500||Xbox.getAnalogHat(LeftHatX)<-7500||Xbox.getAnalogHat(LeftHatY)>7500||Xbox.getAnalogHat(LeftHatY)<-7500||Xbox.getAnalogHat(RightHatX)>7500||Xbox.getAnalogHat(RightHatX)<-7500||Xbox.getAnalogHat(RightHatY)>7500||Xbox.getAnalogHat(RightHatY)<-7500){if(Xbox.getAnalogHat(LeftHatX)>7500||Xbox.getAnalogHat(LeftHatX)<-7500){Serial.print(F("LeftHatX: "));Serial.print(Xbox.getAnalogHat(LeftHatX));Serial.print("\t");}if(Xbox.getAnalogHat(LeftHatY)>7500||Xbox.getAnalogHat(LeftHatY)<-7500){Serial.print(F("LeftHatY: "));Serial.print(Xbox.getAnalogHat(LeftHatY));Serial.print("\t");}if(Xbox.getAnalogHat(RightHatX)>7500||Xbox.getAnalogHat(RightHatX)<-7500){Serial.print(F("RightHatX: "));Serial.print(Xbox.getAnalogHat(RightHatX));Serial.print("\t");}if(Xbox.getAnalogHat(RightHatY)>7500||Xbox.getAnalogHat(RightHatY)<-7500){Serial.print(F("RightHatY: "));Serial.print(Xbox.getAnalogHat(RightHatY));}Serial.println();}if(Xbox.getButtonClick(UP)){Xbox.setLedOn(LED1);Serial.println(F("Up"));}if(Xbox.getButtonClick(DOWN)){Xbox.setLedOn(LED4);Serial.println(F("Down"));}if(Xbox.getButtonClick(LEFT)){Xbox.setLedOn(LED3);Serial.println(F("Left"));}if(Xbox.getButtonClick(RIGHT)){Xbox.setLedOn(LED2);Serial.println(F("Right"));}if(Xbox.getButtonClick(START)){Xbox.setLedMode(ALTERNATING);Serial.println(F("Start"));}if(Xbox.getButtonClick(BACK)){Xbox.setLedBlink(ALL);Serial.println(F("Back"));}if(Xbox.getButtonClick(L3))Serial.println(F("L3"));if(Xbox.getButtonClick(R3))Serial.println(F("R3"));if(Xbox.getButtonClick(LB))Serial.println(F("LB"));if(Xbox.getButtonClick(RB))Serial.println(F("RB"));if(Xbox.getButtonClick(XBOX)){Xbox.setLedMode(ROTATING);Serial.println(F("Xbox"));}if(Xbox.getButtonClick(A))Serial.println(F("A"));if(Xbox.getButtonClick(B))Serial.println(F("B"));if(Xbox.getButtonClick(X))Serial.println(F("X"));if(Xbox.getButtonClick(Y))Serial.println(F("Y"));}delay(1);}
Users will need to turn on and connect the controller to the USB-C host shield with a USB cable, before running the example.
8BitDo controller connected to the USB-C Host Shield with a USB-C cable.
Note
To turn on the controller, press the Start+X buttons. Users should see two status LEDs blinking at the bottom of the controller.
After the example begins, users should see an output in the Serial Monitor with print out based on the user's interaction with their controller.
Bluetooth Connection
In this example, we will be utilizing the XBOXONESBT example from the USB_Host_Shield_2.0 Arduino library. This example can be found in the File dropdown menu (i.e. (1) File > Examples > USB Host Shield Library 2.0 > Xbox > XBOXONESBT). Once the example has been opened, users should see the XBOXONESBT.ino example sketch.
Select the XBOXONESBT example sketch from the File drop-down menu.
/* Example sketch for the Xbox One S Bluetooth library - developed by Kristian Sloth Lauszus For more information visit the Github repository: github.com/felis/USB_Host_Shield_2.0 or send me an e-mail: lauszus@gmail.com */#include<XBOXONESBT.h>#include<usbhub.h>// Satisfy the IDE, which needs to see the include statement in the ino too.#ifdef dobogusinclude#include<spi4teensy3.h>#endif#include<SPI.h>USBUsb;//USBHub Hub1(&Usb); // Some dongles have a hub insideBTDBtd(&Usb);// You have to create the Bluetooth Dongle instance like so/* You can create the instance of the XBOXONESBT class in two ways */// This will start an inquiry and then pair with the Xbox One S controller - you only have to do this once// You will need to hold down the Sync and Xbox button at the same time, the Xbox One S controller will then start to blink rapidly indicating that it is in pairing modeXBOXONESBTXbox(&Btd,PAIR);// After that you can simply create the instance like so and then press the Xbox button on the device//XBOXONESBT Xbox(&Btd);voidsetup(){Serial.begin(115200);#if !defined(__MIPSEL__)while(!Serial);// Wait for serial port to connect - used on Leonardo, Teensy and other boards with built-in USB CDC serial connection#endifif(Usb.Init()==-1){Serial.print(F("\r\nOSC did not start"));while(1);//halt}Serial.print(F("\r\nXbox One S Bluetooth Library Started"));}voidloop(){Usb.Task();if(Xbox.connected()){if(Xbox.getAnalogHat(LeftHatX)>7500||Xbox.getAnalogHat(LeftHatX)<-7500||Xbox.getAnalogHat(LeftHatY)>7500||Xbox.getAnalogHat(LeftHatY)<-7500||Xbox.getAnalogHat(RightHatX)>7500||Xbox.getAnalogHat(RightHatX)<-7500||Xbox.getAnalogHat(RightHatY)>7500||Xbox.getAnalogHat(RightHatY)<-7500){if(Xbox.getAnalogHat(LeftHatX)>7500||Xbox.getAnalogHat(LeftHatX)<-7500){Serial.print(F("LeftHatX: "));Serial.print(Xbox.getAnalogHat(LeftHatX));Serial.print("\t");}if(Xbox.getAnalogHat(LeftHatY)>7500||Xbox.getAnalogHat(LeftHatY)<-7500){Serial.print(F("LeftHatY: "));Serial.print(Xbox.getAnalogHat(LeftHatY));Serial.print("\t");}if(Xbox.getAnalogHat(RightHatX)>7500||Xbox.getAnalogHat(RightHatX)<-7500){Serial.print(F("RightHatX: "));Serial.print(Xbox.getAnalogHat(RightHatX));Serial.print("\t");}if(Xbox.getAnalogHat(RightHatY)>7500||Xbox.getAnalogHat(RightHatY)<-7500){Serial.print(F("RightHatY: "));Serial.print(Xbox.getAnalogHat(RightHatY));}Serial.println();}if(Xbox.getButtonPress(LT)>0||Xbox.getButtonPress(RT)>0){if(Xbox.getButtonPress(LT)>0){Serial.print(F("LT: "));Serial.print(Xbox.getButtonPress(LT));Serial.print("\t");}if(Xbox.getButtonPress(RT)>0){Serial.print(F("RT: "));Serial.print(Xbox.getButtonPress(RT));Serial.print("\t");}Serial.println();}// Set rumble effectstaticuint16_toldLTValue,oldRTValue;if(Xbox.getButtonPress(LT)!=oldLTValue||Xbox.getButtonPress(RT)!=oldRTValue){oldLTValue=Xbox.getButtonPress(LT);oldRTValue=Xbox.getButtonPress(RT);uint8_tleftRumble=map(oldLTValue,0,1023,0,255);// Map the trigger values into a byteuint8_trightRumble=map(oldRTValue,0,1023,0,255);if(leftRumble>0||rightRumble>0)Xbox.setRumbleOn(leftRumble,rightRumble,leftRumble,rightRumble);elseXbox.setRumbleOff();}if(Xbox.getButtonClick(UP))Serial.println(F("Up"));if(Xbox.getButtonClick(DOWN))Serial.println(F("Down"));if(Xbox.getButtonClick(LEFT))Serial.println(F("Left"));if(Xbox.getButtonClick(RIGHT))Serial.println(F("Right"));if(Xbox.getButtonClick(VIEW))Serial.println(F("View"));if(Xbox.getButtonClick(MENU))Serial.println(F("Menu"));if(Xbox.getButtonClick(XBOX)){Serial.println(F("Xbox"));Xbox.disconnect();}if(Xbox.getButtonClick(LB))Serial.println(F("LB"));if(Xbox.getButtonClick(RB))Serial.println(F("RB"));if(Xbox.getButtonClick(LT))Serial.println(F("LT"));if(Xbox.getButtonClick(RT))Serial.println(F("RT"));if(Xbox.getButtonClick(L3))Serial.println(F("L3"));if(Xbox.getButtonClick(R3))Serial.println(F("R3"));if(Xbox.getButtonClick(A))Serial.println(F("A"));if(Xbox.getButtonClick(B))Serial.println(F("B"));if(Xbox.getButtonClick(X))Serial.println(F("X"));if(Xbox.getButtonClick(Y))Serial.println(F("Y"));}}
Users will need to connect the Bluetooth USB module to the USB-C host shield with the USB adapter before running the example. After the example begins, users should see an output in the Serial Monitor with print out based on the user's interaction with their controller.
Bluetooth module connected to the USB-C Host Shield; and paired with an 8BitDo controller.
!! note
Make sure to wait until after the board restarts and executes the example, before pairing the 8BitDo controller with the Bluetooth module.
Bluetooth Pairing the Controller
To turn on the controller, press the Start+X buttons. Users should see two status LEDs blinking at the bottom of the controller. To pair the controller, press and hold the pair button at the top of the controller, next to the USB-C connector, for 3 seconds. Once paired, the controller should vibrate.