SparkFun Ambient Light Sensor - VEML7700  v2.0.0-1-g1693613
Library for the SparkFun Ambient Light Sensor - VEML7700
Loading...
Searching...
No Matches
Deprecated List
Member sfDevVEML7700::getHighThreshold (void)
since version 2.0.0, use highThreshold() instead.
Member sfDevVEML7700::getIntegrationTime (void)
since version 2.0.0, use integrationTime() instead.
Member sfDevVEML7700::getIntegrationTimeStr (void)
since version 2.0.0, use integrationTimeString() instead.
Member sfDevVEML7700::getInterruptStatus (void)
since version 2.0.0, use interruptStatus() instead.
Member sfDevVEML7700::getLowThreshold (void)
since version 2.0.0, use lowThreshold() instead.
Member sfDevVEML7700::getPersistenceProtect (void)
since version 2.0.0, use persistenceProtect() instead.
Member sfDevVEML7700::getPersistenceProtectStr (void)
since version 2.0.0, use persistenceProtect() instead.
Member sfDevVEML7700::getSensitivityMode (void)
since version 2.0.0, use sensitivityMode() instead.
Member sfDevVEML7700::getSensitivityModeStr (void)
since version 2.0.0, use sensitivityModeString() instead.
Class VEML7700
This class is deprecated for version 2.0 of this library. Use SparkFunVEML7700 instead.