SparkFun Ambient Light Sensor - VEML7700  v2.0.0-1-g1693613
Library for the SparkFun Ambient Light Sensor - VEML7700
Loading...
Searching...
No Matches
Class Hierarchy

Go to the graphical class hierarchy

This inheritance list is sorted roughly, but not completely, alphabetically:
[detail level 123]
 CsfDevVEML7700Driver class for the VEML7700 ambient light sensor
 CSparkFunVEML7700Class for interfacing with the VMEL7700 sensor using I2C communication
 CVEML7700Deprecated class for interfacing with the VEML7700 sensor - supports version 1.0.0 of the SparkX library