Installing the Arduino Library

Arduino

This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using the Arduino IDE, library, or board add-on, please review the following tutorials.

Note

If you've never connected an CH340 device to your computer before, you may need to install drivers for the USB-to-serial converter. Check out our section on "How to Install CH340 Drivers" for help with the installation.

SparkFun has written a library to work with the u-blox NEO-F9P. You can obtain this library through the Arduino Library Manager by searching for "SparkFun u-blox GNSS v3". Find the one written by SparkFun Electronics and install the latest version. Users who prefer to manually install the library can get it from the GitHub Repository or download the .ZIP by clicking the button below:

Once you have the library installed checkout the various examples! There are several examples in the library that cover more than just the NEO-F9P. Note that some examples will not apply depending on the modules features. To take advantage of the F9P, we will be looking at the ZED-F9P folder.