![]() |
flux sdk
v01.05.00-6-g190c94c
Embedded C++ SDK
|
This is the complete list of members for _flxDataIn< T >, including all inherited members.
| _flxDataIn() | _flxDataIn< T > | inline |
| addDataLimitValidValue(std::string name, T value) | _flxDataIn< T > | inline |
| addDataLimitValidValue(std::pair< const std::string, T > value) | _flxDataIn< T > | inline |
| addDataLimitValidValue(std::initializer_list< std::pair< const std::string, T > > limitSet) | _flxDataIn< T > | inline |
| clearDataLimit(void) | _flxDataIn< T > | inline |
| dataLimit(void) | _flxDataIn< T > | inline |
| isValueValid(T value) | _flxDataIn< T > | inline |
| set(T const &value)=0 | _flxDataIn< T > | pure virtual |
| set_value(bool v) | flxDataIn | inline |
| set_value(int8_t v) | flxDataIn | inline |
| set_value(int16_t v) | flxDataIn | inline |
| set_value(int32_t v) | flxDataIn | inline |
| set_value(uint8_t v) | flxDataIn | inline |
| set_value(uint16_t v) | flxDataIn | inline |
| set_value(uint32_t v) | flxDataIn | inline |
| set_value(float v) | flxDataIn | inline |
| set_value(double v) | flxDataIn | inline |
| set_value(std::string &v) | flxDataIn | inline |
| setBool(bool value) | _flxDataIn< T > | inlinevirtual |
| setDataLimit(flxDataLimitType< T > &dataLimit) | _flxDataIn< T > | inline |
| setDataLimit(flxDataLimitType< T > *dataLimit) | _flxDataIn< T > | inline |
| setDataLimitRange(T min, T max) | _flxDataIn< T > | inline |
| setDataLimitRange(std::pair< T, T > range) | _flxDataIn< T > | inline |
| setDouble(double value) | _flxDataIn< T > | inlinevirtual |
| setFloat(float value) | _flxDataIn< T > | inlinevirtual |
| setInt16(int16_t value) | _flxDataIn< T > | inlinevirtual |
| setInt32(int32_t value) | _flxDataIn< T > | inlinevirtual |
| setInt8(int8_t value) | _flxDataIn< T > | inlinevirtual |
| setString(std::string &value) | _flxDataIn< T > | inlinevirtual |
| setUInt16(uint16_t value) | _flxDataIn< T > | inlinevirtual |
| setUInt32(uint32_t value) | _flxDataIn< T > | inlinevirtual |
| setUInt8(uint8_t value) | _flxDataIn< T > | inlinevirtual |
| type(void) | _flxDataIn< T > | inlinevirtual |