flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxBusSPI Member List

This is the complete list of members for flxBusSPI, including all inherited members.

begin(bool bInit=false)flxBusSPI
begin(SPIClass &spiPort, SPISettings &spiSettings, bool bInit=false)flxBusSPI
flxBusSPI(void)flxBusSPI
getSPIPort(void)flxBusSPIinline
initialized()flxBusSPIinline
readRegisterRegion(uint8_t cs, uint8_t reg, uint8_t *data, uint16_t numBytes)flxBusSPI
writeRegisterByte(uint8_t cs, uint8_t offset, uint8_t data)flxBusSPI
writeRegisterRegion(uint8_t cs, uint8_t offset, const uint8_t *data, uint16_t length)flxBusSPI