![]() |
flux sdk
v01.05.00-6-g190c94c
Embedded C++ SDK
|
This is the complete list of members for flxDataEditor, including all inherited members.
| beep()=0 | flxDataEditor | pure virtual |
| editField(char *value, size_t lenValue, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |
| editField(std::string &value, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |
| editField(bool &value, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |
| editField(int8_t &value, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |
| editField(int16_t &value, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |
| editField(int32_t &value, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |
| editField(uint8_t &value, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |
| editField(uint16_t &value, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |
| editField(uint32_t &value, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |
| editField(float &value, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |
| editField(double &value, bool hidden=false, uint32_t timeout=60)=0 | flxDataEditor | pure virtual |