![]() |
flux sdk
v01.05.00-6-g190c94c
Embedded C++ SDK
|
This is the complete list of members for flxDataIn, including all inherited members.
| set_value(bool v) | flxDataIn | inline |
| set_value(int8_t v) | flxDataIn | inline |
| set_value(int16_t v) | flxDataIn | inline |
| set_value(int32_t v) | flxDataIn | inline |
| set_value(uint8_t v) | flxDataIn | inline |
| set_value(uint16_t v) | flxDataIn | inline |
| set_value(uint32_t v) | flxDataIn | inline |
| set_value(float v) | flxDataIn | inline |
| set_value(double v) | flxDataIn | inline |
| set_value(std::string &v) | flxDataIn | inline |
| setBool(bool)=0 | flxDataIn | pure virtual |
| setDouble(double)=0 | flxDataIn | pure virtual |
| setFloat(float)=0 | flxDataIn | pure virtual |
| setInt16(int16_t)=0 | flxDataIn | pure virtual |
| setInt32(int32_t)=0 | flxDataIn | pure virtual |
| setInt8(int8_t)=0 | flxDataIn | pure virtual |
| setString(std::string &)=0 | flxDataIn | pure virtual |
| setUInt16(uint16_t)=0 | flxDataIn | pure virtual |
| setUInt32(uint32_t)=0 | flxDataIn | pure virtual |
| setUInt8(uint8_t)=0 | flxDataIn | pure virtual |
| type(void)=0 | flxDataIn | pure virtual |