flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxDataOut Member List

This is the complete list of members for flxDataOut, including all inherited members.

get_value(bool b)flxDataOutinline
get_value(int8_t)flxDataOutinline
get_value(int16_t)flxDataOutinline
get_value(int32_t)flxDataOutinline
get_value(uint8_t)flxDataOutinline
get_value(uint16_t)flxDataOutinline
get_value(uint32_t)flxDataOutinline
get_value(float)flxDataOutinline
get_value(double)flxDataOutinline
get_value(std::string)flxDataOutinline
getBool()=0flxDataOutpure virtual
getDouble()=0flxDataOutpure virtual
getFloat()=0flxDataOutpure virtual
getInt16()=0flxDataOutpure virtual
getInt32()=0flxDataOutpure virtual
getInt8()=0flxDataOutpure virtual
getString()=0flxDataOutpure virtual
getUInt16()=0flxDataOutpure virtual
getUInt32()=0flxDataOutpure virtual
getUInt8()=0flxDataOutpure virtual
type(void)=0flxDataOutpure virtual