![]() |
flux sdk
v01.05.00-6-g190c94c
Embedded C++ SDK
|
This is the complete list of members for flxFormatJSON< BUFFER_SIZE >, including all inherited members.
| _buffer_size | flxFormatJSON< BUFFER_SIZE > | protected |
| _jSection | flxFormatJSON< BUFFER_SIZE > | protected |
| _spDoc | flxFormatJSON< BUFFER_SIZE > | protected |
| add(flxIWriterJSON &newWriter) | flxFormatJSON< BUFFER_SIZE > | inline |
| add(flxIWriterJSON *newWriter) | flxFormatJSON< BUFFER_SIZE > | inline |
| add(flxWriter &newWriter) | flxFormatJSON< BUFFER_SIZE > | inline |
| add(flxWriter *newWriter) | flxFormatJSON< BUFFER_SIZE > | inline |
| beginObservation(const char *szTitle=nullptr) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| beginSection(const char *szName) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| flxOutputFormat::beginSection(const std::string &name) | flxOutputFormat | inlinevirtual |
| bufferSize(void) | flxFormatJSON< BUFFER_SIZE > | inline |
| clearObservation(void) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| endObservation(void) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| endSection() | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| flxFormatJSON() | flxFormatJSON< BUFFER_SIZE > | inline |
| flxOutputFormat() | flxOutputFormat | inline |
| getMaxSizeUsed(void) | flxFormatJSON< BUFFER_SIZE > | inline |
| logValue(const std::string &tag, bool value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, int8_t value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, int16_t value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, int32_t value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, uint8_t value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, uint16_t value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, uint32_t value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, float value, uint16_t precision=3) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, double value, uint16_t precision=3) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, const std::string &value) | flxFormatJSON< BUFFER_SIZE > | inline |
| logValue(const std::string &tag, const char *value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, flxDataArrayBool *value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, flxDataArrayInt8 *value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, flxDataArrayInt16 *value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, flxDataArrayInt32 *value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, flxDataArrayUInt8 *value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, flxDataArrayUInt16 *value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, flxDataArrayUInt32 *value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, flxDataArrayFloat *value, uint16_t precision=3) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, flxDataArrayDouble *value, uint16_t precision=3) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| logValue(const std::string &tag, flxDataArrayString *value) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| flxOutputFormat::logValue(const std::string &tag, std::string &value) | flxOutputFormat | inlinevirtual |
| outputObservation(const char *szBuffer, flxLineType_t type=flxLineTypeData) | flxOutputFormat | inline |
| remove(flxIWriterJSON *oldWriter) | flxFormatJSON< BUFFER_SIZE > | inline |
| remove(flxWriter &oldWriter) | flxFormatJSON< BUFFER_SIZE > | inline |
| remove(flxWriter *oldWriter) | flxFormatJSON< BUFFER_SIZE > | inline |
| reset(void) | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| setBufferSize(size_t new_size) | flxFormatJSON< BUFFER_SIZE > | inline |
| writeObservation() | flxFormatJSON< BUFFER_SIZE > | inlinevirtual |
| writeOutArray(const std::string &tag, flxDataArrayType< T > *theArray) | flxFormatJSON< BUFFER_SIZE > | inlineprotected |
| writeOutArrayDimension(JsonArray &jsonArray, T *&pData, flxDataArrayType< T > *theArray, uint16_t currentDim) | flxFormatJSON< BUFFER_SIZE > | inlineprotected |