flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxKVPStore Member List

This is the complete list of members for flxKVPStore, including all inherited members.

commit(void)flxKVPStoreinline
deleteValue(uint8_t iNS, const char *szKey)flxKVPStore
flxKVPStore()flxKVPStoreinline
getNameSpace(const char *szNS)flxKVPStore
getNameSpaceIndex(const char *szNS, uint8_t &outNSIndex)flxKVPStoreprotected
getValue(uint8_t iNS, const char *szKey, T &value)flxKVPStoreinline
getValue(uint8_t iNS, const char *szKey, char *value, size_t len)flxKVPStoreinline
getValue(uint8_t iNS, const char *szKey, void *value, size_t len)flxKVPStoreinline
initialize(void)flxKVPStore
keyExists(uint8_t iNS, const char *szKey)flxKVPStore
kNullPageflxKVPStorestatic
reset(void)flxKVPStore
setStorageDevice(flxKVPStoreDevice *device)flxKVPStoreinline
setStorageDevice(flxKVPStoreDevice &device)flxKVPStoreinline
setValue(uint8_t iNS, const char *szKey, const char *value)flxKVPStoreinline
setValue(uint8_t iNS, const char *szKey, char *value)flxKVPStoreinline
setValue(uint8_t iNS, const char *szKey, T &value)flxKVPStoreinline
setValue(uint8_t iNS, const char *szKey, const void *value, size_t valueSize)flxKVPStoreinline