![]() |
flux sdk
v01.05.00-6-g190c94c
Embedded C++ SDK
|
This is the complete list of members for flxKVPStoreDevice, including all inherited members.
| close(void)=0 | flxKVPStoreDevice | pure virtual |
| erase(uint32_t iPage)=0 | flxKVPStoreDevice | pure virtual |
| flush(void)=0 | flxKVPStoreDevice | pure virtual |
| read(uint32_t iPage, uint32_t address, void *dest, size_t len)=0 | flxKVPStoreDevice | pure virtual |
| segmentSize()=0 | flxKVPStoreDevice | pure virtual |
| storageSize()=0 | flxKVPStoreDevice | pure virtual |
| write(uint32_t iPage, uint32_t address, const void *src, size_t len)=0 | flxKVPStoreDevice | pure virtual |
| ~flxKVPStoreDevice() | flxKVPStoreDevice | inlinevirtual |