![]() |
flux sdk
v01.05.00-6-g190c94c
Embedded C++ SDK
|
This is the complete list of members for flxSerialField, including all inherited members.
| beep() | flxSerialField | virtual |
| editField(char *value, size_t lenValue, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editField(bool &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editField(std::string &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editField(int8_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editField(int16_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editField(int32_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editField(uint8_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editField(uint16_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editField(uint32_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editField(float &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editField(double &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | inlinevirtual |
| editFieldBool(bool &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldCString(char *value, size_t lenValue, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldDouble(double &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldFloat(float &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldInt(int32_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldInt16(int16_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldInt8(int8_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldString(std::string &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldStringCLI(std::string &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldUInt(uint32_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldUInt16(uint16_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| editFieldUInt8(uint8_t &value, bool hidden=false, uint32_t timeout=60) | flxSerialField | |
| EditReturn_t enum name | flxSerialField | |
| kEditReturnCR enum value | flxSerialField | |
| kEditReturnDownArrow enum value | flxSerialField | |
| kEditReturnEscape enum value | flxSerialField | |
| kEditReturnUpArrow enum value | flxSerialField |