SparkFun IoT Node - LoRaWAN
Firmware and associated Documentation and Firmware for the SparkFun IoT Node - LoRaWAN product
This repository contains the latest firmware for the SparkFun IoT Node - LoRaWAN development board. While the IoT Node - LoRaWAN development board is programmable using Arduino, the IoT Node - LoRa board ships with a firmware application that enables rapid sensor definition and deployment on a Digi LoRaWAN XON network. This repository contains the source for this LoRaWAN application and well as firmware releases.
The IoT Node - LoRaWAN firmware is pre-programmed to automatically log data from 25+ SparkFun Qwiic sensors, all without requiring any hardware setup or code development. Just plug in a qwiic board, and log data to the LoRaWAN network. The IoT Node - LoRaWAN board automatically detects the connected sensor, configures the device and enables logging to the serial console and, if connected, to the Digi LoRaWAN network.
The SparkFun IoT Node - LoRaWAN board and firmware are designed to enable posting data to the LoRaWAN network within minutes, requiring no development or configuration. The SparkFun IoT Node - LoRaWAN board is configured to work with the Dig LoRaWAN network. Once the board is registered with your Digi XON account (via the on-board digital data tag - which is similar to a QR code), the board with this firmware should automatically connect to your Digi LoRaWAN account. Connect a supported qwiic sensor and data is automatically posted to the LoRaWAN network.
The IoT Node - LoRaWAN firmware is highly configurable via an easily to use serial interface. Simply plug in a USB C cable and open a terminal at 115200 Kbps. By default the logging output is automatically streamed to the serial terminal - pressing any key will bring up the menu system.
Latest Firmware
- Version 01.01.00 - Release
NOTE With firmware version v1.1.0 and above, the XBee LR module on the IoT Node - LoRaWAN board must be running firmware version A5013 - (May 1, 2025) or later. Details on the firmware and how to update are located here
Documentation
- Hardware Hookup Guide - Basic hookup guide for the SparkFun IoT Node - LoRaWAN board
- SparkFun IoT Node - LoRaWAN - Hardware Repo for the IoT Node board
Supported Products
- DEV-26060 - SparkFun IoT Node - LoRaWAN
Latest Release
Details on the latest Firmware release are listed on the Release Page