IoT Node - LoRaWAN - Device Settings
The device settings menu of the system presents the property pages for each device connected to the IoT Node - LoRaWAN board.
The contents of the Device Settings page is dynamic and changes based on the devices connected to the board. The following is an example of a device settings listing page:

In this page, the devices MAX17948 and BME280 are listed. Selected an individual device entry will bring up the property page for that device.
Below is the property page for the ***BME280** device:

While the contents of a specific device settings page is dependent on the particular device, each page as a common set of operations.
Parameters
All devices have a set of parameters, as shown in the above device page for the BME280 device.
Parameters can be enabled/disabled, controlling which values are output - logged to the Serial Console and sent to the LoRaWAN.
Each device allows the enabling/disabling of individual parameters, but functions are also provided to enable or disable all parameters with one operation.
When a parameter is disabled, it is highlighted on the devices settings page.
LoRaWAN Sent Values
Not all parameters are sent via the LoRaWAN - only those that make sense for the limitations of the LoRaWAN system. To determine which values are sent, consult the Advanced section of this documentation, or enable verbose messaging and display a devices settings page. The format of this is shown in the settings page of the ENS160 device later on this page.
Properties
If a device as available properties, these are listed on the devices settings page. The following page shows properties and parameter settings for the ENS160 device.

The properties/settings behave just like any other setting within the system. Once set, if a device with the same name/type is loaded, the saved settings are applied at startup.