IoT Node - LoRaWAN - Settings
The following sections provide an overview of the available settings and functions within the settings menu of the IoT Node - LoRaWAN firmware.
The settings system is divided into two sections - Settings and Device Settings as shown in the following image:

Settings - System Settings and Operations
When this entry is selected, the following entries are presented:

Application Settings
The Application Settings menu has the following entries:

Color Output
When enabled (the default), output to the console will use colors to highlight values and functionality. When disabled, all output is plain text. When using a limited serial console application, set this value to false.
Board Name
Set this value any name desired for the particular board. By default this value is empty.
Serial Console Format
This property sets the output format for sensor/log data for the serial console. Available values include CSV, JSON and Disabled. The default value is CSV.
JSON Buffer Size
This is the size - in bytes - the application should use when building JSON formatted output. The default value is 1600 bytes. This value should only be adjusted if logging a large number of values to the serial console.
The maximum bytes used by the JSON system is displayed on the About page of the application (try using !about console command to see this value).
Terminal Baud Rate
Use this value to change the baud rate settings for the serial console. Once changed this value might require a system restart to take effect. The default value is 115200.
Device Names
When enabled (default is disabled), attached devices have their address appended to the name. This is helpful to identify a particular board when two or more of the same board type are attached to the IoT Node board.
Startup Delay
When the IoT Node board starts up, an startup menu is displayed. This settings determines how long to display this menu. Setting this value disables the menu.
The startup menu has the following options:

Pressing the indicted menu key selects that option. If the startup delay expires, a normal startup sequence occurs.
Startup Menu Entries
- 'n' = Normal startup sequence
- 'v' = Verbose output messaging is enabled at startup
- 'a' = Disable qwiic device autoload
- 'l' = List the available qwiic/i2c drivers at startup (this list is deleted after startup)
- 's' = Disable settings restore on startup
Verbose Messages
When enabled, verbose output is enabled. This value is disabled by default.
About...
When selected, the system displays the About page for the application. This reflects the current status of system. This page is also displayed using the !about console command.
LoRaWAN Network
The LoRaWAN Network page has the following settings:

Enabled
Used to enable/disable the LoRaWAN network functionality. This value is enabled by default.
Application EUI
The Application EUI for the LoRaWAN connection
Application Key
The Application Key for the LoRaWAN connection. This value is secret, and while editable, it is not visible when editing.
Network Key
The Network Key for the LoRaWAN connection. This value is secret, and while editable, it is not visible when editing.
LoRaWAN Class
The operating class for the LoRaWAN module. By default this value is set to C.
LoRaWAN Region
The operating region for the LoRaWAN module. By default this value is US915.
Reset
Calls the reset function on the module.
LoRaWAN Logger
This pages has no entires currently.
Logger
The logger system is used to output values to the Serial Console.
The logger has the following settings:

Timestamp Mode
Enables output of a timestamp to the logged information and sets the format of the timestamp. By default this is disabled.
Sample Numbering
If enabled, a sample number is included in the console output of logged data. This value is disabled by default.
Numbering Increment
The amount to increment each sample number when sample numbering is enabled. The default value is 1.
Output ID
When enabled, the board ID is included in the logged output. This value is disabled by default.
Output Name
When enabled, the board Name is included in the logged output. This value is disabled by default.
Rate Metic
When enabled, metrics are recorded for the logging system. This value is disabled by default.
Reset Sample Counter
Resets the data sample number to a user provided value.
Logging Timer
The timer has the following properties:

Interval
The interval for the logging timer. For every interval period, a logging event occurs - sending data to the LoRaWAN and serial console (if enabled). The default value is 90000 ms.
System Control
The System Control page includes the following entries:

Device Restart
When selected, the user is prompted to restart the device/system. This is also available using the !restart console command.
Device Reset
When selected, the user is prompted to reset the device/system. A device reset erases the current saved settings values and restarts the board/system. This is also available using the !reset-device console command.
Time Setup
By default the IOT Node - LoRaWAN is not connected to a timekeeping source and defaults to a start time value of January 1, 1970 (epoch value of 0). But if a time keeping device is added (GNSS or Real Time Clock), this page is used to set time parameters for the board.
The Time Setup property page has the following entries:

Time Zone
The timezone specification string to use for the system clock. By default, the Mountain Time zone (the zone of SparkFun) is used.
Reference Clock
If a reference clock device is connected to the IoT Node board, use this option to select this clock.
Update Interval
Specify how often the system clock is updated using the reference clock in minutes.
Enable Clock Fallback
Adds a secondary reference clock to use if the primary clock becomes unavailable.
Dependant Interval
If a dependant clock is connected (a clock being set by the system clock), this value sets how often the dependant clock device is updated.
Update Connected
If enabled, any connected clocks have their time updated when the system clock is updated.
Save Settings
The Save Settings system is designed to include a "fallback" settings system if available. Normally this might be a JSON file on a SDCard or similar device. At launch, this functionality is not available for the IoT Node - LoRaWAN board.
The Save Settings property page has the following elements:

Fallback Restore
If enabled, restore settings from the fallback system if the primary storage system is unavailable or empty.
Fallback Save
If enabled and a fallback device is available, saving settings to primary storage also saves them to the secondary device.
Buffer Size
The buffer size used for internal I/O operations. This is not used for the IoT Node Board.
Save Settings
When called, the current value of the systems settings is saved to the primary persistent storage system.
Restore Settings
When called, systems settings are restore from the primary storage system.
Clear Settings
When called, the primary (on board) settings storage is erased/reset.
Save to Fallback
If a fallback device is available, when this function is called, system settings are saved to the fallback device.
Restore from Fallback
If a fallback device is available, when this function is called, system settings are restored from the fallback device.