Introduction

SparkFun IoT Node - LoRaWAN
Firmware and associated Documentation and Firmware for the SparkFun IoT Node - LoRaWAN product
This repository contains the latest firmware for the SparkFun IoT Node - LoRaWAN development board. While the IoT Node - LoRaWAN development board is programmable using Arduino, the IoT Node - LoRa board ships with a firmware application that enables rapid sensor definition and deployment on a Digi LoRaWAN XON network. This repository contains the source for this LoRaWAN application and well as firmware releases.
The IoT Node - LoRaWAN firmware is pre-programmed to automatically log data from 25+ SparkFun Qwiic sensors, all without requiring any hardware setup or code development. Just plug in a qwiic board, and log data to the LoRaWAN network. The IoT Node - LoRaWAN board automatically detects the connected sensor, configures the device and enables logging to the serial console and, if connected, to the Digi LoRaWAN network.
The SparkFun IoT Node - LoRaWAN board and firmware are designed to enable posting data to the LoRaWAN network within minutes, requiring no development or configuration. The SparkFun IoT Node - LoRaWAN board is configured to work with the Dig LoRaWAN network. Once the board is registered with your Digi XON account (via the on-board digital data tag - which is similar to a QR code), the board with this firmware should automatically connect to your Digi LoRaWAN account. Connect a supported qwiic sensor and data is automatically posted to the LoRaWAN network.
The IoT Node - LoRaWAN firmware is highly configurable via an easily to use serial interface. Simply plug in a USB C cable and open a terminal at 115200 Kbps. By default the logging output is automatically streamed to the serial terminal - pressing any key will bring up the menu system.
Latest Firmware
- Version 01.01.00 - Release
NOTE With firmware version v1.1.0 and above, the XBee LR module on the IoT Node - LoRaWAN board must be running firmware version A5013 - (May 1, 2025) or later. Details on the firmware and how to update are located here
Documentation
- Hardware Hookup Guide - Basic hookup guide for the SparkFun IoT Node - LoRaWAN board
- SparkFun IoT Node - LoRaWAN - Hardware Repo for the IoT Node board
Supported Products
- DEV-26060 - SparkFun IoT Node - LoRaWAN
Latest Release
Details on the latest Firmware release are listed on the Release Page
Hardware Overview
Hardware Hookup
Arduino Example
Troubleshooting
General Troubleshooting Help
### Not working as expected and need help?
If you need technical assistance and more information on a product that is not working as you expected, we recommend heading on over to the SparkFun Technical Assistance page for some initial troubleshooting.
If you don't find what you need there, the SparkFun Forums are a great place to find and ask for help. If this is your first visit, you'll need to create a forum account to search product forums and post questions.