SparkFun Fingerprint Sensor - FPC2534 Pro  v0.9.9-3-g5d0d172
Library for the SparkFun Fingerprint Sensor - FPC2534 Pro
Loading...
Searching...
No Matches
fpc_cmd_image_request_t Struct Reference

Payload definition of the Image request command. More...

#include <fpc_api.h>

Public Attributes

fpc_cmd_hdr_t cmd
 
uint16_t type
 
uint16_t total_size
 

Detailed Description

Payload definition of the Image request command.

Member Data Documentation

◆ cmd

fpc_cmd_hdr_t fpc_cmd_image_request_t::cmd

Command header.

◆ total_size

uint16_t fpc_cmd_image_request_t::total_size

Size of image. Valid for PUT, set to 0 for GET

◆ type

uint16_t fpc_cmd_image_request_t::type

Image request type. One of CMD_IMAGE_REQUEST_TYPE_*


The documentation for this struct was generated from the following file: