SparkFun Fingerprint Sensor - FPC2534 Pro  v0.9.9-3-g5d0d172
Library for the SparkFun Fingerprint Sensor - FPC2534 Pro
Loading...
Searching...
No Matches
fpc_cmd_navigation_ps_status_event_t Struct Reference

Payload definition of the CMD_NAVIGATION_PS Event. More...

#include <fpc_api.h>

Public Attributes

fpc_cmd_hdr_t cmd
 
int32_t v_impulse
 
int32_t h_impulse
 
uint32_t c_coverage
 
uint16_t gesture
 

Detailed Description

Payload definition of the CMD_NAVIGATION_PS Event.

Member Data Documentation

◆ c_coverage

uint32_t fpc_cmd_navigation_ps_status_event_t::c_coverage

◆ cmd

fpc_cmd_hdr_t fpc_cmd_navigation_ps_status_event_t::cmd

Command header.

◆ gesture

uint16_t fpc_cmd_navigation_ps_status_event_t::gesture

◆ h_impulse

int32_t fpc_cmd_navigation_ps_status_event_t::h_impulse

◆ v_impulse

int32_t fpc_cmd_navigation_ps_status_event_t::v_impulse

The documentation for this struct was generated from the following file: