SparkFun Fingerprint Sensor - FPC2534 Pro  v0.9.9-3-g5d0d172
Library for the SparkFun Fingerprint Sensor - FPC2534 Pro
Loading...
Searching...
No Matches
fpc_cmd_pinctrl_gpio_request_t Struct Reference

Payload definition of the CMD_GPIO_CONTROL Request. More...

#include <fpc_api.h>

Public Attributes

fpc_cmd_hdr_t cmd
 
uint8_t sub_cmd
 
uint8_t pin
 
uint8_t mode
 
uint8_t state
 

Detailed Description

Payload definition of the CMD_GPIO_CONTROL Request.

Member Data Documentation

◆ cmd

fpc_cmd_hdr_t fpc_cmd_pinctrl_gpio_request_t::cmd

Command header.

◆ mode

uint8_t fpc_cmd_pinctrl_gpio_request_t::mode

Gpio mode. One of GPIO_CONTROL_MODE...

◆ pin

uint8_t fpc_cmd_pinctrl_gpio_request_t::pin

Gpio pin (according to product spec).

◆ state

uint8_t fpc_cmd_pinctrl_gpio_request_t::state

Gpio state. One of GPIO_CONTROL_STATE...

◆ sub_cmd

uint8_t fpc_cmd_pinctrl_gpio_request_t::sub_cmd

Sub command. One of GPIO_CONTROL_SUB_CMD...


The documentation for this struct was generated from the following file: