![]() |
SparkFun Fingerprint Sensor - FPC2534 Pro
v0.9.9-3-g5d0d172
Library for the SparkFun Fingerprint Sensor - FPC2534 Pro
|
Frame Header. More...
#include <fpc_api.h>
Public Attributes | |
| uint16_t | version |
| uint16_t | type |
| uint16_t | flags |
| uint16_t | payload_size |
Frame Header.
| uint16_t fpc_frame_hdr_t::flags |
Frame flags. A selection of FPC_FRAME_FLAG_*.
| uint16_t fpc_frame_hdr_t::payload_size |
Size of the following payload.
| uint16_t fpc_frame_hdr_t::type |
Type of frame. One of FPC_FRAME_TYPE_*.
| uint16_t fpc_frame_hdr_t::version |
Protocol version