SparkFun Fingerprint Sensor - FPC2534 Pro  v0.9.9-3-g5d0d172
Library for the SparkFun Fingerprint Sensor - FPC2534 Pro
Loading...
Searching...
No Matches
fpc_id_type_t Struct Reference

Template ID specifier payload. More...

#include <fpc_api.h>

Public Attributes

uint16_t type
 
uint16_t id
 

Detailed Description

Template ID specifier payload.

Member Data Documentation

◆ id

uint16_t fpc_id_type_t::id

Template ID, only valid when type=ID_TYPE_SPECIFIED.

◆ type

uint16_t fpc_id_type_t::type

Type of Specifier. One of ID_TYPE_*.


The documentation for this struct was generated from the following file: