qwiic_soil_moisture_sensor
Python module for the SparkFun Qwiic Soil Moisture Sensor
This python package is a port of the existing SparkFun Soil Moisture Sensor Arduino Examples
This package can be used in conjunction with the overall SparkFun qwiic Python Package
New to qwiic? Take a look at the entire SparkFun qwiic ecosystem.
◆ COMMAND_CHANGE_ADDRESS
| int qwiic_soil_moisture_sensor.COMMAND_CHANGE_ADDRESS = 0x03 |
◆ COMMAND_GET_VALUE
| int qwiic_soil_moisture_sensor.COMMAND_GET_VALUE = 0x05 |
◆ COMMAND_LED_OFF
| int qwiic_soil_moisture_sensor.COMMAND_LED_OFF = 0x00 |
◆ COMMAND_LED_ON
| int qwiic_soil_moisture_sensor.COMMAND_LED_ON = 0x01 |
◆ COMMAND_NOTHING_NEW
| int qwiic_soil_moisture_sensor.COMMAND_NOTHING_NEW = 0x99 |
◆ SENSOR_STATUS
| int qwiic_soil_moisture_sensor.SENSOR_STATUS = 0x3F |
◆ SOIL_MOISTURE_SENSOR_DEFAULT_ADDRESS
| int qwiic_soil_moisture_sensor.SOIL_MOISTURE_SENSOR_DEFAULT_ADDRESS = 0x28 |