Hardware Overview
Important: Read Before Use!
ESD Sensitivity
The mosaic-X5 module is sensitive to ESD. Use a proper grounding system to make sure that the working surface and the components are at the same electric potential.
ESD Precaution
As recommended by the manufacturer, we highly recommend that users take the necessary precautions to avoid damaging their module.
- The Tri-band GNSS RTK breakout board features ESD protection on the USB-C connector and breakout's I/O:
- USB data lines
- I/O PTH pads
- JST connector's pins
- The mosaic-X5 module features internal ESD protection to the
ANT_1antenna input.
Active Antenna
Never inject an external DC voltage into the SMA connector for the GPS antenna, as it may damage the mosaic-X5 module. For instance, when using a splitter to distribute the antenna signal to several GNSS receivers, make sure that no more than one output of the splitter passes DC. Use DC-blocks otherwise.
Info
A 3 - 5.5V DC voltage can be applied to the main antenna from the VANT pin, obviating the need for an external antenna supply or bias-tee.
Board Dimensions
The board dimensions are illustrated in the drawing below; the listed measurements are in inches.
Board dimensions (PDF) for the Tri-band GNSS RTK breakout board, in inches.
Need more measurements?
For more information about the board's dimensions, users can download the eagle files for the board. These files can be opened in Eagle and additional measurements can be made with the dimensions tool.
Eagle - Free Download!
Eagle is a CAD program for electronics that is free to use for hobbyists and students. However, it does require an account registration to utilize the software.
Dimensions Tool
This video from Autodesk demonstrates how to utilize the dimensions tool in Eagle, to include additional measurements:
USB-C Connector
The USB connector is provided to power and interface with the mosaic-X5 GNSS receiver. For most users, it will be the primary method for communicating with the mosaic-X5 module.
USB-C connector on the Tri-band GNSS RTK breakout board.
Power
The Tri-band GNSS RTK breakout board only requires 5V to power all of the board's components. The simplest method to power the board is through the USB-C connector. Alternatively, the board can be converted to utilize 3.3V for low power applications.
Tri-band GNSS RTK breakout board's power connections.
Below, is a general summary of the power circuitry on the board, broken out as PTH pins:
VUSB- The voltage from the USB-C connector, usually 5V.- Input Voltage Range: 4.4 - 5.5 V
- Power source for the entire board.
- Powers the 3.3V voltage regulator (AP2112) and the active antenna preamplifier for the mosaic-X5 module. (1)
- This pin powers the integrated PHY of the mosaic-X5 module's USB interface.
- Features ESD protection and a thermal fuse.
VIN- Alternate input supply voltage for the board.- Alternative power supply input for the board, excluding the integrated PHY of the USB interface.
- Power source for the entire board.
- Powers the 3.3V voltage regulator (AP2112) and the active antenna preamplifier for the mosaic-X5 module. (2)
- Features a thermal fuse.
3.3V- Provides a regulated 3.3V from AP2112 using the power from theVINorVUSB(5V) inputs.- Input Voltage Range: 3.135 - 3.465 V
- The 3.3V AP2112 LDO regulator can source up to 600mA.
V_BATT- Always-on power supply- Input Voltage Range: 3.135 - 3.465 V
- Tied to
3.3V(see the Jumpers section).- Used to power the module in Standby mode.
GND- The common ground or the 0V reference for the voltage supplies.
-
-
While the AP2112 LDO regulator has an input voltage range of 2.5 - 6V, users should supply:
- A minimum of 3.5V for a 3.3V output from the regulator
- A maximum of 5.5V as not to exceed the electrical limitations of the mosaic-X5 module
-
A 3 - 5.5V DC voltage can be applied to the main antenna from the
VANTpin, obviating the need for an external antenna supply or bias-tee.
-
-
A 3 - 5.5V DC voltage can be applied to the main antenna from the
VANTpin, obviating the need for an external antenna supply or bias-tee.
VIN Input Voltage
While the AP2112 LDO regulator has an input voltage range of 2.5 - 6V, users should supply:
- A minimum of 3.5V for a 3.3V output from the regulator
- A maximum of 5.5V as not to exceed the electrical limitations of the mosaic-X5 module
However, users are able to bypass the electrical limitations of the mosaic-X5 module and power the board with up to 6V. Users just need to modify the ANT_V jumper (see the Jumpers section) to the 3V3 pad.
MEAS Pins
These pins can be used to measure the current being drawn through the USB connector or VUSB/VIN pins (see the Jumpers section).
JST Connector
The V pin of the JST connector is designed for an input voltage to VIN. By default, it does not operate as a voltage output.
Bypass - Reverse Current Protection Diode
Danger - Proceed at Your Own Risk!
By bypassing the reverse current protection diode, users should take precautions to ensure that they do not provide an input voltage to the JST connector, when the board is connected to their computer. Otherwise, it may result in damage to the computer's USB bus.
To enable an output voltage on the JST connector, users will need to bypass the protection diode that prevents reverse current to the USB-C connector. This can be done by jumping the VUSB and VIN pins together.
Once jumpered, when the board is powered through the USB-C connector, the V pin of the JST connector will provide an output voltage from the USB-C connector.
Info
For more details, users can reference the schematic and the datasheets of the individual components on the board.
Power Modes
The mosaic-X5 module operates in three different power states.
- Off - The module is completely turned off
- When transitioning to the Off state from Active, recent data may not be lost and not logged to the external SD card
- Standby - The module is in a low-power consumption mode (1)
- The module power consumption in standby is <5mW
- The
PMIC_ON_REQpin is drivenLOW - The
MODULE_RDYpin is in aLOW - Monitors the state of the
ONOFFpin (Not available)
- Active - The module is operating with all functions active
- On power up, the module restarts in the configuration stored in the boot configuration file
- The
PMIC_ON_REQpin is drivenHIGH - The
MODULE_RDYpin is in aHIGH(2)
- Essentially, the same state as Off; except in the transition to the Standby mode, before the module shuts down:
- All logging tasks are terminated
- The SD card is unmounted
- The
PMIC_ON_REQpin is drivenLOW
- Level becomes
HIGHabout 300ms after powering up, reset, or waking up from standby
Info
By default, the board is hardwired to operate only in the Active and Off modes.
For more information on the power management of the mosaic-X5 module, please refer to sections 3.4, 3.5, 4.1, and 4.13 of the hardware manual.
Enabling Standby Mode
Users can enable Standby mode on the mosaic-X5, by modifying the V_BATT jumper (see the Jumpers section) and providing an external power source for the V_BATT pin (3.3V). However, because the ONOFF pin isn't exposed users will need to power cycle the board to return to the Active state.
Drive Current - PMIC_ON_REQ/MODULE_RDY
The drive current on the PMIC_ON_REQ and MODULE_RDY pins is low. Enough to be read by a digital pin on a microcontroller, but not high enough to drive an LED.
Power Consumption
The power consumption of the mosaic-X5 module depends on the GNSS signals enabled and the positioning mode. The table below, lists the average power consumption for common configurations. The current listed, is based on a supply voltage of 3.3V.
| GNSS Signals | Positioning Mode | Power (mW) | Current (mA) |
|---|---|---|---|
| GPS L1 C/A | Stand-Alone (1Hz) | 550 | 167 |
| GPS L1/L2 | RTK (1Hz) | 670 | 203 |
| GPS/GLONASS L1/L2 | RTK (1Hz) | 695 | 211 |
| GPS/GLONASS L1/L2+GALILEO L1/E5a +BeiDou B1C/B2a | RTK (1Hz) | 850 | 258 |
| GPS/GLONASS L1/L2+GALILEO L1/E5a +BeiDou B1C/B2a | RTK (100 Hz) | 930 | 282 |
| GPS/GLONASS L1/L2 + L-band | PPP (1Hz) | 760 | 230 |
| All signals from all GNSS constellations | Static (1Hz) | 910 | 276 |
| All signals from all GNSS constellations +L-band | Static(1Hz) | 980 | 297 |
| All signals from all GNSS constellations +L-band | Static (100Hz) | 1080 | 327 |
Source: mosaic-X5 Hardware Manual
mosaic-X5
The centerpiece of the Tri-band GNSS RTK breakout board, is the mosaic-X5 module from Septentrio. Their mosaic modules are low-power, multi-band, multi-constellation GNSS receivers capable of delivering centimeter-level precision at high update rates. The modules also feature Septentrio's unique AIM+ technology for interference mitigation and anti-spoofing, which ensures their best-in-class reliability and scalable position accuracy.
Features:
- Operating Voltage: 3.135 - 3.465V
- Operating Temperature: -40 - 85°C
- GNSS Support
- GPS: L1C/A, L1PY, L2C, L2P, L5
- GLONASS: L1CA, L2CA, L2P, L3 CDMA
- Beidou: B1I, B1C, B2a, B2b, B2I, B3
- Galileo: E1, E5a, E5b, E5 AltBoc, E6
- QZSS: L1C/A, L1 C/B, L2C, L5
- Navic: L5
- SBAS: Egnos, WA
- Antenna Specifications
- Preamplification Range: 15-50dB
- Bias Voltage: 3.0 - 5.5V
- 448 Hardware Channels
- Update Rate: 100Hz
- Latency: < 10ms
- Time to Fix
- Cold Start: < 45s
- Warm: < 20s
- Reacquisition: 1s
- Timing Precision: 5ns
-
Position Accuracy
Correction Horizontal Vertical RTK 0.6cm (±0.5ppm)
~0.25"1cm (±1ppm)
~.4"DGNSS 40cm
~1.3'70cm
~2.3'SBAS 60cm
~2'80cm
~2.6'Standalone 1.2m
~4'1.9m
~6.2'
Info
The mosaic-X5 has three power modes: Active, Standby, and Off (see the Power Modes section).
Frequency Bands
The mosaic modules are multi-band, multi-constellation GNSS receivers. Below, are charts illustrating the frequency bands utilized by all the global navigation satellite systems and the ones supported by the mosaic-X5 module.
The frequency bands supported by the mosaic-X5 GNSS receiver.
Frequency bands of the global navigation satellite systems. (Source: Tallysman)
Info
For a comparison of the frequency bands supported by the mosaic modules, refer to section 3.1 of the hardware manual.
What are Frequency Bands?
A frequency band is a section of the electromagnetic spectrum, usually denoted by the range of its upper and lower limits. In the radio spectrum, these frequency bands are usually regulated by region, often through a government entity. This regulation prevents the interference of RF communication; and often includes major penalties for any interference with critical infrastructure systems and emergency services.
However, if the various GNSS constellations share similar frequency bands, then how do they avoid interfering with one another? Without going too far into detail, the image above illustrates the frequency bands of each system with a few characteristics specific to their signals. Wit these characteristics in mind, along with other factors, the chart can help users to visualize how multiple GNSS constellations might co-exist with each other.
For more information, users may find these articles of interest:
Position Accuracy
The accuracy of the position reported from the mosaic-X5 module, can be improved based upon the correction method being employed. Currently, RTK corrections provide the highest level of accuracy; however, users should be aware of certain limitations of the system:
- RTK technique requires real-time correction data from a reference station or network of base stations.
- RTK corrections are signal specific (i.e. an RTK network might provide corrections on only
E5band notE5a).
- RTK corrections are signal specific (i.e. an RTK network might provide corrections on only
- The range of the base stations will vary based upon the RTK method being employed.
- The reliability of RTK corrections are inherently reduced in multipath environments. However, with Septentrio's multipath mitigation technology (APME+) on the mosaic-X5, these errors are significantly reduced when compared to multipath mitigation techniques that modify the correlators in the tracking channels.
RTK Corrections
To understand how RTK works, users will need a more fundamental understanding of the signal error sources.
Tip
For the best performance, we highly recommend that users configure the module to utilize/provide RTK corrections with a compatible L1/L2/L5 (tri-band) GNSS antenna and utilize a low-loss cable.
Peripherals and I/O Pins
The mosaic-X5 features several peripherals and I/O pins. Some of these are broken out as pins on the Tri-band GNSS RTK breakout board; whereas, others are broken out to their specific interface (i.e. µSD Carsd slot, USB connector, etc.). Additionally, some of their connections are tied to other components on the board.
Interfaces:
- 4x UART (LVTTL, up to 4 Mbps)
Ethernet (RMII/MDIO), 10/100 Mbps(1)- USB device (2.0, HS)
- SDIO (mass storage)
- 2x GPIO user programmable
- 2x Event markers
- 1x Configurable PPS out
- Not available on the Tri-band GNSS RTK breakout board.
For most users, this will be the primary interface for the mosaic-X5 module.
- When a module is initially connected to a computer, the board will initialize as a USB mass storage device.
- For Windows PCs, the USB driver (1) can be installed from the mass storage device or the RxTools software suite.
- When the SD card is mounted, this drive will contain the contents of the SD card that is inserted on the board.
- Once the USB driver is installed:
- Two virtual
COMports are emulated, which can be used as standardCOMports to access the receiver. - This interface will support Ethernet-over-USB.
- By default, the receiver is not allowed to access the Internet over USB.
- The IP address allocated to the Ethernet-over-USB interface is
192.168.3.1.- The IP address cannot be changed; therefore, only single receiver should be connected to your computer at a time.
- Two virtual
- On Linux, the standard Linux CDC-ACM driver is suitable.
The mosaic-X5 has four UARTs that are organized into separate COM ports. The operation for each of these ports can be configured separately.
COM ports on the Tri-band GNSS RTK breakout board.
COMports 1-3 feature flow control pins, which are disabled by default.COM3is available through the JST connector(1), but the pins can also be accessed from the pads on the bottom of the board.- These ports also support a point-to-point protocol server, by which it can accept TCP/IP connections over a serial link.
Info
By default, the COM ports will be configured with the following settings:
- Baudrate: 115200bps
- Data Bits: 8
- Parity: No
- Stop Bits: 1
- Flow Control: None
Pin Connections
When connecting to the board's UART pins, the pins should be connected based upon the flow of their data. For example, when utilizing the Telemetry Radio or the LoRaSerial Kit:
Users will need to connect a compatible GPS antenna to the L1/2/5 ActiveAnt SMA connector. The type of antenna used with the mosaic-X5 module affects the overall accuracy of the positions calculated by the GNSS receiver.
- An active antenna often features a LNA. This allows the module to boost the signal received by the GNSS module without degrading the SNR.
- The more bands an antenna supports, the greater the performance.
- Faster acquisition time.
- Access and support for the
L5GPS band can potentially mitigate multi-path errors. - Supporting more frequency bands, allows a GNSS receiver to be less susceptible to jamming and spoofing.
Tip
For the best performance, we recommend users choose a compatible L1/L2/L5 (tri-band) GNSS antenna and utilize a low-loss cable.
There are some key parameters related to an antenna that can make or break the signal reception from the satellites. These include the operation frequency, gain, polarization, efficiency and overall loss.
Info
The VANT pin provides external power for an active antenna. By default, this supply voltage is configured at 5V (see the Jumpers section).
Danger
Never inject an external DC voltage into the SMA connector for the GPS antenna, as it may damage the mosaic-X5 module. For instance, when using a splitter to distribute the antenna signal to several GNSS receivers, make sure that no more than one output of the splitter passes DC. Use DC-blocks otherwise.
From the module, the PPS output signal's logic-level is 1.8V. However, for the convenience of users, we have added a buffer and bumped up the signal's logic-level to 3.3V on the Tri-band GNSS RTK breakout. This 3.3V signal output can be access through the SMA connector and the PPS pin. The signal is also connected to the PPS LED, to be used as a visual indicator.
PPS signal's outputs on the Tri-band GNSS RTK breakout board.
Jumpers
See the Jumpers section for more details.
- There is a jumper attached to the
PPSpin. When cut, it disconnects the pin from the PPS signal. - There is a jumper attaches to the
PPSLED. For low power applications, the jumper can be cut to disable thePPSLED.
Use Case
- Users could use this signal in conjunction with the event pins to synchronize two mosaic-X5 modules with each other.
- Users could use this signal to create their own Stratum 0 source for the NTP on a primary time server.
The data logging functionality of the board can be configured through the software/web interfaces or through the use of the LOG button or LOG pin (1). Data logging activity will be indicated by the LOG status LED (2).
- The LOG button and
LOGpin are connected to the same active-high, input of the mosaic-X5. Pressing the button or pulling the pin low will toggle the data logging feature. Whereas, holding them for more than 5 seconds will mount/unmount the SD card (see the Log Button section). - See the SD Card Slot section
The mosaic-X5 module features two general purpose, output LED pins. These pins have a maximum output current of 10 mA and output impedance of 20Ω. In addition, to these pins, there are several status LEDs on the board (see the Status LEDs section).
- The general purpose LED pins are connected to the
RTKandPVTLEDs; and respectively, theRTKandGP_LEDpins. - The PPS output signal is connected to the
PPSpin,PPSLED, andTimePulseSMA connector. - The
LOG_Lpin is connected to theLOGLED.
Info
See the Status LEDs section.
The mosaic-X5 module features two general purpose, output pins. These pins can drive a maximum current of 10mA.
The mosaic-X5 module features two general purpose, event input pins. These pins can be used to time tag external events with a time resolution of 20ns.
Tip
For example, these pins can be used in conjunction with the PPS output signal for time syncing.
The state of PMIC pin indicates when the subsystems are energized and ready (see the Power Modes section). It can be used as a power switch to drive external power to the antenna (VANT) (see the Jumpers section).
The RDY pin indicates the operational mode of the mosaic-X5 module (see the Power Modes section). The level is high when module is operating, and low when in standby or reset.
SMA Connectors
There are two SMA connectors on the Tri-band GNSS RTK breakout board.
The TimePulse connector provides a PPS output signal (see the PPS Output section).
JST Connector
The Tri-band GNSS RTK breakout features a 6-pin JST GH connector, which is polarized and locking. Users can access the COM3 port of the mosaic-X5 module, through the JST connector with our breadboard cable(1).
The JST connector on the Tri-band GNSS RTK breakout board.
The pin connections of the JST connector on the Tri-band GNSS RTK breakout board.
Pin Connections
When connecting to the board's UART pins, the pins should be connected based upon the flow of their data. For example, when utilizing the Telemetry Radio or the LoRaSerial Kit:
V Pin
By default, the power pin (i.e. V or Pin 1) of the JST connector is connected to VIN and configured as a power input. The board can be modified to configure that pin as a power output; however, the modification would bypass some of the safety features of the board (see the Power section).
SD Card Slot
The µSD card slot allows users easily log and store data on the board.
The µSD card slot on the Tri-band GNSS RTK breakout board.
Initial Configuration
Before data logging can occur, it is necessary to create a logging stream from the Logging tab of the web interface or using the RxTools software suite. Streams can contain NMEA or SBF (Septentrio Binary Format) data; SBF can contain RTCM and/or RINEX. (see the Data Logging section)
SD Card Specifications
The mosaic-X5 module is only compatible with SD cards of up to 32GB, formatted with a FAT32 file system.
Standby Mode
When Standby mode is initialized, the module terminates all running processes and unmounts the external SD card to avoid any log file corruption (see the Power Modes section).
LOG Button
Data logging can be controlled with the LOG button (see the Log Button section).
- Pressing the LOG button (< 5s) toggles data logging to the SD card on and off.
- Holding the LOG button for more than 5 seconds (> 5s) and then releasing it, will force the board to:
- Unmount the SD card if it was mounted
- Mount the SD card if it was unmounted
LOG Status LED
The SD card mount status is indicated on the LOG LED andLOG_L pin (see the Status LEDs section).
| LED | Pin | Status |
|---|---|---|
| Off | Low | SD card not present or unmounted |
| On | High | SD card present and mounted |
| Blinking | Pulses | Data logging activity |
Status LEDs
There are five status LEDs on the TMC6300 motor driver:
PWR- Power (Red)- Turns on once power is supplied through the USB-C connector or
VINconnections
- Turns on once power is supplied through the USB-C connector or
PPS- Pulse-Per-Second (Yellow)- Indicates when there is a pulse-per-second signal (see the PPS Output section)
LOG- Data Logging (Green)- Indicates data logging activity (see the SD Card Slot section)
- Off - SD card not present or unmounted
- On - SD card present and mounted
- Blinking - Data logging activity
- Indicates data logging activity (see the SD Card Slot section)
PVT- Position/Velocity/Time Solution (Blue)- Turns on when a PVT solution is available
RTK- RTK Mode (White)- Controlled through
GPIO 02
- Controlled through
The status indicator LEDs on the Tri-band GNSS RTK breakout board.
Buttons
There are two buttons on Tri-band GNSS RTK breakout board: RST and LOG buttons.
Buttons on the Tri-band GNSS RTK breakout board.
Reset Button
The RST (reset) button allows users to reset the mosaic-X5 module without unplugging the board.
RST button on the Tri-band GNSS RTK breakout board.
Log Button
The LOG button allows users easily control the data logging feature and the µSD card, without having to configure the module.
- Pressing the LOG button (< 5s) toggles data logging to the SD card on and off.
- Holding the LOG button for more than 5 seconds (> 5s) and then releasing it, will force the board to:
- Unmount the SD card if it was mounted
- Mount the SD card if it was unmounted
SD Card Status
The SD card mount status is indicated on the LOG LED andLOG_L pin (see the Status LEDs section).
| LED | Pin | Status |
|---|---|---|
| Off | Low | SD card not present or unmounted |
| On | High | SD card present and mounted |
| Blinking | Pulses | Data logging activity |
The LOG button on the Tri-band GNSS RTK breakout board.
Jumpers
Never modified a jumper before?
Check out our Jumper Pads and PCB Traces tutorial for a quick introduction!
There are nine jumpers on the back of the board that can be used to easily modify the hardware connections on the board.
The jumpers on the back of the Tri-band GNSS RTK breakout board.
MEAS-
This jumper can be cut and used to measure the current consumption of the board from the
VUSBand/orVINpower supply inputs. V_BATT-
This jumper can be cut to disconnect the
VBATTpin from the 3.3V output of the AP2112 LDO regulator.Info
The
VBATTpin is the power input for the mosaic-X5 module, when it is in Standby mode. Therefore, it also determines the power state of the mosaic-X5 module, when power is disconnected from theVUSBandVINinputs.- By default, the jumper connected and the
VBATTpin is powered at 3.3V. When the primary power is disconnected, the mosaic-X5 module will enter Standby mode. - If cut, the
VBATTpin will be disconnected from the 3.3V output of the AP2112 LDO regulator. When the primary power is disconnected theVUSBandVINinputs, the mosaic-X5 module will shut off.
- By default, the jumper connected and the
ANT_V-
This jumper can be modified to control the output voltage of the active antenna connection.
Info
By default, the middle pad is connected to the
5Vpad, which draws power from theVUSBand/orVINinputs.Users can modify the jumper, to configure the output voltage of the active antenna connection to 3.3V, by cutting the jumper and connecting the middle pad to the
3V3pad.
There are five jumpers that control power to the status LEDs on the board.
Info
By default, all the jumpers are connected, to power the status LEDs. For low power applications, users can cut the jumpers to disconnect power from each of the LEDs.
PWR_LED- This jumper can be cut to remove power from the red, power LED.PPS_LED- This jumper can be cut to remove power from the yellow LED, which is connected to the PPS signal.LOG_LED- This jumper can be cut to remove power from the green LED, which indicates if data is being logged to the SD card.GP_LED- This jumper can be cut to remove power from the blue LED that is connected to the general purpose pins.RTK_LED- This jumper can be cut to remove power from the white LED, indicating RTK corrections.