Skip to content

Introduction

  • IoT Brushless Motor Driver
    SKU: ROB-22132


    Product Thumbnail

    QR code to play video

  • The SparkFun IoT Brushless Motor Driver is an all-in-one development platform. It includes all the components to create a simple IoT device or learn about control systems. On the boaard, users will find an ESP32 microcontroller, a TMC6300 motor driver, a gimbal motor, a TMAG5273 hall-effect sensor, three INA240A1 inline current sensors, an MCP6021T low-side current sensor, two user buttons, a Qwiic connector, a 3-pin JST connector (for the gimbal motor), and a WS2812 RGB LED.

    The TMC6300 from ADI + Trinamic is a powerful and easy-to-use three-phase motor driver with up to 2A (1.4ARMS) of total drive current. Separate high-side and low-side control of the three half-bridges allows for incredible control of each phase of the motor commutation. We've found the Arduino Simple Field Oriented Control library to work well with the TMC6300 motor driver.

    However, a field-oriented control (FOC) algorithm requires some feedback to close and optimize the control loop. Therefore, we integrated a TMAG5273 hall-effect sensor and INA240A1 current sensor amplifiers (both manufactured by Texas Instruments) into the design of the IoT motor driver board. This allows users to incorporate a position sensor and current sensing into the FOC algorithm or any feedback control loop they choose to implement.

    QR code to product page   Purchase from SparkFun

 Required Materials

To get started, users will need a few items. Now some users may already have a few of these items, feel free to modify your cart accordingly.

  • Computer with an operating system (OS) that is compatible with all the software installation requirements.
  • USB 3.1 Cable A to C - 3 Foot - Used to interface with the IoT Brushless Motor Driver (1)

    1. If your computer doesn't have a USB-A slot, then choose an appropriate cable or adapter.
  • SparkFun IoT Brushless Motor Driver (ESP32 WROOM, TMC6300) (1)

    1. The included gimbal motor requires a 6 to 8V power supply. However, for zero-load, low-speed testing, we have found the power from the USB connection to be sufficient.
Jumper Modification

To modify the jumper, users will need soldering equipment and/or a hobby knife.

New to jumper pads?

Check out our Jumper Pads and PCB Traces Tutorial for a quick introduction!

 Suggested Reading

As a more sophisticated product, we will skip over the more fundamental tutorials (i.e. Ohm's Law and What is Electricity?). However, below are a few tutorials that may help users familiarize themselves with various aspects of the board.

Need to control a different type of motor?

This tutorial is primarily focused on utilizing the TMC6300 motor driver to control a 3-phase brushless DC (BLDC) motor. We would recommend users explore other products for these specific motors and actuators. Below, are additional product tutorials and resources for our other actuator and motor types:

Hardware Overview

Board Dimensions

The board dimensions are illustrated in the drawing below; the listed measurements are in inches.

Board Dimensions

Board dimensions (PDF) for the IoT Motor Driver board, in inches.

Need more measurements?

For more information about the board's dimensions, users can download the eagle files for the board. These files can be opened in Eagle and additional measurements can be made with the dimensions tool.

Eagle - Free Download!

Eagle is a CAD program for electronics that is free to use for hobbyists and students. However, it does require an account registration to utilize the software.

Download from
Autodesk primary logo

📏 Dimensions Tool

This video from Autodesk demonstrates how to utilize the dimensions tool in Eagle, to include additional measurements:

QR code to play video

USB-C Connector

The USB connector is provided to power and program the board. For most users, it will be the primary programming interface for the ESP32 module on the IoT Motor Driver board.

USB-C Connector

USB-C connector on the IoT Motor Driver board.

Power

The IoT Motor Driver only requires 5V to power all of the board's components. The simplest method to power the board is through the USB-C connector. Alternatively, the 3V3 pin can be used to supply power to any of the components, except the motor driver.

Power connections

IoT Motor Driver power connections.

Below, is a general summary of the power circuitry on the board:

  • 3V3 - Provides a regulated 3.3V from the USB (5V) power to the board, excluding the TMC6300 motor driver.
    • Used to power the ESP32-WROOM module, hall-effect and current sensors, CH340C Serial-to-UART bridge, Qwiic connector, and the WS2812 RGB LED.
    • The 3.3V AP2112 LDO regulator can source up to 600mA.
    • Broken out as PTH pin.
  • 3V3_A - Provides a regulated 3.3V from the USB (5V) power to only the TMC6300 motor driver.
    • The motor driver will not function without power from the USB connector.
    • The 3.3V AP63357 LDO regulator can source up to 3.5A.
  • VUSB - The voltage from the USB-C connector, usually 5V.
    • Power source for the entire board.
      • Powers the two 3.3V voltage regulators (AP2112 and AP63357).
    • Features reverse current protection and a thermal fuse.
    • MEAS - These pins can be used to measure the current being drawn through the USB connector (see the Jumpers section).
  • GND - The common ground or the 0V reference for the voltage supplies.
  • Qwiic Connector - Provides a regulated 3.3V voltage to the Qwiic devices.

Info

For more details, users can reference the schematic and the datasheets of the individual components on the board.

Motor Voltage

The Gimbal Stabilizer Motor has an operating voltage range of 6 - 8V. However, we have found that it still functions properly with only 3.3V provided by the IoT Motor Driver board.

CH340 Serial-to-UART

The CH340 allows the ESP32-WROOM to communicate with a computer/host device through the board's USB-C connection. This allows the board to show up as a device on the serial (or COM) port of the computer. Users will need to install the latest drivers for the computer to recognize the board (see Software Overview section).

 Microcontroller - ESP32-WROOM

The brains of the IoT Motor Driver, is an ESP32-WROOM module with 16MB of flash memory. Espressif's ESP32-WROOM module is a versatile, WiFi+BT+BLE MCU module that targets a wide variety of applications. At the core of this module is the ESP32-D0WDQ6 system on a chip (SoC) which is designed to be both scalable and adaptive microcontroller. Its laundry list of features include:

  • Features:

    • Xtensa® Dual-Core 32-bit LX6 Microprocessor (up to 240MHz)
      • 448KB ROM and 520KB SRAM
      • 16MB of Embedded SPI Flash Storage
    • Cryptographic Hardware Accelerators
      • AES, SHA2, ECC, RSA-4096
    • Integrated 802.11 b/g/n WiFi 2.4GHz Transceiver (up to 150Mbps)
    • Integrated dual-mode Bluetooth (Bluetooth v4.2 and BLE)
    • 26 GPIO (including strapping pins)
      • 8x Capacitive Touch Electrodes
    • Operating Voltage: 3.0 to 3.6V
      • WiFi: 380mA (peak)
      • Light-Sleep: 800µA
      • Deep-Sleep: 10 - 150µA
  • ESP32-WROOM
    ESP32-WROOM module on the IoT Motor Driver.

Warning

Users should be aware of the following nuances and details of this board

  • The ESP32-WROOM is only compatible with 2.4GHz WiFi networks; it will not work on the 5GHz bands.
  • For details on the boot mode configuration, please refer to section 3.3 Strapping Pins of the ESP32-WROOM module datasheet.

Info

The ESP32-WROOM module has various power modes:

  • Active - The chip radio is powered on. The chip can receive, transmit, or listen.
  • Modem Sleep - The CPU is operational and the clock is configurable. The Wi-Fi/Bluetooth baseband and radio are disabled.
  • Light Sleep - The CPU is paused. The RTC memory and RTC peripherals, as well as the ULP coprocessor are running.
  • Deep Sleep - Only the RTC memory and RTC peripherals are powered on. The ULP coprocessor is functional.
  • Hibernation - Only one RTC timer on the slow clock and certain RTC GPIOs are active.
  • Off - Chip is powered off

For more information on the power management of the ESP32-WROOM module, pleaser refer to Section 3.7 and Tables: 8 and 17 of the ESP32 SoC Datasheet.

Debugging

For users interested in debugging their code, the JTAG pins are broken out on the board. However, the debugging feature is only available through the ESP-IDF.

  • TMS: GPIO 14
  • TDI: GPIO 12
  • TCK: GPIO 13
  • TDO: GPIO 15

JTAG Pins

The JTAG pins of the ESP32-WROOM module on the IoT Motor Driver.

Firmware Download Mode

Users can manually force the board into the serial bootloader with the BOOT button. Please, refer to the Boot Button section below for more information.

Peripherals and I/O

Warning

Users should be aware of the following nuances of this board

The ESP32-WROOM module has 26 multifunctional GPIO, of which, 16 I/O pins are used to interface with motor driver, sensors, and status LED on the board. Additionally, 13 I/O pins are broken out to PTH pins and the users buttons. All of the IoT Motor Driver pins have a .1" pitch spacing for headers.

While all of the GPIO pins are capable of functioning as digital I/O pins, various pins can have additional capabilities with the pin multiplexing feature of the ESP32 SoC. For more technical specifications on the I/O pins, please refer to the ESP32 SoC datasheet.

  • 13x 12-bit analog to digital converter (ADC) channels
  • 3x UARTs (only two are configured by default in the Arduino IDE, one UART is used for bootloading/debug)
  • 3x SPI (only one is configured by default in the Arduino IDE)
  • 2x I2C (only one is configured by default in the Arduino IDE)
  • 2x I2S Audio
  • 2x digital-to-analog converter (DAC) channels
  • 16x 20-bit PWM outputs
  • 8x Capacitive Touch Inputs

Info

Users should be aware of the following limitations for the board in the Arduino IDE.

  • Not all of the features, listed above, are available in the Arduino IDE. For the full capabilities of the ESP32, the Espressif IDF should be utilized.
    • Only one I2C bus is defined.
    • Only two UART interfaces are available.
      • UART (USB): Serial
      • RX/TX Pins: Serial1
    • Only one SPI bus is defined.

Peripheral Devices

This development board features several components operating together to create an IoT device. Their connections are shown in the diagram below and their operations are listed in the boxes below. For more details on each component, please refer to the sections below.

Block Diagram

Block diagram of the IoT Motor Driver board's peripherals.

  • Inputs


    • TMC6300 Motor Driver
      • Diagnostic Pin
    • TMAG5273 Hall-Effect Sensor
    • INA240 Current-Sense Amplifier
    • MCP6021 Operational Amplifier
    • User Buttons
  • Outputs


    • TMC6300 Motor Driver
      • Half-Bridge Pins
      • Standby Pin
    • RGB Status LED

Pin Functionality

There are several pins that have special functionality in addition to general digital I/O. These pins and their additional functions are listed in the tabs below. For more technical specifications on the I/O pins, you can refer to the schematic, ESP32-WROOM module datasheet, ESP32 SoC datasheet, and documentation for the ESP32 Arduino core.

Any GPIO pin on the ESP32-WROOM module can function as a digital I/O (input or output). However, users will need to declare the pinMode() (link) in the setup of their sketch (programs written in the Arduino IDE) to configure a pin as an input or an output.

  • Inputs


    When configured properly, an input pin will be looking for a HIGH or LOW state. Input pins are High Impedance and takes very little current to move the input pin from one state to another.

    DIAG (TMC6300) GPIO 34
    INT (TMAG5273) GPIO 04
    Button 13 GPIO 13
    Button 14 GPIO 14
  • Outputs


    When configured as an output the pin will be at a HIGH or LOW voltage. Output pins are Low Impedance: This means that they can provide a relatively substantial amount of current to other circuits.

    VIO (TMC6300) GPIO 05
    WS2812 GPIO 02

    Warning

    ⚡ There are electrical limitations to the amount of current that the ESP32-WROOM module can sink or source. For more details, check out the ESP32-WROOM module datasheet.

Tip

Pins cannot be configured to operate simultaneously as an input and output, without implementing the pin as an interrupt.

The ESP32-WROOM module provides a 12-bit ADC input on thirteen of its I/O pins. This functionality is accessed in the Arduino IDE using the analogRead(pin) function. (The available ADC pins are highlighted in the image below.)

Current Sensor INA240 (U) INA240 (V) INA240 (W) MCP6021
Analog Input GPIO 35 GPIO 36 GPIO 39 GPIO 32

Info

By default, in the Arduino IDE, analogRead() returns a 10-bit value. To change the resolution of the value returned by the analogRead() function, use the analogReadResolution(bits) function.

Tip

To learn more about analog vs. digital signals, check out this great tutorial.

The ESP32-WROOM module supports up to sixteen channels of 20-bit PWM (Pulse Width Modulation) outputs on any of its I/O pins. This is accessed in the Arduino IDE using the analogWrite(pin, value) function. (Any I/O pin can be used for the PWM outputs; the available DAC pins, with true analog outputs, are highlighted in the image below.)

Annotated image of DAC pins

Motor Driver UH UL VH VL WH WL
PWM Output GPIO 16 GPIO 17 GPIO 18 GPIO 23 GPIO 19 GPIO 33

Info

By default, in the Arduino IDE, analogWrite() accepts an 8-bit value. To change the resolution of the PWM signal for the analogWrite() function, use the analogWriteResolution(bits) function. (The PWM output is not a true analog signal.)

Tip

To learn more about pulse width modulation (PWM), check out this great tutorial.

The ESP32-WROOM module provides three UART ports. By default, the UART port for the USB connection (Serial) and the labeled UART I/O pins on the board (Serial1) can be accessed through the Arduino IDE using the serial communication class.

Info

By default, in the Arduino IDE, the board definition supports:

  • Serial - UART (USB)
  • Serial1 - Pins: RX/TX (GPIO 16/GPIO 17)
Note
  • The GPIO 16 and GPIO 17 pins of Serial1 are already dedicated to the UH/UL half-bridge on the TMC63000 motor driver and are not broken out for users to access.
  • In order to utilize the serial communication on the strapping pins, users will need to create a custom serial port object and declare which pins to access.

Tip

To learn more about serial communication, check out this great tutorial.

Tip

We have noticed that with the ESP32 Arduino core, Serial.available() does not operate instantaneously. This is due to an interrupt triggered by the UART, to empty the FIFO when the RX pin is inactive for two byte periods:

  • At 9600 baud, hwAvailable takes [number of bytes received + 2] x 1 ms = 11 ms before the UART indicates that data was received from: \r\nERROR\r\n.
  • At 115200 baud, hwAvailable takes [number of bytes received + 2] x .087 ms = ~1 ms before the UART indicates that data was received from: \r\nERROR\r\n.

For more information, please refer to this chatroom discussion.

The ESP32-WROOM module provides three SPI buses. By default, in the Arduino IDE, the SPI class is configured to utilize pins GPIO 18 (SCK), GPIO 19 (POCI), GPIO 23 (PICO). In order to utilize the other SPI ports or objects, users will need to create a custom SPI object and declare which pins to access.

Info

To comply with the latest OSHW design practices, we have adopted the new SPI signal nomenclature (SDO/SDI and PICO/POCI). The terms Master and Slave are now referred to as Controller and Peripheral. The MOSI signal on a controller has been replaced with SDO or PICO. Please refer to this announcement on the decision to deprecate the MOSI/MISO terminology and transition to the SDO/SDI naming convention.

SCK GPIO 18 (SCK)
SDI or POCI GPIO 19 (MISO)
SDO or PICO GPIO 23 (MOSI)
CS GPIO 5 (SS)
Note
  • The GPIO 18,GPIO 19, and GPIO 23 pins of the SPI bus are already dedicated to the VH/WH/VL MOSFETs on the TMC63000 motor driver and are not broken out for users to access.
  • The CS pin associated with GPIO 05 is also already dedicated to the STBY pin of the TMC63000 motor driver and is not broken out for users to access.

Tip

To learn more about the serial peripheral interface (SPI) protocol, check out this great tutorial.

The ESP32-WROOM module module can support up to two I2C buses. By default, in the Arduino IDE, the Wire class is configured to utilize pins GPIO 21 (SDA) and GPIO 22 (SCL). These pins share the same I2C bus with the Qwiic connector and TMAG5273 hall-effect sensor. In order to utilize the other I2C ports, users will need to create a custom Wire object and declare which pins to access.

  • I2C Pins

    SCL GPIO 22
    SDA GPIO 21

    TMAG5273 I2C Address:

    • 0x35 (Default) (7-bit)
    • 0x6A (write)/0x6B (read)
  • Tutorial thumbnail
    Default I2C bus connections for the IoT Motor Driver.

Tip

To learn more about the inter-integrated circuit (I2C) protocol, check out this great tutorial.

 Motor Driver - TMC6300

The TMC6300 from Trinamic Motion Control, part of Analog Devices, is a low voltage, 3-Phase BLDC/PMSM motor driver utilizing separate high-side and low-side control signals for its three half-bridges.

  • Features:

    • VIN: 2.0V to 11.0V
      • Operating current: 7mA
      • Standby current: 30nA
    • VOUT: 1.8V
    • 3 Half-Bridges
      • 3 High-side MOSFETs
      • 3 Low-side MOSFETs
    • I/O Supply Voltage Input
    • Diagnostic Output
    • Overtemperature Protection
      • Shutdown Temperature: 150°C
      • Typical Power Dissipation: 1W
    • Short Protection

    Info

    For more details, please refer to the TMC6300 datasheet.

  • TMC6300 chip on the IoT Motor Driver.

    For users unfamiliar with the TMC6300 motor driver, please check out our hookup guide below.

Half-Bridges

The TMC6300 features high-side and low-side MOSFET pairs of the three available half-bridges which control the commutation of the three motor phases.

6 PWM control of a 3-phase motor commutation.
(Source: Modified from the Block commutation vs. FOC in power tool motor control application note)

The electronic commutation sequence for these MOSFETs will depend on the motor that is connected. For most cases, users will provide a PWM signal to each of these pins. These are active-high pins.

ESP32-WROOM 16 17 18 23 19 33
Motor Driver UH UL VH VL WH WL
Active High

By pulling the pin high, the MOSFET will enable power to flow through that section of the half-bridge.

With the electronic commutation sequence provided to the half-bridges, the output motor phases will drive a connected motor.

The three motor phase outputs (U/V/W) from the TMC6300 are used to drive the gimbal motor, attached through the JST connector.

Motor Commutation

The TMC6300 relies on an electrical commutation sequence/signal to drive the motor phases to a BLDC or PMSM motor. The commutation signals for these motors are trapezoidal for BLDC motors and sinusoidal for PMSM motors.

  • Trapezoidal motor commutation.

  • Sinusoidal motor commutation.

*(Source: [Brushless-DC Motor Driver Considerations and Selection Guide](https://www.ti.com/lit/an/slvaes1a/slvaes1a.pdf) application note)*

Gimbal Motor

Based on measuring the output from one of the coils, our gimbal motor is a PMSM and would require a sinusoidal waveform to drive the motor. It should be noted that a trapezodial waveform can probably be used; however, users may notice effects such as cogging.

Sinusoidal PWM signal.
(Source: Demystifying BLDC motor commutation: Trap, Sine, & FOC)

For a trapezoidal signal, the high-side (HS) and low-side (LS) MOSFETs, can just be driven high or low. However, in order to approximate a sinusoidal signal, a progressively varying PWM signal must be provided with all six signals in sync with each other.

VIO/Standby Pin

In it's default configuration, the VIO pin is used to enable the motor driver and set the logic level voltage of the TMC6300 inputs. However, the VIO pin also operates as a standby pin when it is pulled LOW. In standby, the TMC6300 resets and sits in standby mode.

Users can control the VIO pin with GPIO 05 on the ESP32-WROOM module, to reset the TMC6300 or put it in standby mode.

Diagnostic Pin

The diagnostic pin is triggered based on different faults (i.e. shorts and overtemperature) detected by the IC. By default, the status will be indicated by the, green diagnostic, DIAG LED and will remail LOW until triggered. Once triggered, users will need to disable and reset the TMC6300 or power cycle the board.

Users can monitor the diagnostic pin with GPIO 34 on the ESP32-WROOM module, to determine if the TMC6300 need to be reset to clear a fault.

Current Sense Pin

The current sense pin is the foot point of the U and V half-bridges, with a 0.12Ω resistor attached. Users can measure the voltage across the resistor to determine the current flowing to the motor (see the Low-side Op Amp - MCP6021 section below).

 Hall-Effect Sensor - TMAG5273

The TMAG5273 from Texas Instruments, is a 3-axis hall-effect sensor utilizing a 12-bit ADC. For more information, please refer to the TMAG5273 datasheet.

  • Features:

    • I2C Address:
      • 0x35 (Default) (7-bit)
      • 0x6A (write)/0x6B (read)
    • Magnetic Range (Sensitivity):
      • ± 40mT (820 LSB/mT)
      • ± 80mT (410 LSB/mT)
    • Magnetic Drift: 5%
    • Rotational Accuracy: ± 0.5°/360° rotation
    • Voltage Range: 1.7 - 3.6V
      • Sleep: 5nA
      • Wake-Up/Sleep: 1µA
      • Active: 2.3mA
    • Operating Temperature: –40 - 125°C
    • Integrated temperature compensation
    • Configurable sample rate
  • Tutorial thumbnail
    The TMAG5273 hall-effect sensor on the IoT Motor Driver.

    Magnetic Axes

    On the IoT Motor Driver, users will primarily be interested in magnetic field of the X-Y axes to measure the position of the gimbal motor.

    Magnetic axes
    The magnetic axes of TMAG5273 hall-effect sensor.

Info

For more details, please refer to the TMAG5273 datasheet.

Interrupt Pin

The interrupt pin of the TMAG5723 can be configured in different modes to utilize either the INT or SCL pins.

  • No interrupt
  • Interrupt through INT
  • Interrupt through INT except when I2C busy
  • Interrupt through SCL
  • Interrupt through SCL except when I2C busy

Tip

We recommend utilizing the default INT pin to trigger interrupts; as it is already connected to GPIO 04 of the ESP32-WROOM module.

Bus Contention

Texas Instruments does not recommend sharing the I2C bus with multiple devices when using the SCL pin for the interrupt function. The SCL interrupt can potentially corrupt the transactions with other devices, when present on the same I2C bus.

Note

The TMAG5273 is programmed to detect a magnetic threshold in wake-up or sleep mode. Once the magnetic threshold cross is detected, the device asserts a latched interrupt signal through the INT pin, and goes back to stand-by mode. The interrupt latch is cleared through the SCL pin.

Current Sensors

There are two different types of Op Amps on the board to amplify the input voltage for the current measurements.

  • The INA240 is used for the in-line current measurements between the TMC6300 and the gimabal motor.
  • The MCP6021 is used on the low-side current measurement of the TMC63000's half-bridges.
| **Current Sensor** | INA240 *(`U`)* | INA240 *(`V`)* | INA240 *(`W`)* | MCP6021 | | :----------------- | :------------: | :------------: | :------------: | :-------: | | **Analog Input** | `GPIO 35` | `GPIO 36` | `GPIO 39` | `GPIO 32` |

 Inline - INA240

The INA240 from Texas Instruments, is a voltage-output, current-sense amplifier. For more information, please refer to the INA240 datasheet.

  • Tutorial thumbnail
    The INA240 current-sense amplifier on the IoT Motor Driver.

  • Configured Gain 20 &PlusMn;0.2%
    Bandwidth 100kHz
    Voltage Range Range: 2.7 - 5.5V
    Quiescent Current 1.8 - 2.6mA
    Operating Temperature –40 - 125°C

 Low-side Op Amp - MCP6021

The MCP6021 from Microchip Technology, Inc., is a rail-to-rail input and output operational amplifier. The chip . For more information, please refer to the MCP6021 datasheet.

  • Tutorial thumbnail
    The MCP6021 Op Amp on the IoT Motor Driver.

  • Configured Gain 21
    Bandwidth 10MHz
    Voltage Range Range: 2.5 - 5.5V
    Quiescent Current 0.5 - 1.35mA
    Operating Temperature –40 - 125°C

Status LEDs

There are five status LEDs on the TMC6300 motor driver:

  • PWR - Power (Red)
    • Turns on once power is supplied through the USB-C connector
  • MPWR - Power (Red)
    • Turns on once power is supplied through the USB-C connector
  • DIAG - Diagnostics (Green)
  • STBY - Standby (Blue)
    • Turns on when the motor driver is enabled
    • Turns off, when the IC has been reset and the motor driver is in standby mode
  • STAT - User (RGB)
    • Controlled through GPIO 02

The status indicator LEDs on the TMC6300 motor driver.

WS2812 RGB LED

The WS2812 RGB LED is controlled with a 24-bit (GRB) data signal. This indicator is connected to GPIO 02 and the digital output pin from the LED is available through a test point. For more information, please refer to the WS2812C datasheet.

The status indicator LED (STAT)on the IoT Motor Driver.

Info

The latest ESP32 Arduino core, now provides a basic RGB LED driver for a WS2812 (or NeoPixel) LED populated the board. For an example of how to utilize the RGB LED driver check out the BlinkRGB example code, which can be accessed from the File drop down menu (i.e File > Examples > ESP32 > GPIO > BlinkRGB).

Buttons

There are four buttons on IoT Motor Driver: RST, BOOT, 13, and 14 buttons.

Buttons

Buttons on the IoT Motor Driver.

Factory Programming

The IoT Motor Driver board will come pre-programmed out of the bag. By default, the 13/14 buttons can be used to operate the motor:

  • 13 - Start/Stop the motor's rotation
  • 14 - Switch the direction that the motor is spinning

Reset Button

The RST (reset) button allows users to reset the program running on the ESP32-WROOM module without unplugging the board.

Reset Button

RST button on the IoT Motor Driver.

Boot Control

The BOOT button can be used to force the board into the serial bootloader. Holding down the BOOT button, while connecting the board to a computer through its USB-C connector or resetting the board will cause it to enter the Firmware Download mode. The board will remain in this mode until it power cycles (happens automatically after uploading new firmware) or the RST button is pressed.

  1. Hold the BOOT button down.
  2. Reset the MCU.
    • While unpowered, connect the board to a computer with through the USB-C connection.
    • While powered, press the RST button.
  3. Release the BOOT button.
  4. After programming is completed, reboot the MCU.
    • Press the RST button.
    • Power cycle the board.

Boot Button

BOOT button on the IoT Motor Driver.

Info

⚡ The BOOT button is also connected to GPIO 0.

User Buttons

The 13 and 14 buttons are available for users to configure for their own purposes.

User Buttons

The user buttons (13 and 14) on the IoT Motor Driver.

Factory Programming

The IoT Motor Driver board will come pre-programmed out of the bag. By default, these buttons can be used to operate the motor:

  • 13 - Start/Stop the motor's rotation
  • 14 - Switch the direction that the motor is spinning

Tip

When utilizing the buttons, users should enable the internal pull-up resistors for the GPIO pins.

Jumpers

Never modified a jumper before?

Check out our Jumper Pads and PCB Traces tutorial for a quick introduction!

There are nine jumpers on the back of the board that can be used to easily modify a hardware connections on the board.

  • SHLD - This jumper can be used to disconnect the shield of the USB-C connector from GND.
  • MEAS - This jumper can be used to measure the current consumption of the board.
  • BYP - This jumper can be used to bypass the thermal fuse.
  • LED Jumpers
    • PWR - This jumper can be used to remove power from the red, power LED on the AP2112 LDO regulator.
    • MPWR - This jumper can be used to remove power from the red, power LED on the AP63357 LDO regulator.
    • STBY - This jumper can be used to remove power from the blue, standby LED.
    • DIAG - This jumper can be used to remove power from the green, diagnostic LED.
  • INT - This jumper can be used to remove the pull-up resistor from the INT pin of the hall-effect sensor.
  • I2C - This jumper can be used to remove the pull-up resistors on the I2C bus.

Jumpers

The jumpers on the back of the IoT Motor Driver.

Primary I2C Bus

The Qwiic connector and hall-effect sensor are attached to the primary I2C bus. The primary I2C bus for this board utilizes the pin connections, detailed in the table below:

I2C connections

I2C bus connections on the IoT Motor Driver.

Connection VDD GND SCL SDA
Hall-Effect Sensor
(TMAG5273)
3V3 GND GPIO 22 GPIO 21
Qwiic Connector 3V3 GND GPIO 22 GPIO 21

Qwiic Connector

A Qwiic connector is provided for users to seamlessly integrate with SparkFun's Qwiic Ecosystem. Otherwise, users can connect their I2C devices through the PTH pins broken out on the board.

Qwiic connector and I2C pins

Qwiic connector and I2C pins on the IoT Motor Driver.

What is Qwiic?

Qwiic Logo - light theme Qwiic Logo - dark theme


The Qwiic connect system is a solderless, polarized connection system that allows users to seamlessly daisy chain I2C boards together. Play the video below to learn more about the Qwiic connect system or click on the banner above to learn more about Qwiic products.

Features of the Qwiic System

no soldering - light theme no soldering - dark theme

Qwiic cables (4-pin JST) plug easily from development boards to sensors, shields, accessory boards and more, making easy work of setting up a new prototype.

polarized connector - light theme polarized connector - dark theme

There's no need to worry about accidentally swapping the SDA and SCL wires on your breadboard. The Qwiic connector is polarized so you know you’ll have it wired correctly every time, right from the start.

The PCB connector is part number SM04B-SRSS (Datasheet) or equivalent. The mating connector used on cables is part number SHR04V-S-B or an equivalent (1mm pitch, 4-pin JST connector).

daisy chainable - light theme daisy chainable - dark theme

It’s time to leverage the power of the I2C bus! Most Qwiic boards will have two or more connectors on them, allowing multiple devices to be connected.

Hardware Assembly

USB Programming

The USB connection is utilized for programming and serial communication. Users only need to plug their IoT Motor Driver into a computer using a USB-C cable.

IoT Motor Driver USB connection

The IoT Motor Driver with USB-C cable attached.

Headers

New to soldering?

If you have never soldered before or need a quick refresher, check out our How to Solder: Through-Hole Soldering guide.

The pins for the IoT Motor Driver are broken out into 0.1"-spaced pins on the outer edges of the board. When selecting headers, be sure you are aware of the functionality you require.

Soldering headers

Soldering headers to the IoT Motor Driver.

Qwiic Devices

The Qwiic system allows users to effortlessly prototype with a Qwiic compatible I2C device without soldering. Users can attach any Qwiic compatible sensor or board, with just a Qwiic cable. (*The example below, is for demonstration purposes and is not pertinent to the board functionality or this tutorial.)

Qwiic devices connected to IoT Motor Driver

The BME688 environmental and VL53L1X distance Qwiic sensor boards connected to the IoT Motor Driver.

Software Overview

CH340 Driver

Users will need to install the appropriate driver for their computer to recognize the serial-to-UART chip on their board/adapter. Most of the latest operating systems will recognize the CH340C chip on the board and automatically install the required driver.

To manually install the CH340 driver on their computer, users can download it from the WCH website. For more information, check out our How to Install CH340 Drivers Tutorial.

How to Install CH340 Drivers

How to Install CH340 Drivers

Arduino IDE

Tip

For first-time users, who have never programmed before and are looking to use the Arduino IDE, we recommend beginning with the SparkFun Inventor's Kit (SIK), which is designed to help users get started programming with the Arduino IDE.

Most users may already be familiar with the Arduino IDE and its use. However, for those of you who have never heard the name Arduino before, feel free to check out the Arduino website. To get started with using the Arduino IDE, check out our tutorials below:

Install Board Definition

Install the latest ESP32 board definitions in the Arduino IDE.

[![Installing Board Definitions in the Arduino IDE](https://cdn.sparkfun.com/c/500-282/assets/learn_tutorials/1/2/6/5/sparkfun_boards.PNG)](https://learn.sparkfun.com/tutorials/1265)
[**Installing Board Definitions in the Arduino IDE**](https://learn.sparkfun.com/tutorials/1265)

Info

For more instructions, users can follow this tutorial on Installing Additional Cores provided by Arduino. Users will also need the .json file for the Espressif Arduino core:

https://raw.githubusercontent.com/espressif/arduino-esp32/gh-pages/package_esp32_index.json

When selecting a board to program in the Arduino IDE, users should select the SparkFun ESP32 Thing Plus C from the Tools drop-down menu (_i.e. Tools > Board > ESP32 Arduino > SparkFun ESP32 Thing Plus C). Alternatively, users can also select the ESP32 Dev Module; however, they may lose some pin assignments.

Select the SparkFun ESP32 Thing Plus C from the Tools drop-down menu in the Arduino IDE.

Arduino IDE 2.x.x - Alternative Method

In the newest version of the Arduino IDE 2.x.x, users can also select their board (green) and port (blue) from the Select Board & Port dropdown menu (yellow).

Selecting the SparkFun ESP32 Thing Plus C and COM5 port from the Select Board & Port drop-down menu in the Arduino IDE (v2.0.3).

SparkFun TMAG5273 Arduino Library

The SparkFun TMAG5273 Arduino Library can be installed from the library manager in the Arduino IDE.

SparkFun TMAG5273 Arduino library in the library manager of the Arduino IDE.

Arduino IDE (v1.x.x)

In the Arduino IDE v1.x.x, the library manager will have the following appearance for the SimpleFOC library:

SparkFun TMAG5273 Arduino library in the library managerof the Arduino IDE (v1.x.x).

This library will be primarily used to interact with the TMAG5273 hall-effect sensor and return the rotation angle of the motor.

SimpleFOC Arduino Library

The Simple Field Oriented Control Library can be installed from the library manager in the Arduino IDE.

SimpleFOC library in the library manager of the Arduino IDE.

Arduino IDE (v1.x.x)

In the Arduino IDE v1.x.x, the library manager will have the following appearance for the SimpleFOC library:

SimpleFOC library in the library manager of the Arduino IDE (v1.x.x).

This library utilizes a motor control scheme called field oriented control (FOC), which can utilize a feedback control loop to drive a motor with a higher power efficiency and precision characteristics, like evenly distributed torque control.

Info

For more details about the library, check out the online documentation.

Supported Hardware

For a detailed and up-to-date list of the hardware supported by this library, check out the library's documentation. The following are excerpts taken from the library's documentation page:

Supported microcontrollers

Choosing the Right Microcontroller

There are three main parameters when choosing the microcontroller for your project:

  1. Processing power (clock speed, architecture, etc.) - this will determine the performance of the FOC algorithm and the maximum speed of your motor.
  2. PWM generation capabilities - this will determine the number of motors you can control and the control modes you can use.
  3. ADC sensing capabilities - this will determine the current sensing options you have for your project.

1. Processing power

When it comes to the processing power, the rule of thumb is: - The higher the clock speed the better. - Aim for the FOC execution time of loopFOC() to be above 1kHz (ideally above 5kHz) depending on the motor and sensor combination you are using.

Info

For more details, please refer to the SimpleFOC Arduino library documentation.

Arduino SimpleFOClibrary has a goal to support as many BLDC and stepper motor drivers as possible. Till this moment there are two kinds of motor drivers supported by this library:

Current Limitations

Choosing the Appropriate Driver

Selecting the right hardware is a balance of motor type, power requirements, and the level of control precision you need.

1. Motor Type

  • BLDC Motors: Requires a BLDC driver. Ensure the current and voltage ratings match your motor's specs.
    • ⚠️ No Drone ESCs Traditional drone ESCs are not suitable for FOC because they typically use a fixed commutation scheme and lack the necessary control interfaces.
  • Stepper Motors:
    • Dedicated Stepper Driver: Best for 2-phase motors within standard current ranges (ex.NEMA17)
    • Hybrid Mode: You can actually use any BLDC driver to run a stepper motor. - See example
    • ⚠️ No Step/Dir Drivers Traditional "EasyDrivers" or A4988s (in step/dir mode) cannot be used for FOC because they do not allow direct phase voltage control.

2. Current Requirements

  • Low Current (< 5A): Integrated driver ICs are cost-effective and easy to use.
    • Examples: L6234, DRV8313, DRV8316.
  • High Current (> 5A): Requires discrete MOSFET-based designs with robust thermal management (heatsinks/fans).
    • Examples: DRV8302, VESC-based hardware.
  • Rule of Thumb: Always select a driver with a current rating at least 20-30% higher than your motor's expected continuous current.

📢 Critical: Read before powering up!

Before running any motor, you must ensure your hardware can handle the stall current. FOC can easily pull more current than a driver can handle if not limited in software.

The Worst-Case Calculation Check your motor's phase resistance ($\(R\)\() and your power supply voltage (\)\(V_{DC}\)\(). The maximum possible current (\)\(I_{max}\)$) is:

\[I_{max} = \frac{V_{DC}}{R}\]

Safety Steps: - Compare: If $\(I_{max}\)$ exceeds your driver's rating, you must limit the voltage in software. - Software Limit: Use driver.voltage_limit and (motor.voltage_limit and/or motor.current_limit) to stay within safe bounds. - see motor docs - Power Supply: If you can, use a current-limited lab bench power supply for your initial tests.

Tip

While the TMC6300 isn't directly listed as part of the supported hardware for the SimpleFOC Arduino library, we have verified that is compatible with the library.

Info

For more details, please refer to the SimpleFOC Arduino library documentation.

Arduino SimpleFOClibrary supports two types of BLDC motors:

  • BLDC motors

    • 3 phase (3 wire):

      Gimbal Motors

      Gimbal motors

      Gimbal motors will work basically with any BLDC motor driver, but since the high-performance drivers have current measurement circuits optimized for high currents you will not have any benefit of using them. Therefore low-power BLDC motor drivers will have comparable performance as the expensive high-power, high-performance drivers for gimbal motors. What is in my opinion very cool! 😃 This was one of the main motivations to start developing SimpleFOCShield.

      Some of the characteristics of Gimbal motors are: - High torque on low velocities - Very smooth operation - Internal resistance >10Ω - Currents up to 5A

      High-performance Motors
  • Stepper motors

    • 2 phase (4 wire)
Current Limitations

Before running any motor, you must ensure your hardware can handle the stall current. FOC can easily pull more current than a driver can handle if not limited in software.

The Worst-Case Calculation Check your motor's phase resistance ($\(R\)\() and your power supply voltage (\)\(V_{DC}\)\(). The maximum possible current (\)\(I_{max}\)$) is:

\[I_{max} = \frac{V_{DC}}{R}\]

Safety Steps: - Compare: If $\(I_{max}\)$ exceeds your driver's rating, you must limit the voltage in software. - Software Limit: Use driver.voltage_limit and (motor.voltage_limit and/or motor.current_limit) to stay within safe bounds. - see motor docs - Power Supply: If you can, use a current-limited lab bench power supply for your initial tests.

Info

For more details, please refer to the SimpleFOC Arduino library documentation.

6PWM Motor Driver

Users will need to utilize the BLDCDriver6PWM class to provide the six PWM signals required for the TMC6300 motor driver.

BLDCDriver6PWM

This class provides an abstraction layer for most of the common BLDC drivers, which require six PWM signals. This method offers more control than a three PWM motor drivers, since each of the 6 half-bridges MOSFETs can be controlled independently.

⚠️ Note: When using the 3PWM BLDC driver with a stepper motor, ensure that the common phase Uo is connected to the driver's C phase pin.

Microcontroller Considerations

Step 1. Hardware setup

To create the interface to the BLDC driver you need to specify the 6 PWM pin numbers for each motor phase and optionally enable pin. ```cpp // BLDCDriver6PWM( int phA_h, int phA_l, int phB_h, int phB_l, int phC_h, int phC_l, int en) // - phA_h, phA_l - A phase pwm pin high/low pair // - phB_h, phB_l - B phase pwm pin high/low pair // - phB_h, phC_l - C phase pwm pin high/low pair // - enable pin - (optional input)

⚠️ 6 PWM configuration is very hardware specific and please make sure to respect certain guidelines in order for it to work properly!

  • Hardware PWM


    ⚠️ Note: When using the 6PWM BLDC driver with a stepper motor, ensure that the common phase Uo is connected to the driver's C phase pin.

    Even if the common phase Uo is physically connected to some other driver output (A or B), please provide it as the C phase pin in the driver constructor. This is important for the correct operation of the stepper motor.

    Consider an example of the driver connected to the MCU pins as follows:

    ```cpp

    define PIN_A_H 9

    define PIN_A_L 10

  • Software PWM


    define PIN_C_H 13

    define PIN_C_L 14

    define ENABLE 8

    If the common phase `Uo` is connected to the driver pin `A`, you should still provide it as the `C` phase pin in the driver constructor:
    ```cpp
    // common phase `Uo` connected to driver pin `A` so it is provided as the `C` phase pin
    BLDCDriver6PWM driver = BLDCDriver6PWM(PIN_C_H, PIN_C_L, PIN_B_H, PIN_B_L, PIN_A_H, PIN_A_L, ENABLE);
    

    If the common phase Uo is connected to the driver pin B, you should provide it as the C phase pin in the driver constructor:

    // common phase `Uo` connected to driver pin `B` so it is provided as the `C` phase pin
    BLDCDriver6PWM driver = BLDCDriver6PWM(PIN_A_H, PIN_A_L, PIN_C_H, PIN_C_L, PIN_B_H, PIN_B_L, ENABLE);
    

    Or if the common phase Uo is connected to the driver pin C, you should provide it as the C phase pin in the driver constructor:

    // common phase `Uo` connected to driver pin `C` so it is provided as the `C` phase pin
    BLDCDriver6PWM driver = BLDCDriver6PWM(PIN_A_H, PIN_A_L, PIN_B_H, PIN_B_L, PIN_C_H, PIN_C_L, ENABLE);
    

Arduino UNO support

Info

For more details about the BLDCDriver6PWM class, check out the online documentation.

BLDC Motor

All BLDC motors are handled with the BLDCMotor class.

BLDCMotor

This class implements the BLDC FOC algorithm, motion control loops, and monitoring.

Step 1. Creating the instance of the BLDC motor

To instantiate the BLDC motor we need to create an instance of the BLDCMotor class and provide it the number of pole pairs of the motor. ```cpp // BLDCMotor(int pp, (optional R, KV, Lq, Ld)) // - pp - pole pair number // - R - phase resistance value [Ohm] - optional // - KV - motor KV rating [rpm/V] - optional

Motor Considerations

While, the datasheet for our gimbal motor, indicates that there are 8 pole pairs, we have found that the motor operates more smoothly if the BLDCMotor class is instantiated with 7 pole pairs instead.

cp BLDCMotor motor = BLDCMotor(7);

Info

For more details about the BLDCMotor class, check out the online documentation.

Position Sensor

In order to incorporate the TMAG5273 hall-effect sensor into the FOC algorithm, users will need to utilize the GenericSensor class.

GenericSensor

This class allows users to link a custom position sensor (not already implemented in the SimpleFOC library) by incorporating a few functions into their sketch.

  1. Implement two functions; one to initialize the TMAG5273 and another to read and return the sensor's current position.

    return ...; } ```

    additionally you can optionally implement a function that initialises your sensor

    A quick guide to implement your own sensor class (Advanced)

    Step 1. Implement the function reading your sensor

    Basically all that you need to do in your arduino code is implement a function that reads your sensor and returns an angle in radians between 0 and 2π: ```cpp float readMySensorCallback(){

  2. Instantiate the GenericSensor class and initialize the class by providing it pointers to the two functions.

    } ```

    Step 2. Instantiate GenericSensor class

    To initialize the sensor class you need to provide it the pointer to your function reading the sensor, and optionally the pointer to the function that initialises your sensor. ```cpp

  3. There are two ways to use sensors implemented within the SimpleFOC library:

    • As standalone position sensor
      • In this configuration users would simply read the sensor's position, independently from incorporating the readings into the FOC algorithm.
    • Incorporate it as the motor position sensor for FOC algorithm

      1. Initialize the sensor in the setup() loop:

        Here is a quick example:
        ```cpp
        #include <SimpleFOC.h>
        
        float readMySensorCallback(){
         // read my sensor
         // return the angle value in radians in between 0 and 2PI
         return ...;
        }
        
      2. Link the sensor in the setup() loop:

        float readMySensorCallback(){
         // read my sensor
         // return the angle value in radians in between 0 and 2PI
         return ...;
        }
        
        void initMySensorCallback(){
          // do the init
        }
        

Info

For more instructions on incorporating the GenericSensor class, please refer to the SimpleFOC documentation.

In-line Current Sensing

In order to incorporate the current sensing into the FOC algorithm, users will need to utilize the InlineCurrentSense class.

InlineCurrentSense

This class allows users to link a custom position sensor (not already implemented in the SimpleFOC library) by incorporating a few functions into their sketch.

  1. Instantiate the InlineCurrentSense class and initialize the class by providing the hardware configuration.

    SAMD21 | ✔️
    SAMD51 | ✔️
    Teensy | ✔️ Raspberry Pi Pico | ✔️ Portenta H7 | ✔️ Renesas (UNO R4) | ❌ (TBD) Arduino Nano Matter(📢NEW) | ✔️

  2. Incorporate the current sensor into the FOC algorithm:

    1. Initialize the sensor in the setup() loop:

      InlineCurrentSense current_sense = InlineCurrentSense(shunt_resistor, gain, A0, A1, _NC); // when measuring A and B phase currents and not measuring C // or InlineCurrentSense current_sense = InlineCurrentSense(shunt_resistor, gain, A0, A1); // when measuring A and B phase currents and not measuring C ```

    2. Link the sensor to the motor driver in the setup() loop:

      // - phA - A phase adc pin // - phB - B phase adc pin InlineCurrentSense current_sense = InlineCurrentSense(66.0, A0, A1); ```

    3. Link the sensor to the motor in the setup() loop:

      ```cpp

    current_sense.gain_c = 1.0 / shunt_resistor / gain;

    For example, Arduino <span class="simple">Simple<span class="foc">FOC</span>Shield</span> v2 has the phase B of the current sensing inverted. So in its case you can specify:
    ```cpp
    // inverse current sensing gain on phase b
    current_sense.gain_b *= -1;
    

    // default values of per phase gains
    current_sense.gain_a = 1.0 / shunt_resistor / gain;
    current_sense.gain_b = 1.0 / shunt_resistor / gain;
    

    For example, to invert the phase B current measurement you can easily change it gain to:

    // inverse current sensing gain on phase b
    current_sense.gain_b *= -1;
    

Info

For instructions on incorporating the InlineCurrentSense class, please refer to the SimpleFOC documentation.

Example - BLDC

In this example, users will be utilizing the TMC6300 motor driver to spin the motor.

Example Code

After installing and setting up the Arduino IDE and the Simple FOC Arduino library, users will need to upload the following example code using the SparkFun ESP32 Thing Plus C board definition. This code can be copied or downloaded below:

[:octicons-download-16:{ .heart } Download `BLDC.ino` Example Code](./assets/arduino_examples/BLDC/BLDC.ino){ .md-button .md-button--primary }

Example Code

BLDC.ino
    // Open loop motor control example
    #include <SimpleFOC.h>


    // BLDC motor & driver instance
    // BLDCMotor motor = BLDCMotor(pole pair number);
    BLDCMotor motor = BLDCMotor(7);
    // BLDCDriver3PWM driver = BLDCDriver3PWM(pwmA, pwmB, pwmC, Enable(optional));
    BLDCDriver6PWM driver = BLDCDriver6PWM(5, 6, 9,10, 3, 11);

    // Stepper motor & driver instance
    //StepperMotor motor = StepperMotor(50);
    //StepperDriver4PWM driver = StepperDriver4PWM(9, 5, 10, 6,  8);


    //target variable
    float target_velocity = 6;

    // // instantiate the commander
    Commander command = Commander(Serial);
    // void doTarget(char* cmd) { command.scalar(&target_velocity, cmd); }
    // void doLimit(char* cmd) { command.scalar(&motor.voltage_limit, cmd); }

    void setup() {

      // driver config
      // power supply voltage [V]
      driver.voltage_power_supply = 5;
      // limit the maximal dc voltage the driver can set
      // as a protection measure for the low-resistance motors
      // this value is fixed on startup
      driver.voltage_limit = 5;
      // pwm frequency to be used [Hz]
      // for atmega328 fixed to 32kHz
      // esp32/stm32/teensy configurable
      driver.pwm_frequency = 32000;


      driver.init();
      // link the motor and the driver
      motor.linkDriver(&driver);

      // limiting motor movements
      // limit the voltage to be set to the motor
      // start very low for high resistance motors
      // current = voltage / resistance, so try to be well under 1Amp
      motor.voltage_limit = 3;   // [V]

      // open loop control config
      motor.controller = MotionControlType::velocity_openloop;

      // init motor hardware
      motor.init();

      // add target command T
      // command.add('T', doTarget, "target velocity");
      // command.add('L', doLimit, "voltage limit");

      Serial.begin(115200);
      Serial.println("Motor ready!");
      Serial.println("Set target velocity [rad/s]");
      _delay(1000);

    }

    void loop() {

      // open loop velocity movement
      // using motor.voltage_limit and motor.velocity_limit
      motor.move(target_velocity);

      // user communication
      command.run();


    }

Running the Motor

By default, the motor should spin automatically. However, if users wish to control the speed of the motor, they can uncomment lines 21-22 and 56-57 of code and reprogram the board.

Code Changes Highlighted

Uncomment the following lines of code (21-22 and 56-57):

BLDC.ino
    // Open loop motor control example
    #include <SimpleFOC.h>


    // BLDC motor & driver instance
    // BLDCMotor motor = BLDCMotor(pole pair number);
    BLDCMotor motor = BLDCMotor(7);
    // BLDCDriver3PWM driver = BLDCDriver3PWM(pwmA, pwmB, pwmC, Enable(optional));
    BLDCDriver6PWM driver = BLDCDriver6PWM(5, 6, 9,10, 3, 11);

    // Stepper motor & driver instance
    //StepperMotor motor = StepperMotor(50);
    //StepperDriver4PWM driver = StepperDriver4PWM(9, 5, 10, 6,  8);


    //target variable
    float target_velocity = 6;

    // // instantiate the commander
    Commander command = Commander(Serial);
    // void doTarget(char* cmd) { command.scalar(&target_velocity, cmd); }
    // void doLimit(char* cmd) { command.scalar(&motor.voltage_limit, cmd); }

    void setup() {

      // driver config
      // power supply voltage [V]
      driver.voltage_power_supply = 5;
      // limit the maximal dc voltage the driver can set
      // as a protection measure for the low-resistance motors
      // this value is fixed on startup
      driver.voltage_limit = 5;
      // pwm frequency to be used [Hz]
      // for atmega328 fixed to 32kHz
      // esp32/stm32/teensy configurable
      driver.pwm_frequency = 32000;


      driver.init();
      // link the motor and the driver
      motor.linkDriver(&driver);

      // limiting motor movements
      // limit the voltage to be set to the motor
      // start very low for high resistance motors
      // current = voltage / resistance, so try to be well under 1Amp
      motor.voltage_limit = 3;   // [V]

      // open loop control config
      motor.controller = MotionControlType::velocity_openloop;

      // init motor hardware
      motor.init();

      // add target command T
      // command.add('T', doTarget, "target velocity");
      // command.add('L', doLimit, "voltage limit");

      Serial.begin(115200);
      Serial.println("Motor ready!");
      Serial.println("Set target velocity [rad/s]");
      _delay(1000);

    }

    void loop() {

      // open loop velocity movement
      // using motor.voltage_limit and motor.velocity_limit
      motor.move(target_velocity);

      // user communication
      command.run();


    }

In order to drive the motor, users will need to access the serial monitor and provide the commands necessary to drive the motor. A full list of the available commands can be found in the Simple FOC Arduino library documentation. However, only the T and L commands are enabled in the example code.

Baud Rate

The serial monitor baud rate should be configured to 115200bps.

Example - FOC Algorithm

Example - Factory Reset

This example, allows users to reprogram their board with the same sketch that it comes pre-programmed with from SparkFun.

Example Code

After installing and setting up the Arduino IDE and the Simple FOC Arduino library, users will need to upload the following example code using the SparkFun ESP32 Thing Plus C board definition. This code can be copied or downloaded below:

[:octicons-download-16:{ .heart } Download `IoT_MotorDriver.ino` Example Code](./assets/arduino_examples/IoT_MotorDriver/IoT_MotorDriver.ino){ .md-button .md-button--primary }

Example Code

IoT_MotorDriver.ino
    /******************************************************************************
        IoT Motor Driver Example

        Written By:
            Madison Chodikov
            Eric Orosel
        Company: SparkFun Electronics   
        Date: September 1 2023

        This sketch is a stripped down version of the firmware that is preprogrammed
        on the IoT Motor Driver. It is based on the open loop, velocity motor control
        example from the SimpleFOC Arduino library.

        This sketch will spin the motor based on the button inputs:
            - Button 13: Starts/Stops the motor rotation
            - Button 14: When spinning, switches the direction of rotation

    ===============================================================================
        Products:
            IoT Brushless Motor Driver: https://www.sparkfun.com/products/22132

        Repository:
            https://github.com/sparkfun/SparkFun_IoT_Brushless_Motor_Driver
    ===============================================================================

        SparkFun code, firmware, and software is released under the MIT 
        License (http://opensource.org/licenses/MIT).

        Distributed as-is; no warranty is given.
    ******************************************************************************/

    #include <Wire.h>
    #include <SimpleFOC.h> //http://librarymanager/All#Simple%20FOC


    //GPIO
    #define auxBtn2   13
    #define auxBtn1   14  

    //driver
    #define uh16      16
    #define ul17      17
    #define vh18      18
    #define wh19      19
    #define vl23      23
    #define wl33      33
    #define curSense  32

    bool state = true;

    //motor driver
    BLDCMotor motor = BLDCMotor(7);
    BLDCDriver6PWM driver = BLDCDriver6PWM(uh16, ul17, vh18, vl23, wh19, wl33,  curSense);
    float target_velocity = 0.0;
    Commander command = Commander(Serial);
    void doTarget(char* cmd) { command.scalar(&target_velocity, cmd); }
    void doLimit(char* cmd) { command.scalar(&motor.voltage_limit, cmd); }

    //////////////////////motor demo stuff///////////////////////////
    struct Button{
      const uint8_t PIN;
      uint32_t numberKeyPresses;
      bool pressed;
    };
    Button aux1 = {auxBtn1, 0, false};
    Button aux2 = {auxBtn2, 0, false};

    void IRAM_ATTR isr1(){
      aux1.pressed = true;
      target_velocity = target_velocity*(-1);
      Serial.println("Changing directions.. ");
    }

    void IRAM_ATTR isr2(){
      aux2.numberKeyPresses++;
      aux2.pressed = true;

      if((aux2.numberKeyPresses % 2) == 0)
      {
        target_velocity = 0;
        Serial.println("Stopping motor.. ");
      }
      else
      {
        target_velocity = 5;
        motor.enable();
        Serial.println("Starting motor.. ");
      }
    }


    void setup() {

      //motor demo stuff
      driver.voltage_power_supply = 3.3;
      driver.pwm_frequency = 20000;
      driver.voltage_limit = 4;
      driver.init();
      motor.linkDriver(&driver);
      motor.voltage_limit = 4;
      motor.controller = MotionControlType::velocity_openloop;
      motor.init();
      motor.disable();
      pinMode(aux1.PIN, INPUT_PULLUP); // Sets pin 14 on the ESP32 as an interrupt
      attachInterrupt(aux1.PIN, isr1, FALLING); // Triggers when aux1 is pulled to GND (button pressed)
      pinMode(aux2.PIN, INPUT_PULLUP); // Sets pin 13 on the ESP32 as an interrupt
      attachInterrupt(aux2.PIN, isr2, FALLING); // Triggers when aux2 is pulled to GND (button pressed)
      delay(100);

      Serial.begin(115200);
    }

    /////////////////////////////////////////////////////////////////////////
    void loop() { 

      // Button Press ISR
      if(aux1.pressed){ 
        aux1.pressed = false;
      }

      // Turning motor on and off
      if(aux2.pressed){ 
        aux2.pressed = false;
      }

      // open loop velocity movement
      // using motor.voltage_limit and motor.velocity_limit
      // Basic motor movement
      motor.move(target_velocity);

      // user communication
      command.run();

      delay(5);
    }

Running the Motor

By default, the motor should be disabled and spin freely. Users can utilize the user buttons 13 and 14 to control the motor.

Motor Overheating

When the motor is stopped, the motor driver is still enabled. Therefore, current is still running through the stator coils and holding the motor in place. After a few minutes, users may notice that the motor begins to heat up a bit.

If this becomes an issue, users can modify their code to disable the motor driver when the motor stops. This will prevent the motor from heating up, but the motor will spin freely as the motor driver is no longer engaged.

Modification

Modify the sketch and insert motor.disable(); between lines 80 - 81.

DC.ino
    /******************************************************************************
        IoT Motor Driver Example

        Written By:
            Madison Chodikov
            Eric Orosel
        Company: SparkFun Electronics   
        Date: September 1 2023

        This sketch is a stripped down version of the firmware that is preprogrammed
        on the IoT Motor Driver. It is based on the open loop, velocity motor control
        example from the SimpleFOC Arduino library.

        This sketch will spin the motor based on the button inputs:
            - Button 13: Starts/Stops the motor rotation
            - Button 14: When spinning, switches the direction of rotation

    ===============================================================================
        Products:
            IoT Brushless Motor Driver: https://www.sparkfun.com/products/22132

        Repository:
            https://github.com/sparkfun/SparkFun_IoT_Brushless_Motor_Driver
    ===============================================================================

        SparkFun code, firmware, and software is released under the MIT 
        License (http://opensource.org/licenses/MIT).

        Distributed as-is; no warranty is given.
    ******************************************************************************/

    #include <Wire.h>
    #include <SimpleFOC.h> //http://librarymanager/All#Simple%20FOC


    //GPIO
    #define auxBtn2   13
    #define auxBtn1   14  

    //driver
    #define uh16      16
    #define ul17      17
    #define vh18      18
    #define wh19      19
    #define vl23      23
    #define wl33      33
    #define curSense  32

    bool state = true;

    //motor driver
    BLDCMotor motor = BLDCMotor(7);
    BLDCDriver6PWM driver = BLDCDriver6PWM(uh16, ul17, vh18, vl23, wh19, wl33,  curSense);
    float target_velocity = 0.0;
    Commander command = Commander(Serial);
    void doTarget(char* cmd) { command.scalar(&target_velocity, cmd); }
    void doLimit(char* cmd) { command.scalar(&motor.voltage_limit, cmd); }

    //////////////////////motor demo stuff///////////////////////////
    struct Button{
      const uint8_t PIN;
      uint32_t numberKeyPresses;
      bool pressed;
    };
    Button aux1 = {auxBtn1, 0, false};
    Button aux2 = {auxBtn2, 0, false};

    void IRAM_ATTR isr1(){
      aux1.pressed = true;
      target_velocity = target_velocity*(-1);
      Serial.println("Changing directions.. ");
    }

    void IRAM_ATTR isr2(){
      aux2.numberKeyPresses++;
      aux2.pressed = true;

      if((aux2.numberKeyPresses % 2) == 0)
      {
        target_velocity = 0;
        Serial.println("Stopping motor.. ");
      }
      else
      {
        target_velocity = 5;
        motor.enable();
        Serial.println("Starting motor.. ");
      }
    }


    void setup() {

      //motor demo stuff
      driver.voltage_power_supply = 3.3;
      driver.pwm_frequency = 20000;
      driver.voltage_limit = 4;
      driver.init();
      motor.linkDriver(&driver);
      motor.voltage_limit = 4;
      motor.controller = MotionControlType::velocity_openloop;
      motor.init();
      motor.disable();
      pinMode(aux1.PIN, INPUT_PULLUP); // Sets pin 14 on the ESP32 as an interrupt
      attachInterrupt(aux1.PIN, isr1, FALLING); // Triggers when aux1 is pulled to GND (button pressed)
      pinMode(aux2.PIN, INPUT_PULLUP); // Sets pin 13 on the ESP32 as an interrupt
      attachInterrupt(aux2.PIN, isr2, FALLING); // Triggers when aux2 is pulled to GND (button pressed)
      delay(100);

      Serial.begin(115200);
    }

    /////////////////////////////////////////////////////////////////////////
    void loop() { 

      // Button Press ISR
      if(aux1.pressed){ 
        aux1.pressed = false;
      }

      // Turning motor on and off
      if(aux2.pressed){ 
        aux2.pressed = false;
      }

      // open loop velocity movement
      // using motor.voltage_limit and motor.velocity_limit
      // Basic motor movement
      motor.move(target_velocity);

      // user communication
      command.run();

      delay(5);
    }

Troubleshooting Tips

Need Help?

If you need technical assistance or more information on a product that is not working as you expected, we recommend heading on over to the SparkFun Technical Assistance page for some initial troubleshooting.

SparkFun Technical Assistance Page

If you can't find what you need there, the SparkFun Forums is a great place to search product forums and ask questions.

Account Registration Required

If this is your first visit to our forum, you'll need to create a Forum Account to post questions.

ESP32 Compile Error

If users run into an error similar to, fatal error: soc/soc_caps.h: No such file or directory, it may be due to an issue with the version of the ESP32 Arduino core that is installed in the Boards Manager. Users should make sure the have the latest version of the ESP32 Arduino core installed; or at least a version later than v2.0.1.

Info

For more information, please reference this forum post for the Simple FOC Arduino library.

Resources:

Product Resources

Additional Resources

🏭 Manufacturer's Resources

Analog Devices + Trinamic also provides great resources for the TMC6300 motor driver:

![QR code to the hookup guide](./assets/img/qr_code/hookup_guide.png){ .qr }

Background Resources

Below, are several articles, application notes, and other technical resources on 3-phase motors and utilizing a field-oriented control (FOC) scheme: