Library Setup
Arduino IDE
Most users may already be familiar with the Arduino IDE and its use. However, for those of you who have never heard the name Arduino before, feel free to check out the Arduino website. To get started with using the Arduino IDE, check out our tutorials below:
SparkFun u-blox Cellular Arduino Library
The SparkFun u-blox Cellular Arduino Library is a generic AT command-set library that works with multiple u-blox cellular modules that share the same AT Command Set. This includes the LARA-R6 on this board as well as the SARA-R5 and others. Most of the examples are generic and work with all modules but some require selecting a specific module to function properly.
Download the library through the Arduino Library Manager tool by searching for "SparkFun u-blox Cellular" and download the latest version. Users who prefer to install it manually can download it from the GitHub repository or by clicking the button below:
With the library installed, let's move on to taking a closer look at a few of the examples included in it.