Python Examples
Attention
These instructions are written for the XRP using the XRPCode IDE. However the setup process is very similar for MicroPython and CircuitPython on any other board, so you should be able to follow along with these instructions using your IDE of choice!
Download Examples
First, go to the Qwiic_OTOS_Py repository, open the examples folder, and download the example files you want to run.
Connect your XRP to your computer over USB, navigate to the XRPCode editor, and connect to your XRP. For usage information, see the XRPCode User Guide.
Upload the example files into the root directory (/), or directory of your choice, on the XRP. Begin by finding the Upload to XRP option:
Upload to XRP option in the File Menu
Select the files to upload:
Selecting the Files to Upload
Select the root directory (/), or directory of your choice, on the XRP:
Select the root directory (/)
Click the OK button and wait for the files to upload and save:
Updating
You should then see the examples in the Filesystem panel on the left:
Finding the examples in the FileSystem
Example 1: Basic Readings
This first example just does some basic measurements to make sure everything is hooked up correctly. Assuming you uploaded this example in the procedure above, double-click qwiic_otos_ex1_basic_readings.py in the Filesystem panel on the left:
qwiic_otos_ex1_basic_readings.py XRP File Location
Alternatively, you can expand the link below and copy and paste the code into a shiny new file:
Example 1 Python Code
#!/usr/bin/env python
#-------------------------------------------------------------------------------
# qwiic_otos_ex1_basic_readings.py
#
# This example demonstrates how to read the position and heading from the
# SparkFun Qwiic Optical Tracking Odometry Sensor (OTOS).
#
# This example should be used to verify that the OTOS is connected and
# functioning correctly. It will just print the position and heading tracked
# by the OTOS to the serial monitor. It is recommended that you check out the
# other examples before using the OTOS in your own project.
#-------------------------------------------------------------------------------
# Written by SparkFun Electronics, May 2024
#
# This python library supports the SparkFun Electroncis Qwiic ecosystem
#
# More information on Qwiic is at https://www.sparkfun.com/qwiic
#
# Do you like this library? Help support SparkFun. Buy a board!
#===============================================================================
# Copyright (c) 2023 SparkFun Electronics
#
# Permission is hereby granted, free of charge, to any person obtaining a copy
# of this software and associated documentation files (the "Software"), to deal
# in the Software without restriction, including without limitation the rights
# to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
# copies of the Software, and to permit persons to whom the Software is
# furnished to do so, subject to the following conditions:
#
# The above copyright notice and this permission notice shall be included in all
# copies or substantial portions of the Software.
#
# THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
# IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
# FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE
# AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
# LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
# OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
# SOFTWARE.
#===============================================================================
import qwiic_otos
import sys
import time
def runExample():
print("\nQwiic OTOS Example 1 - Basic Readings\n")
# Create instance of device
myOtos = qwiic_otos.QwiicOTOS()
# Check if it's connected
if myOtos.is_connected() == False:
print("The device isn't connected to the system. Please check your connection", \
file=sys.stderr)
return
# Initialize the device
myOtos.begin()
print("Ensure the OTOS is flat and stationary during calibration!")
for i in range(5, 0, -1):
print("Calibrating in %d seconds..." % i)
time.sleep(1)
print("Calibrating IMU...")
# Calibrate the IMU, which removes the accelerometer and gyroscope offsets
myOtos.calibrateImu()
# Reset the tracking algorithm - this resets the position to the origin,
# but can also be used to recover from some rare tracking errors
myOtos.resetTracking()
# Main loop
while True:
# Get the latest position, which includes the x and y coordinates, plus
# the heading angle
myPosition = myOtos.getPosition()
# Print measurement
print()
print("Position:")
print("X (Inches): {}".format(myPosition.x))
print("Y (Inches): {}".format(myPosition.y))
print("Heading (Degrees): {}".format(myPosition.h))
# Wait a bit so we don't spam the serial port
time.sleep(0.5)
# Alternatively, you can comment out the print and delay code above, and
# instead use the following code to rapidly refresh the data
# print("{}\t{}\t{}".format(myPosition.x, myPosition.y, myPosition.h))
# time.sleep(0.01)
if __name__ == '__main__':
try:
runExample()
except (KeyboardInterrupt, SystemExit) as exErr:
print("\nEnding Example")
sys.exit(0)
Then click the run button in the top right corner:
Run Button
You should see the following output in the Shell:
Example 1 Output
Move the sensor around to see how the coordinates change!
Example 2: Set Units
This example sets the desired units for linear and angular measurements. Can be either meters or inches for linear, and radians or degrees for angular. If not set, the default is inches and degrees. Note that this setting is not stored in the sensor, it's part of the library, so you need to set at the start of all your programs. Assuming you uploaded this example in the procedure above, double-click qwiic_otos_ex2_set_units.py in the Filesystem panel on the left:
qwiic_otos_ex2_set_units.py XRP File Location
Alternatively, you can expand the link below and copy and paste the code into a shiny new file and upload to the XRP as described above.
Example 2 Python Code
#!/usr/bin/env python
#-------------------------------------------------------------------------------
# qwiic_otos_ex2_set_units.py
#
# This example demonstrates how to change the units of the SparkFun Qwiic
# Optical Tracking Odometry Sensor (OTOS).
# The OTOS library defaults to inches and degrees, but you can change the
# units to suit the needs of your project.
#-------------------------------------------------------------------------------
# Written by SparkFun Electronics, May 2024
#
# This python library supports the SparkFun Electroncis Qwiic ecosystem
#
# More information on Qwiic is at https://www.sparkfun.com/qwiic
#
# Do you like this library? Help support SparkFun. Buy a board!
#===============================================================================
# Copyright (c) 2023 SparkFun Electronics
#
# Permission is hereby granted, free of charge, to any person obtaining a copy
# of this software and associated documentation files (the "Software"), to deal
# in the Software without restriction, including without limitation the rights
# to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
# copies of the Software, and to permit persons to whom the Software is
# furnished to do so, subject to the following conditions:
#
# The above copyright notice and this permission notice shall be included in all
# copies or substantial portions of the Software.
#
# THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
# IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
# FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE
# AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
# LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
# OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
# SOFTWARE.
#===============================================================================
import qwiic_otos
import sys
import time
def runExample():
print("\nQwiic OTOS Example 2 - Set Units\n")
# Create instance of device
myOtos = qwiic_otos.QwiicOTOS()
# Check if it's connected
if myOtos.is_connected() == False:
print("The device isn't connected to the system. Please check your connection", \
file=sys.stderr)
return
# Initialize the device
myOtos.begin()
print("Ensure the OTOS is flat and stationary during calibration!")
for i in range(5, 0, -1):
print("Calibrating in %d seconds..." % i)
time.sleep(1)
print("Calibrating IMU...")
# Calibrate the IMU, which removes the accelerometer and gyroscope offsets
myOtos.calibrateImu()
# Set the desired units for linear and angular measurements. Can be either
# meters or inches for linear, and radians or degrees for angular. If not
# set, the default is inches and degrees. Note that this setting is not
# stored in the sensor, it's part of the library, so you need to set at the
# start of all your programs.
myOtos.setLinearUnit(myOtos.kLinearUnitMeters)
# myOtos.setLinearUnit(myOtos.kLinearUnitInches)
myOtos.setAngularUnit(myOtos.kAngularUnitRadians)
# myOtos.setAngularUnit(myOtos.kAngularUnitDegrees)
# Reset the tracking algorithm - this resets the position to the origin,
# but can also be used to recover from some rare tracking errors
myOtos.resetTracking()
# Main loop
while True:
# Get the latest position, which includes the x and y coordinates, plus
# the heading angle
myPosition = myOtos.getPosition()
# Print measurement
print()
print("Position:")
print("X (Meters): {}".format(myPosition.x))
print("Y (Meters): {}".format(myPosition.y))
print("Heading (Radians): {}".format(myPosition.h))
# Wait a bit so we don't spam the serial port
time.sleep(0.5)
if __name__ == '__main__':
try:
runExample()
except (KeyboardInterrupt, SystemExit) as exErr:
print("\nEnding Example")
sys.exit(0)
Notice the following code snippet - this is the section of code that allows you to choose your units:
Code Snippet to Change Units
Then click the run button in the top right corner:
Run Button
You should see the following output in the Shell:
Example 2 Output
Example 3: Calibration
Warning
As of firmware version 1.0, these calibration values will be lost after a power cycle, so you will need to set them each time you power up the sensor.
The data from the OTOS will likely have minor scaling errors that can be calibrated out. This is especially important for the angular scalar, because an incorrect angle measurement causes the linear measurements to be rotated by the wrong angle in the firmware, which can lead to very inaccurate tracking. Assuming you uploaded this example in the procedure above, double-click qwiic_otos_ex3_calibration.py in the Filesystem panel on the left:
qwiic_otos_ex3_calibration.py XRP File Location
Alternatively, you can expand the link below and copy and paste the code into a shiny new file and upload to the XRP as described above.
Example 3 Python Code
#!/usr/bin/env python
#-------------------------------------------------------------------------------
# qwiic_otos_ex3_calibration.py
#
# This example demonstrates how to calibrate the SparkFun Qwiic Optical
# Tracking Odometry Sensor (OTOS).
# This example should be used to calibrate the linear and angular scalars of
# the OTOS to get the most accurate tracking performance. The linear scalar
# can be used to compensate for scaling issues with the x and y measurements,
# while the angular scalar can be used to compensate for scaling issues with
# the heading measurement. Note that if the heading measurement is off, that
# can also cause the x and y measurements to be off, so it's recommended to
# calibrate the angular scalar first.
#-------------------------------------------------------------------------------
# Written by SparkFun Electronics, May 2024
#
# This python library supports the SparkFun Electroncis Qwiic ecosystem
#
# More information on Qwiic is at https:#www.sparkfun.com/qwiic
#
# Do you like this library? Help support SparkFun. Buy a board!
#===============================================================================
# Copyright (c) 2023 SparkFun Electronics
#
# Permission is hereby granted, free of charge, to any person obtaining a copy
# of this software and associated documentation files (the "Software"), to deal
# in the Software without restriction, including without limitation the rights
# to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
# copies of the Software, and to permit persons to whom the Software is
# furnished to do so, subject to the following conditions:
#
# The above copyright notice and this permission notice shall be included in all
# copies or substantial portions of the Software.
#
# THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
# IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
# FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE
# AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
# LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
# OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
# SOFTWARE.
#===============================================================================
import qwiic_otos
import sys
import time
def runExample():
print("\nQwiic OTOS Example 3 - Calibration\n")
# Create instance of device
myOtos = qwiic_otos.QwiicOTOS()
# Check if it's connected
if myOtos.is_connected() == False:
print("The device isn't connected to the system. Please check your connection", \
file=sys.stderr)
return
# Initialize the device
myOtos.begin()
print("Ensure the OTOS is flat and stationary during calibration!")
for i in range(5, 0, -1):
print("Calibrating in %d seconds..." % i)
time.sleep(1)
print("Calibrating IMU...")
# The IMU on the OTOS includes a gyroscope and accelerometer, which could
# have an offset. Note that as of firmware version 1.0, the calibration
# will be lost after a power cycle; the OTOS performs a quick calibration
# when it powers up, but it is recommended to perform a more thorough
# calibration at the start of all your programs. Note that the sensor must
# be completely stationary and flat during calibration! When calling
# calibrateImu(), you can specify the number of samples to take and whether
# to wait until the calibration is complete. If no parameters are provided,
# it will take 255 samples and wait until done; each sample takes about
# 2.4ms, so about 612ms total
myOtos.calibrateImu()
# Alternatively, you can specify the number of samples and whether to wait
# until it's done. If you don't want to wait, you can asynchronously check
# how many samples remain with the code below. Once zero samples remain,
# the calibration is done!
# myOtos.calibrateImu(255, False)
# done = False
# while(done == False):
# # Check how many samples remain
# samplesRemaining = myOtos.getImuCalibrationProgress()
# # If 0 samples remain, the calibration is done
# if(samplesRemaining == 0):
# done = True
# Here we can set the linear and angular scalars, which can compensate for
# scaling issues with the sensor measurements. Note that as of firmware
# version 1.0, these values will be lost after a power cycle, so you will
# need to set them each time you power up the sensor. They can be any value
# from 0.872 to 1.127 in increments of 0.001 (0.1%). It is recommended to
# first set both scalars to 1.0, then calibrate the angular scalar, then
# the linear scalar. To calibrate the angular scalar, spin the robot by
# multiple rotations (eg. 10) to get a precise error, then set the scalar
# to the inverse of the error. Remember that the angle wraps from -180 to
# 180 degrees, so for example, if after 10 rotations counterclockwise
# (positive rotation), the sensor reports -15 degrees, the required scalar
# would be 3600/3585 = 1.004. To calibrate the linear scalar, move the
# robot a known distance and measure the error; do this multiple times at
# multiple speeds to get an average, then set the linear scalar to the
# inverse of the error. For example, if you move the robot 100 inches and
# the sensor reports 103 inches, set the linear scalar to 100/103 = 0.971
myOtos.setLinearScalar(1.0)
myOtos.setAngularScalar(1.0)
# Reset the tracking algorithm - this resets the position to the origin,
# but can also be used to recover from some rare tracking errors
myOtos.resetTracking()
# Main loop
while True:
# Get the latest position, which includes the x and y coordinates, plus
# the heading angle
myPosition = myOtos.getPosition()
# Print measurement
print()
print("Position:")
print("X (Inches): {}".format(myPosition.x))
print("Y (Inches): {}".format(myPosition.y))
print("Heading (Degrees): {}".format(myPosition.h))
# Wait a bit so we don't spam the serial port
time.sleep(0.5)
if __name__ == '__main__':
try:
runExample()
except (KeyboardInterrupt, SystemExit) as exErr:
print("\nEnding Example")
sys.exit(0)
Then click the run button in the top right corner:
Run Button
Calibrating your bot requires you to move it around a bit. First, set both scalars to 1.0, then calibrate the angular scalar, then the linear scalar.
To calibrate the angular scalar, spin the robot by multiple rotations (eg. 10) to get a precise error, then set the scalar to the inverse of the error. Remember that the angle wraps from -180 to 180 degrees, so for example, if after 10 rotations counterclockwise(positive rotation), the sensor reports -15 degrees, the required scalar would be 3600/3585 = 1.004.
Rotating the Optical Tracking Odometry Sensor
To calibrate the linear scalar, move the robot a known distance and measure the error; do this multiple times at multiple speeds to get an average, then set the linear scalar to the inverse of the error. For example, if you move the robot 100 inches and the sensor reports 103 inches, set the linear scalar to 100/103 = 0.971.
Moving the Optical Tracking Odometry Sensor
Example 4: SetOffsetAndPosition
This example shows how to set the offset for the sensor relative to the center of the robot. The units default to inches and degrees, but if you want to use different units, make sure you specify them before setting the offset. Without setting the offset, the OTOS will report the coordinates of itself. If the offset is set, the OTOS will instead report the coordinates of the center of your robot.
Note that the OTOS typically starts tracking from the origin, but if your robot starts at some other location, or you have another source of location information from another sensor that's more accurate, you can send the current location to the OTOS and it will continue tracking from there.
Warning
As of firmware version 1.0, these values will be lost after a power cycle, so you will need to set them each time you power up the sensor.
Assuming you uploaded this example in the procedure above, double-click qwiic_otos_ex4_set_offsets_and_position.py in the Filesystem panel on the left:
qwiic_otos_ex4_set_offsets_and_position.py XRP File Location
Alternatively, you can expand the link below and copy and paste the code into a shiny new file and upload to the XRP as described above.
Example 4 Python Code
#!/usr/bin/env python
#-------------------------------------------------------------------------------
# qwiic_otos_ex4_set_offsets_and_position.py
#
# This example demonstrates how to set the offset and position of the SparkFun
# Qwiic Optical Tracking Odometry Sensor (OTOS).
# If your OTOS is mounted to a robot and is not centered, you can specify the
# offset for the sensor relative to the center of the robot; rather than
# returning the position of the sensor, the OTOS will calculate and return the
# position of the robot's center. If you know where your robot is located,
# such as the starting location or from another sensor, you can send that
# position to the OTOS and it will continue to track from there.
#-------------------------------------------------------------------------------
# Written by SparkFun Electronics, May 2024
#
# This python library supports the SparkFun Electroncis Qwiic ecosystem
#
# More information on Qwiic is at https:#www.sparkfun.com/qwiic
#
# Do you like this library? Help support SparkFun. Buy a board!
#===============================================================================
# Copyright (c) 2023 SparkFun Electronics
#
# Permission is hereby granted, free of charge, to any person obtaining a copy
# of this software and associated documentation files (the "Software"), to deal
# in the Software without restriction, including without limitation the rights
# to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
# copies of the Software, and to permit persons to whom the Software is
# furnished to do so, subject to the following conditions:
#
# The above copyright notice and this permission notice shall be included in all
# copies or substantial portions of the Software.
#
# THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
# IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
# FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE
# AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
# LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
# OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
# SOFTWARE.
#===============================================================================
import qwiic_otos
import sys
import time
def runExample():
print("\nQwiic OTOS Example 4 - Set Offsets and Position\n")
# Create instance of device
myOtos = qwiic_otos.QwiicOTOS()
# Check if it's connected
if myOtos.is_connected() == False:
print("The device isn't connected to the system. Please check your connection", \
file=sys.stderr)
return
# Initialize the device
myOtos.begin()
print("Ensure the OTOS is flat and stationary during calibration!")
for i in range(5, 0, -1):
print("Calibrating in %d seconds..." % i)
time.sleep(1)
print("Calibrating IMU...")
# Calibrate the IMU, which removes the accelerometer and gyroscope offsets
myOtos.calibrateImu()
# Assuming you've mounted your sensor to a robot and it's not centered,
# you can specify the offset for the sensor relative to the center of the
# robot. The units default to inches and degrees, but if you want to use
# different units, specify them before setting the offset! Note that as of
# firmware version 1.0, these values will be lost after a power cycle, so
# you will need to set them each time you power up the sensor. For example,
# if the sensor is mounted 5 inches to the left (negative X) and 10 inches
# forward (positive Y) of the center of the robot, and mounted 90 degrees
# clockwise (negative rotation) from the robot's orientation, the offset
# would be {-5, 10, -90}. These can be any value, even the angle can be
# tweaked slightly to compensate for imperfect mounting (eg. 1.3 degrees).
offset = qwiic_otos.Pose2D(-5, 10, -90)
myOtos.setOffset(offset)
# Reset the tracking algorithm - this resets the position to the origin,
# but can also be used to recover from some rare tracking errors
myOtos.resetTracking()
# After resetting the tracking, the OTOS will report that the robot is at
# the origin. If your robot does not start at the origin, or you have
# another source of location information (eg. vision odometry), you can set
# the OTOS location to match and it will continue to track from there.
currentPosition = qwiic_otos.Pose2D(0, 0, 0)
myOtos.setPosition(currentPosition)
# Main loop
while True:
# Get the latest position, which includes the x and y coordinates, plus
# the heading angle
myPosition = myOtos.getPosition()
# Print measurement
print()
print("Position:")
print("X (Inches): {}".format(myPosition.x))
print("Y (Inches): {}".format(myPosition.y))
print("Heading (Degrees): {}".format(myPosition.h))
# Wait a bit so we don't spam the serial port
time.sleep(0.5)
if __name__ == '__main__':
try:
runExample()
except (KeyboardInterrupt, SystemExit) as exErr:
print("\nEnding Example")
sys.exit(0)
Then click the run button in the top right corner:
Run Button
The offset values depend on the axes conventions that you choose for your robot. Below are 2 animations showing ENU (East-North-Up) and NWU (North-West-Up) axes conventions with the XRP, and the required offset values for the indicated location of the OTOS for each. In this case, the sensor is mounted 2 inches to the right ("East"), 4 inches forward ("North"), and with the x-axis to the right ("East").
OTOS offsets with ENU axes conventions
OTOS offsets with NWU axes conventions
With the ENU convention, the OTOS axes are aligned with the robot axes, so the offset angle is zero. With the NWU convention, the OTOS axes are rotated -90 degrees (right-hand rule about the "up" z-axis) relative to the robot axes. So the offset values would be {2, 4, 0} for ENU and {4, -2, -90} for NWU. These can be any value, even the angle can be tweaked slightly to compensate for imperfect mounting (eg. 1.3 degrees).
These four examples cover the basics - there are more examples to explore in the GitHub Repo!