Arduino Examples
Now that we have our library and board add-on installed, we can start experimenting with the breakout board. For the scope of this tutorial, we will highlight the examples provided in the GitHub hardware repo to get started.
Example 1: Read Buttons, Write LEDs
From your downloads, open the example labeled as Example1-ReadButtons_WriteLEDs.ino. This example reads the button presses and writes to the non-addressable LED using the PCA9554 I/O I2C Expander.
For users using an Arduino microcontroller, select your board in the Tools menu (in our case the SparkFun ESP32 IoT RedBoard) and the correct Port it enumerated on.
You can also copy or paste the code as shown below. Then click "Upload".
/*
Using the Qwiic Directional Pad
By: Nathan Seidle
SparkFun Electronics
Date: October 8th, 2024
License: This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).
Feel like supporting our work? Buy a board from SparkFun!
https://www.sparkfun.com/products/14733
This example demonstrates how to use pinMode and digitalRead/Write to read the directional pad and turn
on/off the RGB LED channels.
Hardware Connections:
Plug the Qwiic board to your Arduino/ESP32 or other
Press the buttons
Watch each LED turn on one-at-a-time
*/
#include <SparkFun_I2C_Expander_Arduino_Library.h> // Click here to get the library: http://librarymanager/All#SparkFun_I2C_Expander_Arduino_Library
SFE_PCA95XX io; // Defaults to the PCA9554 at I2C address 0x20
int buttonUp = 0;
int buttonDown = 1;
int buttonRight = 2;
int buttonLeft = 3;
int buttonCenter = 4;
int ledBlue = 5;
int ledGreen = 6;
int ledRed = 7;
void setup()
{
Serial.begin(115200);
delay(250);
Serial.println("Qwiic Directional Pad Example");
Wire.begin();
// Initialize the PCA9554, default address = 0x20
if (io.begin() == false) //Device Address, Number of GPIO
{
Serial.println("PCA9554 not detected. Please check wiring. Freezing...");
while (1)
;
}
io.pinMode(buttonUp, INPUT);
io.pinMode(buttonDown, INPUT);
io.pinMode(buttonLeft, INPUT);
io.pinMode(buttonRight, INPUT);
io.pinMode(buttonCenter, INPUT);
io.pinMode(ledRed, OUTPUT);
io.pinMode(ledGreen, OUTPUT);
io.pinMode(ledBlue, OUTPUT);
redOff();
greenOff();
blueOff();
Serial.println("Qwiic Directional Pad online!");
}
void loop()
{
Serial.print("Button: ");
if (io.digitalRead(buttonUp) == LOW)
{
Serial.print("Up");
redOn();
greenOff();
blueOff();
}
else if (io.digitalRead(buttonDown) == LOW)
{
Serial.print("Down");
redOff();
greenOn();
blueOff();
}
else if (io.digitalRead(buttonLeft) == LOW)
{
Serial.print("Left");
redOn();
greenOff();
blueOn();
}
else if (io.digitalRead(buttonRight) == LOW)
{
Serial.print("Right");
redOff();
greenOn();
blueOn();
}
else if (io.digitalRead(buttonCenter) == LOW)
{
Serial.print("Center");
redOn();
greenOn();
blueOn();
}
else
{
Serial.print(" None");
redOff();
greenOff();
blueOff();
}
Serial.println();
delay(100);
}
void redOn()
{
io.digitalWrite(ledRed, LOW);
}
void redOff()
{
io.digitalWrite(ledRed, HIGH);
}
void greenOn()
{
io.digitalWrite(ledGreen, LOW);
}
void greenOff()
{
io.digitalWrite(ledGreen, HIGH);
}
void blueOn()
{
io.digitalWrite(ledBlue, LOW);
}
void blueOff()
{
io.digitalWrite(ledBlue, HIGH);
}
After uploading the code, open the Serial Monitor or terminal emulator of your choice with the baud rate set to 115200. Press down on any of the buttons. You will notice a serial output indicating which button was pressed in the Arduino Serial Monitor. Looking to the board, you will notice the LED changing color with respect to the button press.
Example 2: Interrupt Pin
Note
Example 3 from the SparkFun I2C Expander Arduino Library uses the IoT RedBoard - ESP32's pin 14 for the interrupt. The example in this tutorial is slightly different and uses pin 4 for the interrupt.
From your downloads, open the example labeled as Example2_InterruptReadButtons_WriteLEDs.ino. This example reads the button presses and writes to the non-addressable LED whenever there is an interrupt using the PCA9554 I/O I2C Expander. Make sure to connect the Qwiic Directional Pad's interrupt pin to the IoT RedBoard's pin 4.
For users using an Arduino microcontroller, select your board in the Tools menu (in our case the SparkFun ESP32 IoT RedBoard) and the correct Port it enumerated on.
You can also copy or paste the code as shown below. Then click "Upload".
/*
Using the PCA9554 with Interrupts
Modified by: Ho Yun "Bobby" Chan
Orignally Written By: Nathan Seidle
SparkFun Electronics
Date: November 22nd, 2024
License: This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).
Feel like supporting our work? Buy a board from SparkFun!
https://www.sparkfun.com/products/17047 - Qwiic GPIO
https://www.sparkfun.com/products/26784 - Qwiic Power Switch
https://www.sparkfun.com/products/26851 - Qwiic Directional Pad
This example demonstrates how to use interrupts to check for new pin changes on the Qwiic Directional Pad
and turn on/off the RGB LED channels
Hardware Connections:
Plug the Qwiic Directional Pad into a Qwiic enabled board (SparkFun Thing Plus C, RedBoard, RedBoard IoT, etc)
If you don't have a platform with a Qwiic connection use the SparkFun Qwiic Breadboard Jumper (https://www.sparkfun.com/products/17912)
Connect a wire from a GPIO pin that is interrupt capable to the !INT pin on the Qwiic Directional Pad
Open the serial monitor at 115200 baud to see the output.
*/
#include <SparkFun_I2C_Expander_Arduino_Library.h> // Click here to get the library: http://librarymanager/All#SparkFun_I2C_Expander_Arduino_Library
//SFE_PCA95XX io(PCA95XX_PCA9534); // Create a PCA9534 - Has interrupt pin
//SFE_PCA95XX io(PCA95XX_PCA9536); // Create a PCA9536 - Has optional interrupt pin
//SFE_PCA95XX io(PCA95XX_PCA9537); // Create a PCA9537 - Has interrupt pin
SFE_PCA95XX io(PCA95XX_PCA9554); // Create a PCA9554 - Has interrupt pin
//SFE_PCA95XX io(PCA95XX_PCA9556); // Create a PCA9556 - No interrupt pin / Not compatible with this code
//SFE_PCA95XX io(PCA95XX_PCA9557); // Create a PCA9557 - No interrupt pin / Not compatible with this code
int buttonUp = 0;
int buttonDown = 1;
int buttonRight = 2;
int buttonLeft = 3;
int buttonCenter = 4;
int ledBlue = 5;
int ledGreen = 6;
int ledRed = 7;
int gpioExpander_interrupt = 4; //INT of PCA9554 is connected to ESP pin 4. Goes low when an input pin changes.
bool buttonPressed = false;
//Interrupt that is called when INT pin goes low
void IRAM_ATTR gpioExpanderISR() {
buttonPressed = true;
}
void setup() {
Serial.begin(115200);
delay(250);
Serial.println("Qwiic Directional Pad Example");
Wire.begin();
// Initialize the PCA95xx with its default I2C address
if (io.begin() == false) {
Serial.println("PCA9554 not detected. Please check wiring. Freezing...");
while (1)
;
}
pinMode(gpioExpander_interrupt, INPUT_PULLUP);
io.pinMode(buttonUp, INPUT);
io.pinMode(buttonDown, INPUT);
io.pinMode(buttonLeft, INPUT);
io.pinMode(buttonRight, INPUT);
io.pinMode(buttonCenter, INPUT);
io.pinMode(ledRed, OUTPUT);
io.pinMode(ledGreen, OUTPUT);
io.pinMode(ledBlue, OUTPUT);
redOff();
greenOff();
blueOff();
Serial.println("Qwiic Directional Pad online!");
attachInterrupt(gpioExpander_interrupt, gpioExpanderISR, CHANGE);
}
void loop() {
//Wait for interrupt to fire
if (buttonPressed == true) {
Serial.println("Interrupt! ");
//Get all the pins in one read to save time
uint8_t currentState = io.getInputRegister();
// Pins are pulled high so when we see low, button is being pressed
if ((currentState & (1 << buttonUp)) == 0) {
Serial.println("Up");
//RED
redOn();
greenOff();
blueOff();
} else if ((currentState & (1 << buttonDown)) == 0) {
Serial.println("Down");
//GREEN
redOff();
greenOn();
blueOff();
} else if ((currentState & (1 << buttonLeft)) == 0) {
Serial.println("Left");
//MAGENTA
redOn();
greenOff();
blueOn();
} else if ((currentState & (1 << buttonRight)) == 0) {
Serial.println("Right");
//CYAN
redOff();
greenOn();
blueOn();
} else if ((currentState & (1 << buttonCenter)) == 0) {
Serial.println("Center");
//WHITE
redOn();
greenOn();
blueOn();
} else {
Serial.println(" None");
//OFF
redOff();
greenOff();
blueOff();
}
buttonPressed = false;
}
}
void redOn() {
io.digitalWrite(ledRed, LOW);
}
void redOff() {
io.digitalWrite(ledRed, HIGH);
}
void greenOn() {
io.digitalWrite(ledGreen, LOW);
}
void greenOff() {
io.digitalWrite(ledGreen, HIGH);
}
void blueOn() {
io.digitalWrite(ledBlue, LOW);
}
void blueOff() {
io.digitalWrite(ledBlue, HIGH);
}
After uploading the code, open the Serial Monitor or terminal emulator of your choice with the baud rate set to 115200. Press down on any of the buttons. You will notice a serial output indicating which button was pressed in the Arduino Serial Monitor whenever there is a button press. Looking to the board, you will notice the LED changing color with respect to the button press.