Drawing Settings/State
Methods for setting the drawing state of the library.
setFont()
This method is called to set the current font in the library. The current font is used when calling the text() method on this device.
The default font for the device is 5x7.
| Parameter | Type | Description |
|---|---|---|
theFont |
QwiicFont |
The font to set as current in the device |
theFont |
QwiicFont* |
Pointer to the font to set as current in the device. |
For the library, fonts are added to your program by including them via include files which are part of this library.
The following fonts are included:
| Font | Include File | Font Variable | Description |
|---|---|---|---|
| 5x7 | <res/qw_fnt_5x7.h> |
QW_FONT_5X7 |
A full, 5 x 7 font |
| 31x48 | <res/qw_fnt_31x48.h> |
QW_FONT_31X48 |
A full, 31 x 48 font |
| Seven Segment | <res/qw_fnt_7segment.h> |
QW_FONT_7SEGMENT |
Numbers only |
| 8x16 | <res/qw_fnt_8x16.h> |
QW_FONT_8X16 |
A full, 8 x 16 font |
| Large Numbers | <res/qw_fnt_largenum.h> |
QW_FONT_LARGENUM |
Numbers only |
For each font, the font variables are objects with the following attributes:
| Attribute | Value |
|---|---|
width |
The font width in pixels |
height |
The font height in pixels |
start |
The font start character offset |
n_chars |
The number of characters |
map_width |
The width of the font map |
Example use of a font object attribute:
getFont()
This method returns the current font for the device.
| Parameter | Type | Description |
|---|---|---|
| return value | QwiicFont* |
A pointer to the current font. See setFont() for font object details. |
getFontName()
This method returns the height in pixels of a provided String based on the current device font.
| Parameter | Type | Description |
|---|---|---|
| return value | String | The name of the current font. |
getStringWidth()
This method returns the width in pixels of a provided String based on the current device font.
| Parameter | Type | Description |
|---|---|---|
| text | String |
The string used to determine width |
| return value | unsigned int |
The width of the provide string, as determined using the current font. |
getStringHeight()
This method returns the height in pixels of a provided String based on the current device font.
| Parameter | Type | Description |
|---|---|---|
| text | String |
The string used to determine height |
| return value | unsigned int |
The height of the provide string, as determined using the current font. |
setDrawMode()
This method sets the current draw mode for the library. The draw mode determines how pixels are set on the screen during drawing operations.
| Parameter | Type | Description |
|---|---|---|
| rop | grRasterOp_t |
The raster operation (ROP) to set the graphics system to. |
Raster operations device how source (pixels to draw) are represented on the destination device. The available Raster Operation (ROP) codes are:
| ROP Code | Description |
|---|---|
| grROPCopy | default Drawn pixel values are copied to the device screen |
| grROPNotCopy | A not operation is applied to the source value before copying to screen |
| grROPNot | A not operation is applied to the destination (screen) value |
| grROPXOR | A XOR operation is performed between the source and destination values |
| grROPBlack | A value of 0, or black is drawn to the destination |
| grROPWhite | A value of 1, or black is drawn to the destination |
getDrawMode()
This method returns the current draw mode for the library. The draw mode determines how pixels are set on the screen during drawing operations.
| Parameter | Type | Description |
|---|---|---|
| return value | grRasterOp_t |
The current aster operation (ROP) of the graphics system. |