Software Setup
Installation
Arduino
This guide assumes you are using the latest version of the Arduino IDE on your desktop. The following resources available at SparkFun provide the details on setting up and configuring Arduino to use this library.
The SparkFun Qwiic OLED Arduino Library is available within in the Arduino library manager, which is launched via the Sketch > Include Libraries > Manage Libraries … menu option in the Arduino IDE. Just search for SparkFun Qwiic OLED Library.
Note
If you've never connected a USB-to-serial converter to your computer before, you may need to install drivers. The drivers will depend on what is populated on your Arduino development board. Check out the following tutorials for help with the installation.
General Use Pattern
After installing this library in your local Arduino environment, begin with a standard Arduino sketch, and include the header file for this library.
The next step is to declare the object for the SparkFun qwiic OLED device used. Like most Arduino sketches, this is done at a global scope (after the include file declaration), not within the setup() or loop() functions.
The user selects from one of the following classes:
| Class | Qwiic OLED Device |
|---|---|
QwiicMicroOLED |
SparkFun Qwiic Micro OLED |
QwiicNarrowOLED |
SparkFun Qwiic OLED Display (128x32) |
QwiicTransparentOLED |
SparkFun Transparent Graphical OLED |
Qwiic1in3OLED |
SparkFun Qwiic OLED 1.3" Display (128x32) |
For this example, the Qwiic Micro OLED is used.
In the setup() function of this sketch, like all of the SparkFun qwiic libraries, the device is initialized by calling the begin() method. This method returns a value of true on success, or false on failure.
int width, height; // global variables for use in the sketch
void setup()
{
Serial.begin(115200);
if(!myOLED.begin()){
Serial.println("Device failed to initialize");
while(1); // halt execution
}
Serial.println("Device is initialized");
}
Now that the library is initialized, the desired graphics are drawn. Here we erase the screen and draw simple series of lines that originate at the screen origin and fan out across the height of the display.
Note
Graphics are not send to the OLED device when drawn. Updates are only sent to the device when the display() method is called. This minimizes data transfers to the OLED device, delivering a responsive display response.
myOLED.erase(); // Erase the screen
myOLED.display(); // Send erase to device
delay(1000); // Slight pause
// Draw our lines from point (0,0) to (i, screen height)
for(int i=0; i < width; i+= 6){
myOLED.line(0, 0, i, height-1); // draw the line
myOLED.display(); // Send the new line to the device for display
}
Library Provided Examples
The SparkFun Qwiic OLED Arduino Library, includes a wide variety of examples. These are available from the Examples menu of the Arduino IDE, and in the examplesfolder of this repository.
For a detailed description of the examples, see the Examples section of the documentation.