![]() |
SparkFun Optical Tracking Odometry Sensor
v1.0.2-11-gb69b326
Library for the SparkFun Optical Tracking Odometry Sensor
|
Status register bit fields. More...
#include <sfDevOTOS.h>
Public Attributes | |
| struct { | |
| uint8_t warnTiltAngle: 1 | |
| Returns 1 if the tilt angle threshold has been exceeded. While set, the accelerometer data is ignored. More... | |
| uint8_t warnOpticalTracking: 1 | |
| Returns 1 if the optical tracking is unreliable. While set, only the IMU data is used for tracking unless warnTiltAngle is set. More... | |
| uint8_t reserved: 4 | |
| Reserved bits, do not use. More... | |
| uint8_t errorPaa: 1 | |
| Returns 1 if the optical sensor has a fatal error. More... | |
| uint8_t errorLsm: 1 | |
| Returns 1 if the IMU has a fatal error. More... | |
| }; | |
| uint8_t | value |
| Raw register value. More... | |
Status register bit fields.
| struct { ... } sfe_otos_status_t::@7 |
| uint8_t sfe_otos_status_t::errorLsm |
Returns 1 if the IMU has a fatal error.
| uint8_t sfe_otos_status_t::errorPaa |
Returns 1 if the optical sensor has a fatal error.
| uint8_t sfe_otos_status_t::reserved |
Reserved bits, do not use.
| uint8_t sfe_otos_status_t::value |
Raw register value.
| uint8_t sfe_otos_status_t::warnOpticalTracking |
Returns 1 if the optical tracking is unreliable. While set, only the IMU data is used for tracking unless warnTiltAngle is set.
| uint8_t sfe_otos_status_t::warnTiltAngle |
Returns 1 if the tilt angle threshold has been exceeded. While set, the accelerometer data is ignored.