Arduino Example
Now that we have our library and board add-on installed, we can start experimenting with the breakout board. For the scope of this tutorial, we will highlight the example in the Arduino Library to get started.
Upload Arduino Example
After unzipping the compressed files, navigate to the example: File > Examples > SparkFun Qwiic Power Switch Arduino Library > Example1_PowerOnOff. This example allows you to toggle power and isolate the I2C lines for the OUT port through a serial terminal. The example also allows you to read GPIO1 and GPIO2.
For users using an Arduino microcontroller, select your board in the Tools menu (in our case the SparkFun ESP32 Thing Plus C) and the correct Port it enumerated on.
You can also copy or paste the code as shown below. Then click "Upload".
/*
Using the Qwiic Power Switch
By: Paul Clark (PaulZC)
Date: April 23rd, 2020
Based extensively on:
Using the PCA9536 -- Digital Output
By: Jim Lindblom
SparkFun Electronics
Date: May 4, 2018
License: This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).
This example demonstrates how to use the Qwiic Power Switch and read the additional GPIO pins
Hardware Connections:
Attach your Arduino to the Qwiic Power Switch IN
Plug your Qwiic device into the Qwiic Power Switch OUT
https://www.sparkfun.com/products/15081
*/
#include <Wire.h>
#include <SparkFun_Qwiic_Power_Switch_Arduino_Library.h>
QWIIC_POWER mySwitch;
void setup(void)
{
Serial.begin(115200);
while (!Serial)
; //Wait for user to open terminal
Serial.println(F("Qwiic Power Switch Example"));
Wire.begin();
if (mySwitch.begin() == false) //Connect to the power switch using Wire port
{
Serial.println(F("Qwiic Power Switch not detected at default I2C address. Please check wiring. Freezing."));
while (1)
;
}
// Configure GPIO1 and GPIO2 as INPUT
mySwitch.pinMode(1, INPUT);
mySwitch.pinMode(2, INPUT);
Serial.println(F("1) Enable power and I2C"));
Serial.println(F("2) Disable power and I2C"));
Serial.println(F("3) Enable I2C isolation"));
Serial.println(F("4) Disable I2C isolation"));
}
void loop()
{
if (Serial.available())
{
byte incoming = Serial.read();
if (incoming == '1')
{
// Switch the power on
mySwitch.powerOn();
Serial.println(F("Power is ON. I2C isolation is disabled."));
}
else if (incoming == '2')
{
// Switch the power off
mySwitch.powerOff();
Serial.println(F("Power is OFF. I2C isolation is enabled."));
}
else if (incoming == '3')
{
// Enable I2C isolation = I2C bus _is_ isolated
mySwitch.isolationOn();
Serial.println(F("I2C isolation enabled. I2C is isolated."));
}
else if (incoming == '4')
{
// Disable I2C isolation = I2C bus _is not_ isolated
mySwitch.isolationOff();
Serial.println(F("I2C isolation disabled. I2C is not isolated."));
}
// Read and print the GPIO1/GPIO2 state
Serial.print(F("GPIO1 is: "));
Serial.println(mySwitch.digitalRead(1));
Serial.print(F("GPIO2 is: "));
Serial.println(mySwitch.digitalRead(2));
// Read any extra Serial bytes (e.g. CR or LF)
while (Serial.available() > 0)
{
Serial.read();
}
}
}
Tip
Instead of reading GPIO1 and GPIO2, you can write to the GPIO pins to set the pins HIGH or LOW. You will need to change the following lines of code in the setup() and loop() functions where the GPIO1 and GPIO2 are initialized and read.
setup(){
.
.
.
// Configure GPIO1 and GPIO2 as INPUT
mySwitch.pinMode(1, INPUT);
mySwitch.pinMode(2, INPUT);
.
.
.
}
void loop() {
.
.
.
// Read and print the GPIO1/GPIO2 state
Serial.print(F("GPIO1 is: "));
Serial.println(mySwitch.digitalRead(1));
Serial.print(F("GPIO2 is: "));
Serial.println(mySwitch.digitalRead(2));
.
.
.
}
Instead of an INPUT, you will change each GPIO pin as an OUTPUT. Additionally, you will need to set the pin as a HIGH or LOW.
setup(){
.
.
.
// Configure GPIO1 and GPIO2 as OUTPUT
mySwitch.pinMode(1, OUTPUT);
mySwitch.pinMode(2, OUTPUT);
.
.
.
}
void loop() {
.
.
.
// Write to GPIO1 & GPIO2
Serial.println(F("GPIO1 is set to HIGH."));
mySwitch.digitalWrite(1, HIGH);
Serial.println(F("GPIO2 is set to LOW."));
mySwitch.digitalWrite(2, LOW);
.
.
.
}
To test, simply attach an LED with a current limiting resistor between the GPIO and GND. The LED should light up when the pin is HIGH and turn off when set to LOW. Of course, you can also connect a multimeter set to read the voltage between the GPIO pin nd GND. The GPIO pin should read 3.3V when set to HIGH and 0V when set to LOW.
After uploading the code, open the Serial Monitor or terminal emulator of your choice with the baud rate set to 115200. You will be presented with a few options to configure the Qwiic Power Switch:
- 1 — Power is ON I2C isolation is disabled.
- 2 — Power is OFF. I2C isolation is enabled.
- 3 — I2C isolation enabled. I2C is isolated.
- 4 — I2C isolation disabled. I2C is not isolated.
Let's send a 2 to turn power off the Qwiic Power Switch's output and isolate the I2C data and clock lines. The Arduino will output a message: "Power is OFF. I2C isolation is enabled." The Arduino will also read the Qwiic Power Switch's GPIO1 and GPIO2. In this case, there was nothing connected to either GPIO so the pin reading was 1 indicating a HIGH. If there was a logic LOW, the pin would read 0 indicating a LOW.
If the Qwiic-enabled board includes a built-in LED, you can see if power is enabled. The power LED (as well as any other LED on the board) should have turned off as soon as power is disabled at the OUT port. In this case, the Qwiic Power Switch's OUT and ZED-F9P's LEDs when power was disabled and I2C isolation is enabled.
Note
If power is OFF at the OUT port but you decide to disable I2C isolation, you may notice a voltage at the 3.3V OUT pin from the pull-up resistors connected to the I2C lines.
If you would like to verify that the I2C lines are isolated, try turning the power back on by sending a 1 and then sending a 3 to isolate the I2C lines. While still applying power to the Qwiic Power Switch, try re-uploading code to the Arduino for the Qwiic-enabled board that is connected to the Qwiic Power Switch's OUT. Assuming that the example code checks for the Qwiic-enabled device, you should receive a message indicating that the Qwiic-enabled device was not detected.
Note
Of course, you could also use the Arduino I2C scanner to scan the I2C bus and detect I2C devices. When scanning, you should only see the Qwwic Power Switch and anything that was connected before the IN port. Anything after the OUT will not be detected on the OUT port if power was disabled or the lines were isolated.