Hardware Overview
In this section, we will highlight the hardware and pins that are broken out on the SparkFun Soft Power Switch - JST 2mm. For more information, check out our Resources and Going Further on the components used on the breakout board.
Soft Power Switch Versions
The SparkX Mk1 Soft Power Switch is great, but we do see occasional issues caused by component tolerances or the operating temperature. Mk2 is based on an application note by Texas Instruments, and is a completely digital design. It is based around a 74LVC1G175 D-type flip-flop - remember those?! - and is insensitive to temperature and component variation.
It also includes improvements like:
- An over-current self-resetting 2A fuse.
- Input and output LEDs.
- LED jumpers.
- Improved momentary button (i.e. the height of the button is increased).
Differences include:
- The Soft Power Switch - JST 2mm works up to 5.5V only (the Mk1 is good up to 12V).
- For Mk2, driving the fast OFF pin HIGH by the system will force fast power off via software. However for Mk1, the fast OFF pin was driven low.
- Slightly bigger PCB: 1.0"x1.0" sized breakout (the Mk1 was 0.8"x1.0").
Power
Warning
The Soft Power Switch - JST 2mm works up to 5.5V only. (Mk1 is good up to 12V.)
Warning
The Soft Power Switch - JST 2mm was designed to work with DC loads. Unfortunately, the board is not designed for AC loads.
Note
Once the Soft Power Switch - JST 2mm is powered, it will take a few seconds to discharge power after disconnecting the power source from the IN port. So if you decide to do quick power cycle, the board can still be powered if there is not a long enough delay.
The maximum input voltage that the Soft Power Switch - JST 2mm can handle is 5.5V while the minimum input voltage is 1.8V. The board was designed to be used with single cell LiPo batteries with the built-in 2-pin JST connector, so the typical voltage will be about 3.7V nominally. The maximum current draw that the board can handle is 2A continuous and 4A peak (fuse protected). With the VIN LED disabled, the board has a very low quiescent current: <1µA @ 3.75V.
- VIN — This pin is the voltage input. As stated above, the maximum input voltage is 5.5V while the minimum is 1.8V. Voltage is applied to this pin from a single cell LiPo battery which is about 3.7V nominally.
- VOUT — The output voltage of the board whenever the switch is active.
- GND — Of course, is the common, ground voltage (0V reference) for the system.
The Soft Power Switch - JST 2mm also supports battery charging. If the target device has onboard LiPo charging, current can be passed back through the switch circuit and charge the battery.
Power Button and Button State
The board includes a built-in momentary push button as the power button. This pin is broken out to a PTH for users to connect an external button. There is also the PUSH pin to indicate the button's state. The PUSH pin can act as an output to a microcontroller indicating the state of the power button (HIGH = not pressed, LOW = user is pressing power button). This can be used as an input to your firmware to begin to shut down before power is lost. Alternatively, there is also an OFF pin that can be driven HIGH by the system forcing fast power off via software. Below is a summary of the pins broken out.
- BTN — Short for button. If desired, connect this input pin to an external button between BTN and GND.
- PUSH — Open-drain output. This pin requires a pull-up resistor. A low indicates the button is pushed.
- OFF — Drive HIGH to turn the output off.
Note
For Mk2, driving the fast OFF pin HIGH by the system will force fast power off via software. However for Mk1, the fast OFF pin was driven low.
LEDs
- VIN — The VIN LED connects to the input voltage. This indicates when there is voltage at VIN. This LED can be disabled with the LED jumper on the back of the board and below the silkscreen labeled IN.
- VOUT — The VOUT LED connects to the output voltage. This indicates when there is voltage at VOUT. This LED can be disabled with the LED jumper on the back of the board and below the silkscreen labeled OUT.
Jumpers
Note
If this is your first time working with jumpers, check out the How to Work with Jumper Pads and PCB Traces tutorial for more information.
The back of the board includes jumpers to configure the board.
- LED (below IN) — By default, the LED jumper located below the silkscreen labeled IN is closed. This connects the VIN LED to the input voltage. Cutting this will disable the LED for the input voltage.
- LED (below OUT) — By default, the LED jumper located below the silkscreen labeled OUT is closed. This connects the LED to the output voltage. Cutting this jumper will disable the LED for the output voltage.
3D Model
A 3D model of the board and components was exported to a STEP file using KiCad.
Board Dimensions
The board is 1.0" x 1.0" (2.54mm x 2.54mm). There are 4x mounting holes by the corners of the board. You can use 4-40 standoffs to mount the board to a panel or enclosure.