AS7343 Arduino Library Setup

Arduino

This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino IDE, library, or board add-on, please readh through the following tutorials:

The SparkFun AS7343 Arduino Library helps users get started with the AS7343 with seven examples that go through how to use different features of the AS7343. The library is built around the SparkFun Arduino Toolkit and requires installation of both libraries to work. Install the libraries using the Arduino library manager by opening the tool and searching for "SparkFun Toolkit" and "SparkFun AS7343" and installing the latest releases of both libraries. Users who prefer to manually install the libraries can download ZIP files of them here: SparkFun Toolkit (ZIP) and SparkFun AS7343 Arduino Library (ZIP).