Quick Start
In this Quick Start Guide we'll connect the SparkFun Spectral Sensor Breaout - AS7343 (Qwiic) to an IoT RedBoard - ESP32 to output measurements of visible and near-infrared light and display them in a colorful web terminal bar graph.
If you're not familiar with using sensor breakouts, development boards or the development environments covered in this guide, refer to the Hardware & Arduino Setup sections of this Hookup Guide for a detailed overview of the board along with instructions on setting up and using the SparkFun AS7343 Arduino Library. For those who prefer to run this example in MicroPython, read on to the AS7343 Python Setup and Python Examples sections of this guide.
Basic Assembly
As this is a Qwiic breakout, assembling the circuit only requires connecting the sensor breakout to a Qwiic-compatible development board like the IoT RedBoard - ESP32. Connect the Spectral Sensor Breakout to the IoT RedBoard with a Qwiic cable and then connect the IoT RedBoard to your computer with a USB-C cable like the photo below demonstrates:
Arduino Web Terminal Bar Graph Example
The Arduino Web Terminal Bar Graph example sets up the AS7343 to output from all channels and format the data to work with the SparkFun Web Serial Plotter tool and display it in a bar graph. The Web Terminal Bar Graph site only works in a Chromium-based browser (sorry, no Firefox) and just requires a serial connection over USB to your microcontroller.
- Open the Arduino IDE
- Open the Library Manager tool and search for "SparkFun Toolkit" and "SparkFun AS7343" and install the latest versions of both libraries.
- If necessary, open the Boards Manager and search for "ESP32" to install the IoT RedBoard - ESP32 board definition.
- Open "Example 7 - Web Terminal Bar Graphs" from the SparkFun AS7343 Arduino Library and select your board (IoT RedBoard - ESP32) and Port.
- Click the "Upload" button and wait for the code to finish compiling and uploading.
- Open this link in a browser and select the COM port of the IoT RedBoard.
- Try moving the Spectral Sensor around and pointing it at different objects/colors and watch the Bar Graph in the bottom half of the window update every 1s like the gif below.
Code to Note
The code begins by setting the AS7343 to operate with default settings and prints out whether or not it fails or begins:
if (mySensor.begin() == false)
{
Serial.println("Sensor failed to begin. Please check your wiring!");
Serial.println("Halting...");
while (1)
;
}
Serial.println("Sensor began.")
After initializing the sensor and powering it on, the code then sets the AS7343's AutoSmux to output all 18 channels and prints out the result:
if (mySensor.setAutoSmux(AUTOSMUX_18_CHANNELS) == false)
{
Serial.println("Failed to set AutoSmux.");
Serial.println("Halting...");
while (1)
;
}
Serial.println("AutoSmux set to 18 channels.");
The main loop turns the white LED on to illuminate the sensing area and then takes a reading from all channels once per second:
mySensor.ledOn();
delay(100);
// Read all data registers
// if it fails, print a failure message and continue
if (mySensor.readSpectraDataFromSensor() == false)
{
Serial.println("Failed to read spectral data.");
}
Finally, in order to format the data for the web serial terminal, the code fills the buffer with channel data in a specific order and prints the buffer for the web terminal to output the bar graph data correctly:
sprintf(buffer, "%d,%d,%d,%d,%d,%d,%d,%d,%d,%d,%d,%d,%d\n",
mySensor.getChannelData(CH_PURPLE_F1_405NM),
mySensor.getChannelData(CH_DARK_BLUE_F2_425NM),
mySensor.getChannelData(CH_BLUE_FZ_450NM),
mySensor.getChannelData(CH_LIGHT_BLUE_F3_475NM),
mySensor.getChannelData(CH_BLUE_F4_515NM),
mySensor.getChannelData(CH_GREEN_F5_550NM),
mySensor.getChannelData(CH_GREEN_FY_555NM),
mySensor.getChannelData(CH_ORANGE_FXL_600NM),
mySensor.getChannelData(CH_BROWN_F6_640NM),
mySensor.getChannelData(CH_RED_F7_690NM),
mySensor.getChannelData(CH_DARK_RED_F8_745NM),
mySensor.getChannelData(CH_VIS_1),
mySensor.getChannelData(CH_NIR_855NM));
Serial.print(buffer);