Arduino Example
Now that we've installed the espressif boards package in Arduino, it's time to upload our first sketch to make sure everything is working properly.
Blink RGB Example
The ESP32 core includes integrated code support for easily controlling a WS2812 LED and an example demonstrating how to cycle an RGB LED like the one found on this Thing Plus so long as the board variant defines it as RGB_BUILTIN. The Thing Plus ESP32-C6 does define IO23 as RBG_BUILTIN so this example and all other code calling for the built-in RGB LED works for this board. Open the example by navigating to File > Examples > ESP32 > GPIO > BlinkRGB like the screenshot below shows:
Select the board (SparkFun Thing Plus - C6) and Port and click "Upload". After uploading you should see the STAT LED on the board turn on full white, turn off, and then cycle through red, green, and blue repeatedly.
USB CDC On Boot Settings
Take note of the option labeled "USB CDC on Boot" when selecting the Board from the Tools menu. This option sets the serial outputs and defines their label for use in code. The SparkFun variants default to Enable USB CDC on boot which sets both Serial and Serial0 as available serial ports. In this configuration, Serial corresponds to the direct USB/Serial converter on the chip (and the USB-C interface) and Serial0 corresponds to the UART0 bus (default pins are 16 and 17).
With either setting, Serial1 is available and refers to the UART1 bus (default pins are 4 and 5).