Installing the CP2102 USB Driver

Warning

Make sure to manually install the driver for the CP2102N with the following instructions. The driver that Windows auto-installs will not work with the auto-reset circuit on the board and can cause serial uploads to fail.

You will also need to install the SiLabs CP210X Driver, which can be found here: USB to UART Bridge VCP Driver.

Note

If applicable, make sure you are using the proper driver files for your CPU architecture. This is usually indicated by a folder or file name with "x86" for 32-bit processors or "x64" for 64-bit processors.