More Examples!!!

Of course, this only skims the surface of what the SparkFun Thing Plus - NORA-W306 can do. There are a handful of examples from the board support package that were not highlighted in this tutorial and are being ported by our friends at Realtek with the NORA-W306 module. From the menu, try opening the other examples listed for hte board: File > Examples > Examples for AW_CU488 Thing Plus (RTL8721DM)

More Arduino Examples!
More Arduino Examples!

Note

Some of the examples listed in the menu may still be under development. Make sure to be patient as they include more support for the NORA-W306 module.

Or try adding another Qwiic-enabled device or a breakout board to your next project!