Hardware Assembly
USB Connector
The USB connection is utilized for programming and serial communication. Users only need to plug their RA6M5 Thing Plus into a computer using a USB-C cable.
The RA6M5 Thing Plus with USB-C cable attached.
LiPo Battery
For remote IoT applications, a LiPo battery can be connected. Additionally, users may be interested in utilizing a solar panel and USB-C cable to recharge their battery.
Warning
Users should avoid pulling on the wires of a battery to disconnect it from the board. Instead, it is recommended that a pair of dikes (i.e. diagonal wire cutters), pliers, or tweezers be used to pull on the JST connector housing, to avoid damaging the battery wiring.
Breakout Pins
The PTH pins on the RA6M5 Thing Plus are broken out into 0.1"-spaced pins on the edges of the board.
New to soldering?
If you have never soldered before or need a quick refresher, check out our How to Solder: Through-Hole Soldering guide.
Headers
Headers are versatile in their compatibility with shields, breadboards, or jumper wires.
Soldering headers to the RA6M5 Thing Plus.
Stackable Headers
Our Feather Stackable Header Kit is a great option for stacking on shields (w/ Feather footprint) or on a breadboard; while leaving its pins still accessible.
SD Card Slot
The RA6M5 Thing Plus includes a µSD card slot on the back of the board. The cardholder functions through a push/pull operation. (The card slot doesn't include a spring retention mechanism; cards are held in place through friction.)
Users can slide-in or pull-out a µSD card from the cardholder.
SD Card Compatibility
The R6M5 Thing Plus supports µSD cards with a FAT32 file system (i.e. only cards up to 32GB in size).
Qwiic Devices
The Qwiic system allows users to effortlessly prototype with a Qwiic compatible I2C device without soldering. Users can attach any Qwiic compatible sensor or board, with just a Qwiic cable. (*The example below, is for demonstration purposes and is not pertinent to the board functionality or this tutorial.)
The BME688 environmental and VL53L1X distance Qwiic sensor boards connected to the RA6M5 Thing Plus.