![]() |
Xbee Arduino
Arduino Driver for Xbee
|
#include <xbee_lr.h>
Public Attributes | |
| uint8_t | port |
| uint8_t | payloadSize |
| uint8_t * | payload |
| uint8_t | ack |
| uint8_t | status |
| uint8_t | frameId |
| int8_t | rssi |
| int8_t | snr |
| uint8_t | dr |
| uint32_t | counter |
| uint8_t XBeeLRPacket_s::ack |
| uint32_t XBeeLRPacket_s::counter |
| uint8_t XBeeLRPacket_s::dr |
| uint8_t XBeeLRPacket_s::frameId |
| uint8_t* XBeeLRPacket_s::payload |
| uint8_t XBeeLRPacket_s::payloadSize |
| uint8_t XBeeLRPacket_s::port |
| int8_t XBeeLRPacket_s::rssi |
| int8_t XBeeLRPacket_s::snr |
| uint8_t XBeeLRPacket_s::status |