#include <xbee.h>
◆ connect
| bool(* XBeeVTable::connect) (XBee *self) |
◆ connected
| bool(* XBeeVTable::connected) (XBee *self) |
◆ disconnect
| bool(* XBeeVTable::disconnect) (XBee *self) |
◆ handleRxPacketFrame
| void(* XBeeVTable::handleRxPacketFrame) (XBee *self, void *frame) |
◆ handleTransmitStatusFrame
| void(* XBeeVTable::handleTransmitStatusFrame) (XBee *self, void *frame) |
◆ hardReset
| void(* XBeeVTable::hardReset) (XBee *self) |
◆ init
| bool(* XBeeVTable::init) (XBee *self, uint32_t baudrate, void *device) |
◆ process
| void(* XBeeVTable::process) (XBee *self) |
◆ sendData
| uint8_t(* XBeeVTable::sendData) (XBee *self, const void *data) |
◆ softReset
| bool(* XBeeVTable::softReset) (XBee *self) |
The documentation for this struct was generated from the following file: