flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
_flxFSSDMMCard Class Reference

#include <flxFSSDMMCard.h>

Inheritance diagram for _flxFSSDMMCard:
flxIFileSystem flxDescriptor

Public Member Functions

 _flxFSSDMMCard (_flxFSSDMMCard const &)=delete
 
void operator= (_flxFSSDMMCard const &)=delete
 
bool initialize ()
 
bool initialize (uint8_t pinCS)
 
bool initialize (uint8_t pinCS, uint8_t pinPower)
 
void setPower (bool powerOn)
 
bool power (void)
 
void setPowerPin (uint8_t pin)
 
void setCSPin (uint8_t pin)
 
flxFSFile open (const char *name, flxFileOpenMode_t mode, bool create=false)
 
bool exists (const char *name)
 
bool remove (const char *name)
 
bool rename (const char *nameFrom, const char *nameTo)
 
bool mkdir (const char *path)
 
bool rmdir (const char *path)
 
uint64_t size (void)
 
uint64_t total (void)
 
const char * type (void)
 
uint64_t used (void)
 
bool enabled (void)
 
FS fileSystem (void)
 
virtual flxFSFile open (const char *name, flxFileOpenMode_t mode, bool create=false)=0
 
virtual bool exists (const char *name)=0
 
virtual bool remove (const char *name)=0
 
virtual bool rename (const char *nameFrom, const char *nameTo)=0
 
virtual bool mkdir (const char *path)=0
 
virtual bool rmdir (const char *path)=0
 
virtual uint64_t size (void)=0
 
virtual const char * type (void)=0
 
virtual bool enabled (void)=0
 
virtual FS fileSystem (void)=0
 
- Public Member Functions inherited from flxDescriptor
 flxDescriptor ()
 
void setName (const char *new_name)
 Set the Name object - storing the pointer to the provided string No allocation is performed. If the previous name was allocated, it is freed. More...
 
void setName (const char *new_name, const char *new_desc)
 Set the Name object and the Description for the object. Both strings are constants. More...
 
void setName (char *new_name)
 Set the Name object, but makes a copy of the input string since the input is not const. If the previous name was allocated, it is freed. More...
 
const char * name ()
 Return a const char pointer to the name of the object. More...
 
std::string name_ (void)
 Returns a std::string of the name of the object. More...
 
void setDescription (const char *new_desc)
 Set the Description object - the input value is constant and not copied. If the previous description was allocated, it is freed. More...
 
void setDescription (char *new_desc)
 Set the Description object - the input value is not constant and is copied. If the previous description was allocated, it is freed. More...
 
const char * description ()
 Return the constant C string pointer to the description of the object. More...
 
std::string description_ (void)
 Return the description of the object as a std::string. More...
 
void setTitle (const char *title)
 Set the Title object - the title is optional and is used mostly for UX or organizational purposes. The input value is constant and not copied. If the previous title was allocated, it is freed. More...
 
void setTitleAlloc (char *new_title)
 Set the Title of the object , but make an explict copy of the provided string. More...
 
const char * title (void)
 Return the C constant string pointer to the title of the object. More...
 

Static Public Member Functions

static _flxFSSDMMCard & get (void)
 

Additional Inherited Members

- Public Types inherited from flxIFileSystem
enum  flxFileOpenMode_t { kFileWrite = 1 , kFileRead , kFileAppend }
 
- Protected Attributes inherited from flxDescriptor
const char * _name
 
bool _nameAlloc
 
const char * _desc
 
bool _descAlloc
 
const char * _title
 
bool _titleAlloc
 

Constructor & Destructor Documentation

◆ _flxFSSDMMCard()

_flxFSSDMMCard::_flxFSSDMMCard ( _flxFSSDMMCard const &  )
delete

Member Function Documentation

◆ enabled()

bool _flxFSSDMMCard::enabled ( void  )
inlinevirtual

Implements flxIFileSystem.

◆ exists()

bool _flxFSSDMMCard::exists ( const char *  name)
virtual

Implements flxIFileSystem.

◆ fileSystem()

FS _flxFSSDMMCard::fileSystem ( void  )
virtual

Implements flxIFileSystem.

◆ get()

static _flxFSSDMMCard & _flxFSSDMMCard::get ( void  )
inlinestatic

◆ initialize() [1/3]

bool _flxFSSDMMCard::initialize ( )

◆ initialize() [2/3]

bool _flxFSSDMMCard::initialize ( uint8_t  pinCS)

◆ initialize() [3/3]

bool _flxFSSDMMCard::initialize ( uint8_t  pinCS,
uint8_t  pinPower 
)

◆ mkdir()

bool _flxFSSDMMCard::mkdir ( const char *  path)
virtual

Implements flxIFileSystem.

◆ open()

flxFSFile _flxFSSDMMCard::open ( const char *  name,
flxFileOpenMode_t  mode,
bool  create = false 
)
virtual

Implements flxIFileSystem.

◆ operator=()

void _flxFSSDMMCard::operator= ( _flxFSSDMMCard const &  )
delete

◆ power()

bool _flxFSSDMMCard::power ( void  )
inline

◆ remove()

bool _flxFSSDMMCard::remove ( const char *  name)
virtual

Implements flxIFileSystem.

◆ rename()

bool _flxFSSDMMCard::rename ( const char *  nameFrom,
const char *  nameTo 
)
virtual

Implements flxIFileSystem.

◆ rmdir()

bool _flxFSSDMMCard::rmdir ( const char *  path)
virtual

Implements flxIFileSystem.

◆ setCSPin()

void _flxFSSDMMCard::setCSPin ( uint8_t  pin)
inline

◆ setPower()

void _flxFSSDMMCard::setPower ( bool  powerOn)

◆ setPowerPin()

void _flxFSSDMMCard::setPowerPin ( uint8_t  pin)
inline

◆ size()

uint64_t _flxFSSDMMCard::size ( void  )
virtual

Implements flxIFileSystem.

◆ total()

uint64_t _flxFSSDMMCard::total ( void  )

◆ type()

const char * _flxFSSDMMCard::type ( void  )
virtual

Implements flxIFileSystem.

◆ used()

uint64_t _flxFSSDMMCard::used ( void  )

The documentation for this class was generated from the following files: