flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
_flxParameterIn< T, Object, _setter > Member List

This is the complete list of members for _flxParameterIn< T, Object, _setter >, including all inherited members.

_descflxDescriptorprotected
_descAllocflxDescriptorprotected
_flxDataIn()_flxDataIn< T >inline
_flxParameterIn()_flxParameterIn< T, Object, _setter >inline
_flxParameterIn(T min, T max)_flxParameterIn< T, Object, _setter >inline
_flxParameterIn(std::initializer_list< std::pair< const std::string, T > > limitSet)_flxParameterIn< T, Object, _setter >inline
_nameflxDescriptorprotected
_nameAllocflxDescriptorprotected
_titleflxDescriptorprotected
_titleAllocflxDescriptorprotected
addDataLimitValidValue(std::string name, T value)_flxDataIn< T >inline
addDataLimitValidValue(std::pair< const std::string, T > value)_flxDataIn< T >inline
addDataLimitValidValue(std::initializer_list< std::pair< const std::string, T > > limitSet)_flxDataIn< T >inline
clearDataLimit(void)_flxDataIn< T >inline
dataLimit(void)_flxParameterIn< T, Object, _setter >inlinevirtual
description()flxDescriptorinline
description_(void)flxDescriptorinline
editValue(flxDataEditor &theEditor)_flxParameterIn< T, Object, _setter >inlinevirtual
enabled(void)flxParameterinline
flxDescriptor()flxDescriptorinline
flxParameter()flxParameterinline
isValueValid(T value)_flxDataIn< T >inline
name()flxDescriptorinline
name_(void)flxDescriptorinline
operator()(Object *obj)_flxParameterIn< T, Object, _setter >inline
operator()(Object *obj, const char *name)_flxParameterIn< T, Object, _setter >inline
operator()(Object *obj, const char *name, const char *desc)_flxParameterIn< T, Object, _setter >inline
operator()(Object *obj, const char *name, const char *desc, flxParamValueType_t vtype)_flxParameterIn< T, Object, _setter >inline
operator()(T const &value)_flxParameterIn< T, Object, _setter >inline
set(T const &value)_flxParameterIn< T, Object, _setter >inlinevirtual
set_value(bool v)flxDataIninline
set_value(int8_t v)flxDataIninline
set_value(int16_t v)flxDataIninline
set_value(int32_t v)flxDataIninline
set_value(uint8_t v)flxDataIninline
set_value(uint16_t v)flxDataIninline
set_value(uint32_t v)flxDataIninline
set_value(float v)flxDataIninline
set_value(double v)flxDataIninline
set_value(std::string &v)flxDataIninline
setBool(bool value)_flxDataIn< T >inlinevirtual
setDataLimit(flxDataLimitType< T > &dataLimit)_flxDataIn< T >inline
setDataLimit(flxDataLimitType< T > *dataLimit)_flxDataIn< T >inline
setDataLimitRange(T min, T max)_flxDataIn< T >inline
setDataLimitRange(std::pair< T, T > range)_flxDataIn< T >inline
setDescription(const char *new_desc)flxDescriptorinline
setDescription(char *new_desc)flxDescriptorinline
setDouble(double value)_flxDataIn< T >inlinevirtual
setEnabled(bool enabled)flxParameterinlinevirtual
setFloat(float value)_flxDataIn< T >inlinevirtual
setInt16(int16_t value)_flxDataIn< T >inlinevirtual
setInt32(int32_t value)_flxDataIn< T >inlinevirtual
setInt8(int8_t value)_flxDataIn< T >inlinevirtual
setName(const char *new_name)flxDescriptorinline
setName(const char *new_name, const char *new_desc)flxDescriptorinline
setName(char *new_name)flxDescriptorinline
setString(std::string &value)_flxDataIn< T >inlinevirtual
setTitle(const char *title)flxDescriptorinline
setTitleAlloc(char *new_title)flxDescriptorinline
setUInt16(uint16_t value)_flxDataIn< T >inlinevirtual
setUInt32(uint32_t value)_flxDataIn< T >inlinevirtual
setUInt8(uint8_t value)_flxDataIn< T >inlinevirtual
setValue(flxDataVariable &value)_flxParameterIn< T, Object, _setter >inlinevirtual
setValueType(flxParamValueType_t type)flxParameterinline
title(void)flxDescriptorinline
to_string()flxParameterIninline
type()_flxParameterIn< T, Object, _setter >inlinevirtual
valueType(void)flxParameterinline