flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxParameter Class Referenceabstract

#include <flxCoreParam.h>

Inheritance diagram for flxParameter:
flxDescriptor flxParameterIn flxParameterOut _flxParameterIn< flxDevNAU7802, &flxDevNAU7802::calculate_calibration_factor > _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_epoch > _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_seconds > _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_minutes > _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_hours > _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_date > _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_weekday > _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_month > _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_year > _flxParameterIn< flxDevSGP40, &flxDevSGP40::write_rh > _flxParameterIn< flxDevSGP40, &flxDevSGP40::write_temperature > _flxParameterIn< flxDevSTC31, &flxDevSTC31::write_rh > _flxParameterIn< flxDevSTC31, &flxDevSTC31::write_temperature > _flxParameterIn< flxDevSTC31, &flxDevSTC31::write_pressure > _flxParameterIn< flxLogger, &flxLogger::reset_sample_number > _flxParameterIn< T, Object, _setter > flxParameterInString< Object, _setter > flxParameterInVoidType flxParameterOutArray flxParameterOutScalar

Public Member Functions

 flxParameter ()
 
bool enabled (void)
 
flxParamValueType_t valueType (void)
 
void setValueType (flxParamValueType_t type)
 
virtual void setEnabled (bool enabled)
 
virtual flxDataType_t type (void)=0
 
- Public Member Functions inherited from flxDescriptor
 flxDescriptor ()
 
void setName (const char *new_name)
 Set the Name object - storing the pointer to the provided string No allocation is performed. If the previous name was allocated, it is freed. More...
 
void setName (const char *new_name, const char *new_desc)
 Set the Name object and the Description for the object. Both strings are constants. More...
 
void setName (char *new_name)
 Set the Name object, but makes a copy of the input string since the input is not const. If the previous name was allocated, it is freed. More...
 
const char * name ()
 Return a const char pointer to the name of the object. More...
 
std::string name_ (void)
 Returns a std::string of the name of the object. More...
 
void setDescription (const char *new_desc)
 Set the Description object - the input value is constant and not copied. If the previous description was allocated, it is freed. More...
 
void setDescription (char *new_desc)
 Set the Description object - the input value is not constant and is copied. If the previous description was allocated, it is freed. More...
 
const char * description ()
 Return the constant C string pointer to the description of the object. More...
 
std::string description_ (void)
 Return the description of the object as a std::string. More...
 
void setTitle (const char *title)
 Set the Title object - the title is optional and is used mostly for UX or organizational purposes. The input value is constant and not copied. If the previous title was allocated, it is freed. More...
 
void setTitleAlloc (char *new_title)
 Set the Title of the object , but make an explict copy of the provided string. More...
 
const char * title (void)
 Return the C constant string pointer to the title of the object. More...
 

Additional Inherited Members

- Protected Attributes inherited from flxDescriptor
const char * _name
 
bool _nameAlloc
 
const char * _desc
 
bool _descAlloc
 
const char * _title
 
bool _titleAlloc
 

Constructor & Destructor Documentation

◆ flxParameter()

flxParameter::flxParameter ( )
inline

Member Function Documentation

◆ enabled()

bool flxParameter::enabled ( void  )
inline

◆ setEnabled()

virtual void flxParameter::setEnabled ( bool  enabled)
inlinevirtual

Reimplemented in _flxParameterOut< T, Object, _getter >, _flxParameterOut< double, Object, _getter >, _flxParameterOut< float, Object, _getter >, _flxParameterOut< float, flxDevACS37800, _getter >, _flxParameterOut< flxDevACS37800, &flxDevACS37800::read_pos_angle >, _flxParameterOut< flxDevACS37800, &flxDevACS37800::read_pos_power_factor >, _flxParameterOut< float, flxDevADS1015, _getter >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_single_0 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_single_1 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_single_2 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_single_3 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_differential_P0_N1 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_differential_P0_N3 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_differential_P1_N3 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_differential_P2_N3 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readu_single_0 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readu_single_1 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readu_single_2 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readu_single_3 >, _flxParameterOut< float, flxDevADS122C04, _getter >, _flxParameterOut< float, flxDevAHT20, _getter >, _flxParameterOut< float, flxDevAMG8833, _getter >, _flxParameterOut< flxDevAS7265X, &flxDevAS7265X::read_output_type >, _flxParameterOut< float, flxDevAS7265X, _getter >, _flxParameterOut< float, flxDevAS7331, _getter >, _flxParameterOut< flxDevAS7343, &flxDevAS7343::get_blue_value >, _flxParameterOut< flxDevAS7343, &flxDevAS7343::get_green_value >, _flxParameterOut< flxDevAS7343, &flxDevAS7343::get_red_value >, _flxParameterOut< flxDevAS7343, &flxDevAS7343::get_nir_value >, _flxParameterOut< flxDevAS7343, &flxDevAS7343::get_flicker_value >, _flxParameterOut< flxDevAnalogPin, &flxDevAnalogPin::read_pin_value >, _flxParameterOut< float, flxDevBME280, _getter >, _flxParameterOut< float, flxDevBME68x, _getter >, _flxParameterOut< flxDevBME68x, &flxDevBME68x::read_Status >, _flxParameterOut< float, flxDevBMI270, _getter >, _flxParameterOut< double, flxDevBMP384, _getter >, _flxParameterOut< float, flxDevBMP581, _getter >, _flxParameterOut< float, flxDevBMV080, _getter >, _flxParameterOut< flxDevBMV080, &flxDevBMV080::is_obstructed >, _flxParameterOut< flxDevBioHub, &flxDevBioHub::read_heart_rate >, _flxParameterOut< flxDevBioHub, &flxDevBioHub::read_confidence >, _flxParameterOut< flxDevBioHub, &flxDevBioHub::read_oxygen >, _flxParameterOut< flxDevBioHub, &flxDevBioHub::read_status >, _flxParameterOut< flxDevBioHub, &flxDevBioHub::read_extended_status >, _flxParameterOut< float, flxDevBioHub, _getter >, _flxParameterOut< flxDevButton, &flxDevButton::read_button_state >, _flxParameterOut< float, flxDevCCS811, _getter >, _flxParameterOut< flxDevENS160, &flxDevENS160::read_AQI >, _flxParameterOut< flxDevENS160, &flxDevENS160::read_TVOC >, _flxParameterOut< flxDevENS160, &flxDevENS160::read_ETOH >, _flxParameterOut< flxDevENS160, &flxDevENS160::read_ECO2 >, _flxParameterOut< float, flxDevENS160, _getter >, _flxParameterOut< float, flxDevFS3000, _getter >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_year >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_month >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_day >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_hour >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_min >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_sec >, _flxParameterOut< double, flxDevGNSS, _getter >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_siv >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_fix >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_carrier_soln >, _flxParameterOut< float, flxDevGNSS, _getter >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_tow >, _flxParameterOut< float, flxDevISM330Base, _getter >, _flxParameterOut< float, flxDevLPS25HB, _getter >, _flxParameterOut< float, flxDevMAX17048, _getter >, _flxParameterOut< float, flxDevMCP9600, _getter >, _flxParameterOut< double, flxDevMMC5983Base, _getter >, _flxParameterOut< flxDevMMC5983Base, &flxDevMMC5983Base::read_temperature >, _flxParameterOut< float, flxDevMS5637, _getter >, _flxParameterOut< float, flxDevMS8607, _getter >, _flxParameterOut< float, flxDevMicroPressure, _getter >, _flxParameterOut< float, flxDevNAU7802, _getter >, _flxParameterOut< double, flxDevOPT4048, _getter >, _flxParameterOut< flxDevOPT4048, &flxDevOPT4048::get_lux >, _flxParameterOut< flxDevPASCO2V01, &flxDevPASCO2V01::read_CO2 >, _flxParameterOut< flxDevRV8803, &flxDevRV8803::read_year >, _flxParameterOut< flxDevRV8803, &flxDevRV8803::get_epoch >, _flxParameterOut< flxDevSCD30, &flxDevSCD30::read_CO2 >, _flxParameterOut< float, flxDevSCD30, _getter >, _flxParameterOut< flxDevSCD40, &flxDevSCD40::read_CO2 >, _flxParameterOut< float, flxDevSCD40, _getter >, _flxParameterOut< float, flxDevSDP3X, _getter >, _flxParameterOut< float, flxDevSEN54, _getter >, _flxParameterOut< flxDevSGP30, &flxDevSGP30::read_tvoc >, _flxParameterOut< flxDevSGP30, &flxDevSGP30::read_co2 >, _flxParameterOut< flxDevSGP30, &flxDevSGP30::read_h2 >, _flxParameterOut< flxDevSGP30, &flxDevSGP30::read_ethanol >, _flxParameterOut< flxDevSGP40, &flxDevSGP40::read_voc >, _flxParameterOut< float, flxDevSHTC3, _getter >, _flxParameterOut< float, flxDevSTC31, _getter >, _flxParameterOut< flxDevSTHS34PF80, &flxDevSTHS34PF80::read_Presence >, _flxParameterOut< flxDevSTHS34PF80, &flxDevSTHS34PF80::read_Motion >, _flxParameterOut< float, flxDevSTHS34PF80, _getter >, _flxParameterOut< flxDevSoilMoisture, &flxDevSoilMoisture::read_moisture_value >, _flxParameterOut< float, flxDevSoilMoisture, _getter >, _flxParameterOut< flxDevTMF882X, &flxDevTMF882X::read_photon_count >, _flxParameterOut< flxDevTMF882X, &flxDevTMF882X::read_ref_photon_count >, _flxParameterOut< flxDevTMF882X, &flxDevTMF882X::read_ambient_light >, _flxParameterOut< double, flxDevTMP117, _getter >, _flxParameterOut< flxDevTwist, &flxDevTwist::read_button_state >, _flxParameterOut< flxDevTwist, &flxDevTwist::get_twist_count >, _flxParameterOut< flxDevVCNL4040, &flxDevVCNL4040::read_proximity >, _flxParameterOut< flxDevVCNL4040, &flxDevVCNL4040::read_lux >, _flxParameterOut< float, flxDevVEML6075, _getter >, _flxParameterOut< flxDevVEML7700, &flxDevVEML7700::read_ambient_light >, _flxParameterOut< flxDevVEML7700, &flxDevVEML7700::read_white_level >, _flxParameterOut< float, flxDevVEML7700, _getter >, _flxParameterOut< flxDevVL53L1X, &flxDevVL53L1X::read_distance >, _flxParameterOut< flxDevVL53L1X, &flxDevVL53L1X::read_range_status >, _flxParameterOut< flxDevVL53L1X, &flxDevVL53L1X::read_signal_rate >, _flxParameterOut< flxLogger, &flxLogger::get_sample_number >, flxParameterOutString< Object, _getter >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_iso8601 >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_yyyy_mm_dd >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_yyyy_dd_mm >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_dd_mm_yyyy >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_hh_mm_ss >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_fix_string >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_carrier_soln_string >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_date_USA >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_date >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_time >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_iso8601 >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_iso8601_tz >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_day >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_day_short >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_ordinal >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_month >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_month_short >, flxParameterOutString< flxDevSerial, &flxDevSerial::read_serial_value >, flxParameterOutString< flxLogger, &flxLogger::get_timestamp >, flxParameterOutString< flxLogger, &flxLogger::get_device_id >, flxParameterOutString< flxLogger, &flxLogger::get_name >, flxParameterOutString< flxLogger, &flxLogger::get_source >, flxParameterOutArrayType< T, Object, _getter >, flxParameterOutArrayType< double, Object, _getter >, flxParameterOutArrayType< float, Object, _getter >, flxParameterOutArrayType< float, flxDevAMG8833, _getter >, flxParameterOutArrayType< flxDevAS7343, &flxDevAS7343::get_spectral_data >, flxParameterOutArrayType< float, flxDevGNSS, _getter >, flxParameterOutArrayType< flxDevTMF882X, &flxDevTMF882X::read_confidence >, flxParameterOutArrayType< flxDevTMF882X, &flxDevTMF882X::read_distance >, flxParameterOutArrayType< flxDevTMF882X, &flxDevTMF882X::read_channel >, flxParameterOutArrayType< flxDevTMF882X, &flxDevTMF882X::read_sub_capture >, flxParameterOutArrayType< flxDevVL53L5, &flxDevVL53L5::read_distance >, and flxParameterOutArrayString< Object, _getter >.

◆ setValueType()

void flxParameter::setValueType ( flxParamValueType_t  type)
inline

◆ type()

virtual flxDataType_t flxParameter::type ( void  )
pure virtual

Implemented in _flxParameterOut< T, Object, _getter >, _flxParameterOut< double, Object, _getter >, _flxParameterOut< float, Object, _getter >, _flxParameterOut< float, flxDevACS37800, _getter >, _flxParameterOut< flxDevACS37800, &flxDevACS37800::read_pos_angle >, _flxParameterOut< flxDevACS37800, &flxDevACS37800::read_pos_power_factor >, _flxParameterOut< float, flxDevADS1015, _getter >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_single_0 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_single_1 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_single_2 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_single_3 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_differential_P0_N1 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_differential_P0_N3 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_differential_P1_N3 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readi_differential_P2_N3 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readu_single_0 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readu_single_1 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readu_single_2 >, _flxParameterOut< flxDevADS1015, &flxDevADS1015::readu_single_3 >, _flxParameterOut< float, flxDevADS122C04, _getter >, _flxParameterOut< float, flxDevAHT20, _getter >, _flxParameterOut< float, flxDevAMG8833, _getter >, _flxParameterOut< flxDevAS7265X, &flxDevAS7265X::read_output_type >, _flxParameterOut< float, flxDevAS7265X, _getter >, _flxParameterOut< float, flxDevAS7331, _getter >, _flxParameterOut< flxDevAS7343, &flxDevAS7343::get_blue_value >, _flxParameterOut< flxDevAS7343, &flxDevAS7343::get_green_value >, _flxParameterOut< flxDevAS7343, &flxDevAS7343::get_red_value >, _flxParameterOut< flxDevAS7343, &flxDevAS7343::get_nir_value >, _flxParameterOut< flxDevAS7343, &flxDevAS7343::get_flicker_value >, _flxParameterOut< flxDevAnalogPin, &flxDevAnalogPin::read_pin_value >, _flxParameterOut< float, flxDevBME280, _getter >, _flxParameterOut< float, flxDevBME68x, _getter >, _flxParameterOut< flxDevBME68x, &flxDevBME68x::read_Status >, _flxParameterOut< float, flxDevBMI270, _getter >, _flxParameterOut< double, flxDevBMP384, _getter >, _flxParameterOut< float, flxDevBMP581, _getter >, _flxParameterOut< float, flxDevBMV080, _getter >, _flxParameterOut< flxDevBMV080, &flxDevBMV080::is_obstructed >, _flxParameterOut< flxDevBioHub, &flxDevBioHub::read_heart_rate >, _flxParameterOut< flxDevBioHub, &flxDevBioHub::read_confidence >, _flxParameterOut< flxDevBioHub, &flxDevBioHub::read_oxygen >, _flxParameterOut< flxDevBioHub, &flxDevBioHub::read_status >, _flxParameterOut< flxDevBioHub, &flxDevBioHub::read_extended_status >, _flxParameterOut< float, flxDevBioHub, _getter >, _flxParameterOut< flxDevButton, &flxDevButton::read_button_state >, _flxParameterOut< float, flxDevCCS811, _getter >, _flxParameterOut< flxDevENS160, &flxDevENS160::read_AQI >, _flxParameterOut< flxDevENS160, &flxDevENS160::read_TVOC >, _flxParameterOut< flxDevENS160, &flxDevENS160::read_ETOH >, _flxParameterOut< flxDevENS160, &flxDevENS160::read_ECO2 >, _flxParameterOut< float, flxDevENS160, _getter >, _flxParameterOut< float, flxDevFS3000, _getter >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_year >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_month >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_day >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_hour >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_min >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_sec >, _flxParameterOut< double, flxDevGNSS, _getter >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_siv >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_fix >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_carrier_soln >, _flxParameterOut< float, flxDevGNSS, _getter >, _flxParameterOut< flxDevGNSS, &flxDevGNSS::read_tow >, _flxParameterOut< float, flxDevISM330Base, _getter >, _flxParameterOut< float, flxDevLPS25HB, _getter >, _flxParameterOut< float, flxDevMAX17048, _getter >, _flxParameterOut< float, flxDevMCP9600, _getter >, _flxParameterOut< double, flxDevMMC5983Base, _getter >, _flxParameterOut< flxDevMMC5983Base, &flxDevMMC5983Base::read_temperature >, _flxParameterOut< float, flxDevMS5637, _getter >, _flxParameterOut< float, flxDevMS8607, _getter >, _flxParameterOut< float, flxDevMicroPressure, _getter >, _flxParameterOut< float, flxDevNAU7802, _getter >, _flxParameterOut< double, flxDevOPT4048, _getter >, _flxParameterOut< flxDevOPT4048, &flxDevOPT4048::get_lux >, _flxParameterOut< flxDevPASCO2V01, &flxDevPASCO2V01::read_CO2 >, _flxParameterOut< flxDevRV8803, &flxDevRV8803::read_year >, _flxParameterOut< flxDevRV8803, &flxDevRV8803::get_epoch >, _flxParameterOut< flxDevSCD30, &flxDevSCD30::read_CO2 >, _flxParameterOut< float, flxDevSCD30, _getter >, _flxParameterOut< flxDevSCD40, &flxDevSCD40::read_CO2 >, _flxParameterOut< float, flxDevSCD40, _getter >, _flxParameterOut< float, flxDevSDP3X, _getter >, _flxParameterOut< float, flxDevSEN54, _getter >, _flxParameterOut< flxDevSGP30, &flxDevSGP30::read_tvoc >, _flxParameterOut< flxDevSGP30, &flxDevSGP30::read_co2 >, _flxParameterOut< flxDevSGP30, &flxDevSGP30::read_h2 >, _flxParameterOut< flxDevSGP30, &flxDevSGP30::read_ethanol >, _flxParameterOut< flxDevSGP40, &flxDevSGP40::read_voc >, _flxParameterOut< float, flxDevSHTC3, _getter >, _flxParameterOut< float, flxDevSTC31, _getter >, _flxParameterOut< flxDevSTHS34PF80, &flxDevSTHS34PF80::read_Presence >, _flxParameterOut< flxDevSTHS34PF80, &flxDevSTHS34PF80::read_Motion >, _flxParameterOut< float, flxDevSTHS34PF80, _getter >, _flxParameterOut< flxDevSoilMoisture, &flxDevSoilMoisture::read_moisture_value >, _flxParameterOut< float, flxDevSoilMoisture, _getter >, _flxParameterOut< flxDevTMF882X, &flxDevTMF882X::read_photon_count >, _flxParameterOut< flxDevTMF882X, &flxDevTMF882X::read_ref_photon_count >, _flxParameterOut< flxDevTMF882X, &flxDevTMF882X::read_ambient_light >, _flxParameterOut< double, flxDevTMP117, _getter >, _flxParameterOut< flxDevTwist, &flxDevTwist::read_button_state >, _flxParameterOut< flxDevTwist, &flxDevTwist::get_twist_count >, _flxParameterOut< flxDevVCNL4040, &flxDevVCNL4040::read_proximity >, _flxParameterOut< flxDevVCNL4040, &flxDevVCNL4040::read_lux >, _flxParameterOut< float, flxDevVEML6075, _getter >, _flxParameterOut< flxDevVEML7700, &flxDevVEML7700::read_ambient_light >, _flxParameterOut< flxDevVEML7700, &flxDevVEML7700::read_white_level >, _flxParameterOut< float, flxDevVEML7700, _getter >, _flxParameterOut< flxDevVL53L1X, &flxDevVL53L1X::read_distance >, _flxParameterOut< flxDevVL53L1X, &flxDevVL53L1X::read_range_status >, _flxParameterOut< flxDevVL53L1X, &flxDevVL53L1X::read_signal_rate >, _flxParameterOut< flxLogger, &flxLogger::get_sample_number >, flxParameterOutArrayType< T, Object, _getter >, flxParameterOutArrayType< double, Object, _getter >, flxParameterOutArrayType< float, Object, _getter >, flxParameterOutArrayType< float, flxDevAMG8833, _getter >, flxParameterOutArrayType< flxDevAS7343, &flxDevAS7343::get_spectral_data >, flxParameterOutArrayType< float, flxDevGNSS, _getter >, flxParameterOutArrayType< flxDevTMF882X, &flxDevTMF882X::read_confidence >, flxParameterOutArrayType< flxDevTMF882X, &flxDevTMF882X::read_distance >, flxParameterOutArrayType< flxDevTMF882X, &flxDevTMF882X::read_channel >, flxParameterOutArrayType< flxDevTMF882X, &flxDevTMF882X::read_sub_capture >, flxParameterOutArrayType< flxDevVL53L5, &flxDevVL53L5::read_distance >, flxParameterOutArrayString< Object, _getter >, _flxParameterIn< T, Object, _setter >, _flxParameterIn< flxDevNAU7802, &flxDevNAU7802::calculate_calibration_factor >, _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_epoch >, _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_seconds >, _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_minutes >, _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_hours >, _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_date >, _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_weekday >, _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_month >, _flxParameterIn< flxDevRV8803, &flxDevRV8803::set_year >, _flxParameterIn< flxDevSGP40, &flxDevSGP40::write_rh >, _flxParameterIn< flxDevSGP40, &flxDevSGP40::write_temperature >, _flxParameterIn< flxDevSTC31, &flxDevSTC31::write_rh >, _flxParameterIn< flxDevSTC31, &flxDevSTC31::write_temperature >, _flxParameterIn< flxDevSTC31, &flxDevSTC31::write_pressure >, _flxParameterIn< flxLogger, &flxLogger::reset_sample_number >, flxParameterInString< Object, _setter >, flxParameterInVoid< Object, _setter >, flxParameterInVoid< flxDevBMI270, &flxDevBMI270::write_reset_step_count >, flxParameterInVoid< flxDevGNSS, &flxDevGNSS::factory_default >, flxParameterInVoid< flxDevNAU7802, &flxDevNAU7802::calculate_zero_offset >, flxParameterInVoid< flxDevSoilMoisture, &flxDevSoilMoisture::calibrate_low_value >, flxParameterInVoid< flxDevSoilMoisture, &flxDevSoilMoisture::calibrate_high_value >, flxParameterInVoid< flxDevTMF882X, &flxDevTMF882X::factory_calibration >, flxParameterInVoid< flxDevice, &flxDevice::disable_all_parameters >, flxParameterInVoid< flxDevice, &flxDevice::enable_all_parameters >, flxParameterInVoid< flxSettingsSave, &flxSettingsSave::save_settings >, flxParameterInVoid< flxSettingsSave, &flxSettingsSave::restore_settings >, flxParameterInVoid< flxSettingsSave, &flxSettingsSave::reset >, flxParameterInVoid< flxSettingsSave, &flxSettingsSave::restore_fallback >, flxParameterInVoid< flxSettingsSave, &flxSettingsSave::save_fallback >, flxParameterInVoid< flxSysFirmware, &flxSysFirmware::restartDevicePrompt >, flxParameterInVoid< flxSysFirmware, &flxSysFirmware::factory_reset >, flxParameterInVoid< flxSysFirmware, &flxSysFirmware::update_firmware_SD >, flxParameterInVoid< flxSysFirmware, &flxSysFirmware::update_firmware_OTA >, flxParameterInVoid< flxSystem, &flxSystem::restartDevicePrompt >, flxParameterInVoid< flxSystem, &flxSystem::resetDevicePrompt >, flxParameterOutString< Object, _getter >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_iso8601 >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_yyyy_mm_dd >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_yyyy_dd_mm >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_dd_mm_yyyy >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_hh_mm_ss >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_fix_string >, flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_carrier_soln_string >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_date_USA >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_date >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_time >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_iso8601 >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_iso8601_tz >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_day >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_day_short >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_ordinal >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_month >, flxParameterOutString< flxDevRV8803, &flxDevRV8803::read_month_short >, flxParameterOutString< flxDevSerial, &flxDevSerial::read_serial_value >, flxParameterOutString< flxLogger, &flxLogger::get_timestamp >, flxParameterOutString< flxLogger, &flxLogger::get_device_id >, flxParameterOutString< flxLogger, &flxLogger::get_name >, flxParameterOutString< flxLogger, &flxLogger::get_source >, flxParameterOut, and flxParameterOutScalar.

◆ valueType()

flxParamValueType_t flxParameter::valueType ( void  )
inline

The documentation for this class was generated from the following file: