flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxParameterInVoid< Object, _setter > Class Template Reference

#include <flxCoreParam.h>

Inheritance diagram for flxParameterInVoid< Object, _setter >:
flxParameterInVoidType flxParameterIn flxParameter flxDescriptor

Public Member Functions

 flxParameterInVoid ()
 
 flxParameterInVoid (Object *me)
 
flxDataType_t type ()
 
void operator() (Object *obj)
 
void operator() (Object *obj, const char *name)
 
void operator() (Object *obj, const char *name, const char *desc)
 
void operator() (Object *obj, const char *name, const char *desc, flxParamValueType_t vtype)
 
void set ()
 
void operator() ()
 
flxEditResult_t editValue (flxDataEditor &theEditor)
 
flxDataLimit * dataLimit (void)
 
bool setValue (flxDataVariable &value)
 
- Public Member Functions inherited from flxParameterInVoidType
 flxParameterInVoidType ()
 
virtual void set (void)=0
 
- Public Member Functions inherited from flxParameterIn
virtual flxEditResult_t editValue (flxDataEditor &)=0
 
virtual bool setValue (flxDataVariable &)=0
 
virtual flxDataLimit * dataLimit (void)=0
 
std::string to_string ()
 
- Public Member Functions inherited from flxParameter
 flxParameter ()
 
bool enabled (void)
 
flxParamValueType_t valueType (void)
 
void setValueType (flxParamValueType_t type)
 
virtual void setEnabled (bool enabled)
 
virtual flxDataType_t type (void)=0
 
- Public Member Functions inherited from flxDescriptor
 flxDescriptor ()
 
void setName (const char *new_name)
 Set the Name object - storing the pointer to the provided string No allocation is performed. If the previous name was allocated, it is freed. More...
 
void setName (const char *new_name, const char *new_desc)
 Set the Name object and the Description for the object. Both strings are constants. More...
 
void setName (char *new_name)
 Set the Name object, but makes a copy of the input string since the input is not const. If the previous name was allocated, it is freed. More...
 
const char * name ()
 Return a const char pointer to the name of the object. More...
 
std::string name_ (void)
 Returns a std::string of the name of the object. More...
 
void setDescription (const char *new_desc)
 Set the Description object - the input value is constant and not copied. If the previous description was allocated, it is freed. More...
 
void setDescription (char *new_desc)
 Set the Description object - the input value is not constant and is copied. If the previous description was allocated, it is freed. More...
 
const char * description ()
 Return the constant C string pointer to the description of the object. More...
 
std::string description_ (void)
 Return the description of the object as a std::string. More...
 
void setTitle (const char *title)
 Set the Title object - the title is optional and is used mostly for UX or organizational purposes. The input value is constant and not copied. If the previous title was allocated, it is freed. More...
 
void setTitleAlloc (char *new_title)
 Set the Title of the object , but make an explict copy of the provided string. More...
 
const char * title (void)
 Return the C constant string pointer to the title of the object. More...
 

Additional Inherited Members

- Public Attributes inherited from flxParameterInVoidType
bool prompt
 
- Protected Attributes inherited from flxDescriptor
const char * _name
 
bool _nameAlloc
 
const char * _desc
 
bool _descAlloc
 
const char * _title
 
bool _titleAlloc
 

Constructor & Destructor Documentation

◆ flxParameterInVoid() [1/2]

template<class Object , void(Object::*)() _setter>
flxParameterInVoid< Object, _setter >::flxParameterInVoid ( )
inline

◆ flxParameterInVoid() [2/2]

template<class Object , void(Object::*)() _setter>
flxParameterInVoid< Object, _setter >::flxParameterInVoid ( Object *  me)
inline

Member Function Documentation

◆ dataLimit()

template<class Object , void(Object::*)() _setter>
flxDataLimit * flxParameterInVoid< Object, _setter >::dataLimit ( void  )
inlinevirtual

Implements flxParameterIn.

◆ editValue()

template<class Object , void(Object::*)() _setter>
flxEditResult_t flxParameterInVoid< Object, _setter >::editValue ( flxDataEditor &  theEditor)
inlinevirtual

Implements flxParameterIn.

◆ operator()() [1/5]

template<class Object , void(Object::*)() _setter>
void flxParameterInVoid< Object, _setter >::operator() ( )
inline

◆ operator()() [2/5]

template<class Object , void(Object::*)() _setter>
void flxParameterInVoid< Object, _setter >::operator() ( Object *  obj)
inline

◆ operator()() [3/5]

template<class Object , void(Object::*)() _setter>
void flxParameterInVoid< Object, _setter >::operator() ( Object *  obj,
const char *  name 
)
inline

◆ operator()() [4/5]

template<class Object , void(Object::*)() _setter>
void flxParameterInVoid< Object, _setter >::operator() ( Object *  obj,
const char *  name,
const char *  desc 
)
inline

◆ operator()() [5/5]

template<class Object , void(Object::*)() _setter>
void flxParameterInVoid< Object, _setter >::operator() ( Object *  obj,
const char *  name,
const char *  desc,
flxParamValueType_t  vtype 
)
inline

◆ set()

template<class Object , void(Object::*)() _setter>
void flxParameterInVoid< Object, _setter >::set ( void  )
inlinevirtual

◆ setValue()

template<class Object , void(Object::*)() _setter>
bool flxParameterInVoid< Object, _setter >::setValue ( flxDataVariable &  value)
inlinevirtual

Implements flxParameterIn.

◆ type()

template<class Object , void(Object::*)() _setter>
flxDataType_t flxParameterInVoid< Object, _setter >::type ( void  )
inlinevirtual

Implements flxParameter.


The documentation for this class was generated from the following file: