flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxParameterOutString< Object, _getter > Class Template Reference

#include <flxCoreParam.h>

Inheritance diagram for flxParameterOutString< Object, _getter >:
flxParameterOutScalar _flxDataOutString flxParameterOut flxDataOut flxDataOut flxParameter flxDescriptor

Public Member Functions

 flxParameterOutString ()
 
flxDataType_t type (void)
 
void operator() (Object *obj)
 
void operator() (Object *obj, const char *name)
 
void operator() (Object *obj, const char *name, const char *desc)
 
void operator() (Object *obj, const char *name, const char *desc, flxParamValueType_t vtype)
 
void setEnabled (bool bEnabled)
 
std::string get () const
 
std::string operator() () const
 
bool getBool ()
 Get the data as a boolean. More...
 
int8_t getInt8 ()
 Get the data as an int8_t. More...
 
int16_t getInt16 ()
 Get the data as an int16_t. More...
 
int32_t getInt32 ()
 Get the data as an int32_t. More...
 
uint8_t getUInt8 ()
 Get the data as a uint8_t. More...
 
uint16_t getUInt16 ()
 Get the data as a uint16_t. More...
 
uint32_t getUInt32 ()
 Get the data as a uint32_t. More...
 
float getFloat ()
 Get the data as a float. More...
 
double getDouble ()
 Get the data as a double. More...
 
std::string getString ()
 Get the data as a string. More...
 
- Public Member Functions inherited from flxParameterOutScalar
flxParameterOutScalar * accessor ()
 
virtual flxDataType_t type (void)=0
 
- Public Member Functions inherited from flxParameterOut
 flxParameterOut ()
 
 flxParameterOut (uint8_t flags)
 
virtual flxDataType_t type (void)=0
 
virtual uint16_t precision (void)
 
virtual flxParameterOut * accessor ()=0
 
uint8_t flags ()
 
- Public Member Functions inherited from flxParameter
 flxParameter ()
 
bool enabled (void)
 
flxParamValueType_t valueType (void)
 
void setValueType (flxParamValueType_t type)
 
virtual void setEnabled (bool enabled)
 
virtual flxDataType_t type (void)=0
 
- Public Member Functions inherited from flxDescriptor
 flxDescriptor ()
 
void setName (const char *new_name)
 Set the Name object - storing the pointer to the provided string No allocation is performed. If the previous name was allocated, it is freed. More...
 
void setName (const char *new_name, const char *new_desc)
 Set the Name object and the Description for the object. Both strings are constants. More...
 
void setName (char *new_name)
 Set the Name object, but makes a copy of the input string since the input is not const. If the previous name was allocated, it is freed. More...
 
const char * name ()
 Return a const char pointer to the name of the object. More...
 
std::string name_ (void)
 Returns a std::string of the name of the object. More...
 
void setDescription (const char *new_desc)
 Set the Description object - the input value is constant and not copied. If the previous description was allocated, it is freed. More...
 
void setDescription (char *new_desc)
 Set the Description object - the input value is not constant and is copied. If the previous description was allocated, it is freed. More...
 
const char * description ()
 Return the constant C string pointer to the description of the object. More...
 
std::string description_ (void)
 Return the description of the object as a std::string. More...
 
void setTitle (const char *title)
 Set the Title object - the title is optional and is used mostly for UX or organizational purposes. The input value is constant and not copied. If the previous title was allocated, it is freed. More...
 
void setTitleAlloc (char *new_title)
 Set the Title of the object , but make an explict copy of the provided string. More...
 
const char * title (void)
 Return the C constant string pointer to the title of the object. More...
 
- Public Member Functions inherited from flxDataOut
virtual flxDataType_t type (void)=0
 Return the type of the data. More...
 
virtual bool getBool ()=0
 Get the data as a boolean. More...
 
virtual int8_t getInt8 ()=0
 Get the data as an int8_t. More...
 
virtual int16_t getInt16 ()=0
 Get the data as an int16_t. More...
 
virtual int32_t getInt32 ()=0
 Get the data as an int32_t. More...
 
virtual uint8_t getUInt8 ()=0
 Get the data as a uint8_t. More...
 
virtual uint16_t getUInt16 ()=0
 Get the data as a uint16_t. More...
 
virtual uint32_t getUInt32 ()=0
 Get the data as a uint32_t. More...
 
virtual float getFloat ()=0
 Get the data as a float. More...
 
virtual double getDouble ()=0
 Get the data as a double. More...
 
virtual std::string getString ()=0
 Get the data as a string. More...
 
bool get_value (bool b)
 Get the value object as a bool. More...
 
int8_t get_value (int8_t)
 Get the value object as an int8_t. More...
 
int16_t get_value (int16_t)
 Get the value object as an int16_t. More...
 
int32_t get_value (int32_t)
 Get the value object as an int32_t. More...
 
uint8_t get_value (uint8_t)
 Get the value object as a uint8_t. More...
 
uint16_t get_value (uint16_t)
 Get the value object as a uint16_t. More...
 
uint32_t get_value (uint32_t)
 Get the value object as a uint32_t. More...
 
float get_value (float)
 Get the value object as a float. More...
 
double get_value (double)
 Get the value object as a double. More...
 
std::string get_value (std::string)
 Get the value object as a string. More...
 
- Public Member Functions inherited from _flxDataOutString
flxDataType_t type (void)
 Return the type of the data. More...
 
virtual std::string get (void) const =0
 
bool getBool ()
 Get the data as a boolean. More...
 
int8_t getInt8 ()
 Get the data as an int8_t. More...
 
int16_t getInt16 ()
 Get the data as an int16_t. More...
 
int32_t getInt32 ()
 Get the data as an int32_t. More...
 
uint8_t getUInt8 ()
 Get the data as a uint8_t. More...
 
uint16_t getUInt16 ()
 Get the data as a uint16_t. More...
 
uint32_t getUInt32 ()
 Get the data as a uint32_t. More...
 
float getFloat ()
 Get the data as a float. More...
 
double getDouble ()
 Get the data as a double. More...
 
std::string getString ()
 Get the data as a string. More...
 

Additional Inherited Members

- Public Types inherited from _flxDataOutString
typedef std::string value_type
 
- Protected Member Functions inherited from flxParameterOut
void setFlag (uint8_t flag)
 
- Protected Attributes inherited from flxDescriptor
const char * _name
 
bool _nameAlloc
 
const char * _desc
 
bool _descAlloc
 
const char * _title
 
bool _titleAlloc
 

Constructor & Destructor Documentation

◆ flxParameterOutString()

template<class Object , std::string(Object::*)() _getter>
flxParameterOutString< Object, _getter >::flxParameterOutString ( )
inline

Member Function Documentation

◆ get()

template<class Object , std::string(Object::*)() _getter>
std::string flxParameterOutString< Object, _getter >::get ( void  ) const
inlinevirtual

Implements _flxDataOutString.

◆ getBool()

template<class Object , std::string(Object::*)() _getter>
bool flxParameterOutString< Object, _getter >::getBool ( )
inlinevirtual

Get the data as a boolean.

Returns
bool

Implements flxDataOut.

◆ getDouble()

template<class Object , std::string(Object::*)() _getter>
double flxParameterOutString< Object, _getter >::getDouble ( )
inlinevirtual

Get the data as a double.

Returns
double

Implements flxDataOut.

◆ getFloat()

template<class Object , std::string(Object::*)() _getter>
float flxParameterOutString< Object, _getter >::getFloat ( )
inlinevirtual

Get the data as a float.

Returns
float

Implements flxDataOut.

◆ getInt16()

template<class Object , std::string(Object::*)() _getter>
int16_t flxParameterOutString< Object, _getter >::getInt16 ( )
inlinevirtual

Get the data as an int16_t.

Returns
int16_t

Implements flxDataOut.

◆ getInt32()

template<class Object , std::string(Object::*)() _getter>
int32_t flxParameterOutString< Object, _getter >::getInt32 ( )
inlinevirtual

Get the data as an int32_t.

Returns
int32_t

Implements flxDataOut.

◆ getInt8()

template<class Object , std::string(Object::*)() _getter>
int8_t flxParameterOutString< Object, _getter >::getInt8 ( )
inlinevirtual

Get the data as an int8_t.

Returns
int8_t

Implements flxDataOut.

◆ getString()

template<class Object , std::string(Object::*)() _getter>
std::string flxParameterOutString< Object, _getter >::getString ( )
inlinevirtual

Get the data as a string.

Returns
std::string

Implements flxDataOut.

◆ getUInt16()

template<class Object , std::string(Object::*)() _getter>
uint16_t flxParameterOutString< Object, _getter >::getUInt16 ( )
inlinevirtual

Get the data as a uint16_t.

Returns
uint16_t

Implements flxDataOut.

◆ getUInt32()

template<class Object , std::string(Object::*)() _getter>
uint32_t flxParameterOutString< Object, _getter >::getUInt32 ( )
inlinevirtual

Get the data as a uint32_t.

Returns
uint32_t

Implements flxDataOut.

◆ getUInt8()

template<class Object , std::string(Object::*)() _getter>
uint8_t flxParameterOutString< Object, _getter >::getUInt8 ( )
inlinevirtual

Get the data as a uint8_t.

Returns
uint8_t

Implements flxDataOut.

◆ operator()() [1/5]

template<class Object , std::string(Object::*)() _getter>
std::string flxParameterOutString< Object, _getter >::operator() ( ) const
inline

◆ operator()() [2/5]

template<class Object , std::string(Object::*)() _getter>
void flxParameterOutString< Object, _getter >::operator() ( Object *  obj)
inline

◆ operator()() [3/5]

template<class Object , std::string(Object::*)() _getter>
void flxParameterOutString< Object, _getter >::operator() ( Object *  obj,
const char *  name 
)
inline

◆ operator()() [4/5]

template<class Object , std::string(Object::*)() _getter>
void flxParameterOutString< Object, _getter >::operator() ( Object *  obj,
const char *  name,
const char *  desc 
)
inline

◆ operator()() [5/5]

template<class Object , std::string(Object::*)() _getter>
void flxParameterOutString< Object, _getter >::operator() ( Object *  obj,
const char *  name,
const char *  desc,
flxParamValueType_t  vtype 
)
inline

◆ setEnabled()

template<class Object , std::string(Object::*)() _getter>
void flxParameterOutString< Object, _getter >::setEnabled ( bool  bEnabled)
inlinevirtual

Reimplemented from flxParameter.

◆ type()

template<class Object , std::string(Object::*)() _getter>
flxDataType_t flxParameterOutString< Object, _getter >::type ( void  )
inlinevirtual

Implements flxParameterOutScalar.


The documentation for this class was generated from the following file: