flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
DataLoggerAIOTConnectionHandler Class Reference

#include <flxIoTArduino.h>

Inheritance diagram for DataLoggerAIOTConnectionHandler:

Public Member Functions

 DataLoggerAIOTConnectionHandler (void)
 
virtual unsigned long getTime ()
 
virtual Client & getClient () override
 
virtual UDP & getUDP () override
 
void setConnected (bool isConnected)
 

Protected Member Functions

NetworkConnectionState update_handleInit ()
 
NetworkConnectionState update_handleConnecting ()
 
NetworkConnectionState update_handleConnected ()
 
NetworkConnectionState update_handleDisconnecting ()
 
NetworkConnectionState update_handleDisconnected ()
 

Detailed Description

our version of the connection handler for arduino IoT. The default assumes it's controlling the WiFi. Sorry, the DataLogger is..

Constructor & Destructor Documentation

◆ DataLoggerAIOTConnectionHandler()

DataLoggerAIOTConnectionHandler::DataLoggerAIOTConnectionHandler ( void  )
inline

Member Function Documentation

◆ getClient()

virtual Client & DataLoggerAIOTConnectionHandler::getClient ( )
inlineoverridevirtual

◆ getTime()

virtual unsigned long DataLoggerAIOTConnectionHandler::getTime ( )
inlinevirtual

◆ getUDP()

virtual UDP & DataLoggerAIOTConnectionHandler::getUDP ( )
inlineoverridevirtual

◆ setConnected()

void DataLoggerAIOTConnectionHandler::setConnected ( bool  isConnected)
inline

◆ update_handleConnected()

NetworkConnectionState DataLoggerAIOTConnectionHandler::update_handleConnected ( )
inlineprotected

◆ update_handleConnecting()

NetworkConnectionState DataLoggerAIOTConnectionHandler::update_handleConnecting ( )
inlineprotected

◆ update_handleDisconnected()

NetworkConnectionState DataLoggerAIOTConnectionHandler::update_handleDisconnected ( )
inlineprotected

◆ update_handleDisconnecting()

NetworkConnectionState DataLoggerAIOTConnectionHandler::update_handleDisconnecting ( )
inlineprotected

◆ update_handleInit()

NetworkConnectionState DataLoggerAIOTConnectionHandler::update_handleInit ( )
inlineprotected

The documentation for this class was generated from the following file: