flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxDataLimitType< T > Class Template Referenceabstract

#include <flxCoreTypes.h>

Inheritance diagram for flxDataLimitType< T >:
flxDataLimit flxDataLimitSetType< std::string > flxDataLimitRange< T > flxDataLimitSetType< T >

Public Member Functions

virtual bool isValid (T value)=0
 
- Public Member Functions inherited from flxDataLimit
virtual ~flxDataLimit ()
 
virtual flxDataLimit_t type (void)
 
flxDataLimitList & limits (void)
 
void addLimit (flxDataLimitDesc &item)
 
void clearLimits (void)
 
virtual std::string getName (flxDataVariable &var)
 

Additional Inherited Members

- Public Types inherited from flxDataLimit
enum  dataLimitType_t { dataLimitNone = 0 , dataLimitRange , dataLimitSet }
 
- Public Attributes inherited from flxDataLimit
flxDataLimitList _dataLimits
 

Member Function Documentation

◆ isValid()

template<typename T >
virtual bool flxDataLimitType< T >::isValid ( T  value)
pure virtual

The documentation for this class was generated from the following file: