![]() |
flux sdk
v01.05.00-6-g190c94c
Embedded C++ SDK
|
This is the complete list of members for flxJob, including all inherited members.
| callHandler(void) | flxJob | inline |
| flxJob() | flxJob | inline |
| flxJob(const char *name, uint32_t in_period) | flxJob | inline |
| name(void) | flxJob | inline |
| oneShot(void) | flxJob | inline |
| period(void) | flxJob | inline |
| setHandler(T *inst, void(T::*func)()) | flxJob | inline |
| setName(const char *name) | flxJob | inline |
| setOneShot(bool bOneShot) | flxJob | inline |
| setPeriod(uint32_t in_period) | flxJob | inline |
| setup(const char *name, uint32_t in_period, T *inst, void(T::*func)(), bool bOneShot=false) | flxJob | inline |