flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxMessageBlock< T > Class Template Reference

#include <flxCoreMsg.h>

Inheritance diagram for flxMessageBlock< T >:
flxMessageBlockCore

Public Member Functions

 flxMessageBlock ()
 
 flxMessageBlock (std::initializer_list< std::pair< const T, const char * > > msgSet)
 
const char * get (int idMessage)
 
const char * get (int idMessage) const
 
virtual const char * get (int idMessage)=0
 
virtual const char * get (int idMessage) const =0
 

Constructor & Destructor Documentation

◆ flxMessageBlock() [1/2]

template<typename T >
flxMessageBlock< T >::flxMessageBlock ( )
inline

◆ flxMessageBlock() [2/2]

template<typename T >
flxMessageBlock< T >::flxMessageBlock ( std::initializer_list< std::pair< const T, const char * > >  msgSet)
inline

Member Function Documentation

◆ get() [1/2]

template<typename T >
const char * flxMessageBlock< T >::get ( int  idMessage)
inlinevirtual

Implements flxMessageBlockCore.

◆ get() [2/2]

template<typename T >
const char * flxMessageBlock< T >::get ( int  idMessage) const
inlinevirtual

Implements flxMessageBlockCore.


The documentation for this class was generated from the following file: